您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

1-25 / 163

排序:
ADS YouTube 影片
Keysight EEsof EDA 在 YouTube 上的先進設計系統(ADS)影片播放清單。

基本展示 2019-07-26

Keysight RFPro in ADS for EM-Circuit Co-Simulation
Keysight RFPro simplifies EM-Circuit co-simulation for the design of RF Modules, MMIC, RFIC and RF Board.

基本展示 2019-03-29

Workspace Management in ADS 2019
Learn about some of the new workspace management features that are part of Advanced Design System (ADS) 2019.

基本展示 2019-01-29

SystemVue 影片庫
Keysight EEsof EDA 在 YouTube 上的 SystemVue 影片播放清單

基本展示 2019-01-09

Datalink Add-on in ADS 2019
Learn how to use the Datalink Add-on feature in Advanced Design System (ADS) 2019 which enables advanced data analysis directly from Data Display using Python.

基本展示 2019-01-03

Avoidance Routing in ADS 2019
Learn how to use the Avoidance Routing feature in Advanced Design System (ADS) 2019 to automatically build DRC-compliant RF Module and Package Designs

基本展示 2019-01-03

Keysight EEsof EDA Videos on YouTube
YouTube channel of Keysight EEsof EDA Videos

基本展示 2018-11-26

How to Solve Signal Integrity Problems: The Basics
How to Solve Signal Integrity Problems: The Basics shows you how to use basic signal integrity (SI) analysis techniques such as eye diagrams, S-parameters, time-domain reflectometry (TDR) and single pulse response to solve signal integrity problems.

使用說明影片 2018-09-18

How to Design for Power Integrity: Optimizing Decoupling Capacitors
This short video will show how to optimize the decoupling capacitors for your next power delivery network.

使用說明影片 2018-06-01

Introduction to Wafer-level Measurement Solutions (WMS) – WMS Series Part 1 of 6
In this video we present an overview of the hardware and software used for making wafer level measurements up to 110 GHz.This is part of a 6 part video series on wafer level measurements.

基本展示 2018-05-09

Automated on-wafer millimeter wave measurements demo – WMS Series Part 2 of 6
In this demo, we measure S-parameters on a GaAs MESFET and capacitor structure in an automated fashion across the wafer. This leverages a lot of pieces together that will be explained in later videos: • configuring the WaferPro Express software to drive other instruments and wafer prober software • wafer alignment • RF S-parameter calibration • WaferPro Express project set up

基本展示 2018-05-09

Perform on-wafer RF calibration – WMS Series Part 5 of 6
In this video, we demonstrate an on wafer network analyzer calibration to 50 GHz.

基本展示 2018-05-09

Configure WaferPro Express for measurements and probing – WMS Series Part 3 of 6
In this video, we will show you how to connect WaferPro Express to the instruments and then to the Velox prober control software.

基本展示 2018-05-09

Set up a measurement project with WaferPro Express – WMS Series Part 6 of 6
In this video, we will set up a new project in WaferPro Express, defining our measurements on our desired devices.

基本展示 2018-05-09

Align wafer probes and create a wafer map – WMS Series Part 4 of 6
In this video, we demonstrate how to align a wafer to the reference plane of our probing system using the auto align feature in Velox. We will then generate a wafer map.

基本展示 2018-05-09

How to Avoid Costly Mistakes in Designing Phased Array Systems
This video will show how to avoid 3 costly steps in designing a phased array. 1) Not predicting the failure of spurious emission masks (SEM) in simulation, which leads to higher development cost and missing time to market windows. 2) Not exploring thoroughly in one simulation, which leads to blind angles. 3) Relying primarily on spreadsheet calculations, which leads to longer design and development cycles.

使用說明影片 2018-02-01

IEEE 802.11ax: Physical Layer Overview
This video provides an overview of the IEEE 802.11ax WLAN standard highlighting the major physical layer technologies and features that are different from legacy WLAN standards.

基本展示 2017-10-02

IEEE 802.11ax: Overcoming Design and Test Challenges with 89600 VSA Software
The IEEE 802.11ax introduces various new technologies and features to meet its goal of higher efficiency, capacity and coverage for a better user experience, especially for dense deployment. These new technologies increase design complexity and create a number of new test challenges. This video covers key IEEE 802.11ax transmitter design and test challenges and how to overcome those challenges with Keysight’s 89600 VSA software.

基本展示 2017-10-02

Top 10 New Signal Integrity and Power Integrity Features in ADS 2017
Advanced Design System (ADS) 2017 is coming soon and here are the top 10 new and exciting Signal Integrity (SI) and Power Integrity (PI) features. The new features aim to save engineers’ time and increase productivity.

基本展示 2017-09-16

Quick Start Guide for ADS in Power Electronics
This guide shows you how to get started with ADS for high di/dt power electronics: incorporate an EM-based model of the layout parasitics from your PCB traces into the circuit simulation.

基本展示 2017-08-15

How to Estimate Voltage Spikes from Layout Parasitic Inductance in Switched-Mode Power Supplies
We showed you how to deal with layout parasitic inductance in our previous video entitled “How to design DC-to-DC power converters”, but a frequently asked question was “When should I start to worry about layout parasitics inductance? Is there a quick rule of thumb that says kind of ‘Caution: Further investigation’s needed?’” The answer is yes and this follow up video is about how to make these estimates.

使用說明影片 2017-07-17

How to Simplify Device Model Extraction using an Open Source User Interface
This video shows an example of an IC-CAP custom user interface (UI) for device modeling. In the selected modeling application, the DC modeling of a Zener diode is intentionally kept simple in order to demonstrate the features of the UI.

使用說明影片 2017-06-26

EDAcafé - DAC 2017 Interview: Michel Azarian, Silicon RFIC EDA Program Manager
Sanjay Gangal from EDAcafé interviews Michel Azarian (Keysight Technologies' Silicon RFIC EDA Program Manager) at Design Automation Conference (DAC) 2017.

基本展示 2017-06-22

IMS 2017: Top 5 Must-See 5G Products
Sponsored by Qorvo, Wireless Design and Development (WDD) counts down the best 5G products out of this year's International Microwave Symposium.

基本展示 2017-06-19

Time & Frequency Domain Simulation-to-Measurement Techniques by Mike Resso
This presentation discusses a step-by-step process that signal integrity engineers can follow to ensure their success in designing with USB Type-C devices.

基本展示 2017-06-18

1 2 3 4 5 6 7 下一頁