您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

1-25 / 136

排序:
Automotive FMCW Analysis with U3851A RF Microwave Courseware
Frequency Modulated Continuous Wave (FMCW) is widely use automotive industry. In this document, we will discuss about FMCW simulation with SystemVue and real-world measurement with the prototyping kit.

應用手冊 2019-07-16

PDF PDF 1.47 MB
Drive Down the Cost of Test Using the ENA Series Vector Network Analyzers - Application Note
Discussion of the contributions of the Keysight ENA series vector network analyzer to drive down the cost of test in production lines. Including an in depth analysis of the total cost of ownership.

應用手冊 2019-06-04

PDF PDF 2.42 MB
Signal Integrity Analysis Series Part 1: Single-Port TDR, TDR/TDT, and 2-Port TDR - Application Note
This Application Note focuses on part 1: those which use a single-port TDR, those which use TDR/TDT, and those which use 2-port TDR.

應用手冊 2019-04-25

如何對 Type-C™ 裝置 執行 USB 電力傳輸(PD)測試
USB Type-CTM 是一項突破性標準,旨在支援全新的超輕薄電腦與裝置,並提供更快的資料速率、更強大的功能及靈活性。USB Type-C 的關鍵點在於裝置間的連接、電源管理,以及確保有效的資料傳輸。

應用手冊 2019-04-20

信號分析量測基礎原理 - 應用說明
對射頻工程師來說,頻譜分析儀或信號分析儀是一種基本又不可或缺的量測工具,使用於產品生命週期的所有階段。效能、 準確度和速度等主要特性,可協助研發工程師提升設計品質,並有助於製造工程師提高測試效率和產品品質。本說明提供了各種技術,可幫助您輕鬆駕馭應用程式的主信號分析。

應用手冊 2019-04-04

Noise Figure Measurement Accuracy - The Y-Factor Method - Application Note
Specific to instruments that use the Y-factor method for noise figure measurements, this app note discusses measurement basics, avoidable errors, loss and temperature corrections, and uncertainties.

應用手冊 2019-03-19

Power Handling Capability of Electromechanical Switches
This application note discusses the power handling of the hot switching and cold switching of EM switches.

應用手冊 2019-02-13

USB 2.0 Compliance Testing with Infiniium Oscilloscopes - Application Note
This Application Note discusses the solution for the USB 2.0 test suite. The Keysight solution is the only one-box solution that uses the official USB-IF scripts for precompliance ans compliance testing.

應用手冊 2019-01-29

Metrology-Grade Measurement Challenges - Application Note
This application note analyzes the sources that contribute to measurement uncertainties and summarizes how to achieve the most accurate measurement results with the Keysight N5531X.

應用手冊 2018-12-20

PDF PDF 819 KB
Probe soldering guidelines for Keysight InfiniiMax probes - Application Note
There are various ways to connect test instrumentation probes to devices under test(DUTs). One such method is soldering, which provides a reliable connection and minimizes parasitic probing effects by keeping wire lengths and connections as short as possible. Many of Keysight's high performance oscilloscopes probes utilize soldered connections.

應用手冊 2018-10-07

PDF PDF 7.73 MB
最佳化射頻和微波頻譜分析儀的動態範圍 -- 應用說明
頻譜分析儀的動態範圍通常定義為:同時出現在頻譜分析儀輸入端之最大與最小信號的比率(以 dB 為單位),其中較小信號的量測可容許到特定程度的不確定性。欲量測的信號可為諧波相關或非諧波相關。

應用手冊 2018-08-13

EMI Troubleshooting: The Need for Close Field Probes - Application Note
This application note introduces close field probes and explains how specific probes offer distinct advantages in electromagnetic compatibility (EMC) radiated emission pre-compliance test.

應用手冊 2018-08-07

An Overview of the Electrical Validation of 10BASE-T, 100BASE-TX, and 1000BASE-T - Application Note
The technology used in these ports, commonly known as “LAN” or “NIC” ports, is usually one of the 10BASE-T, 100BASE-TX, and 1000BASE-T standards or a combination of them.

應用手冊 2018-07-25

Probing a Midpoint of a Transmission Line that is Not Load Terminated - White Paper
With the advent of variable on die termination (i.e. ODT) many systems like low power double data rate memory (LPDDR) have the ability to either terminate a line in its characteristic impedance for high speed operation or terminate it with an open for lower speed operation. Many times there is a desire to probe the transmission line to monitor the signals on the line. When the transmission line is terminated in close to its characteristic impedance, the signals can be readily observed. However, if the line is terminated in an impedance that is not close to the characteristic impedance then it may not be possible to accurately measure the signals.

應用手冊 2018-07-03

PDF PDF 1.98 MB
Bandwidth Boosting Techniques for the Infiniimax Probe Amp and Probe Head - Application Note
Keysight InfiniiMax differential probes are DSP corrected to have a flat magnitude and phase response to provide the highest possible accuracy. The bandwidth chosen to correct to is typically around 3dB non-corrected bandwidth. Usually, extending the bandwidth much beyond that point will increase the noise floor, and if pushed even further, can cause unrealistic noise artifacts. However, the N5381A/B solder-in probe head in combination with the InfiniiMax 1169A/B probe amp is an excellent candidate for extending the bandwidth beyond the 3dB point because the N5381A/B is peaked past the normal 12 GHz bandwidth, and the peaking of the probe head can help compensate for the roll-off of the probe amp bandwidth.

應用手冊 2018-06-21

PDF PDF 4.96 MB
購買經濟型示波器時常見的 5 個錯誤 - 應用說明
根據測試需求選擇合適的示波器並不容易,尤其是預算並不充裕時。您想購買物有所值的產品,不會因為預算有限便犧牲品質。藉由了解人們在購買經濟型示波器時最常犯的錯誤,您可做出最明智的採購決策。

應用手冊 2018-06-06

8 大秘訣幫助您精準執行示波器探測 - 應用說明
本應用說明介紹 8 個重要秘訣,協助您為自己的應用選擇適合的探棒,進而提高示波器探測能力。

應用手冊 2018-04-16

信號分析量測基礎原理 - 應用說明
8大祕訣執行更佳的頻譜分析儀測量A/N:1286-1

應用手冊 2018-04-11

PDF PDF 8 MB
實際溫度量測 - 應用說明
此應用說明旨在探索更多常見的溫度量測技術,並介紹可提高準確度的程序。

應用手冊 2018-03-25

Optimizing Dynamic Range for Distortion Measurements - Application Note
This application note covers high dynamic range measurement techniques for the new PSA Performance Spectrum Analyzer Series. The note describes the best way to use the PSA series to make distortion measurements such as ACP, intermodulation, and harmonic distortion.

應用手冊 2018-03-12

PDF PDF 2.11 MB
Measuring Frequency Response with E5061B LF Network Analyzer
This application note describes fundamentals on low frequency network analysis by featuring the E5061B LF-RF network analyzer. Here we mainly discuss simple low frequency 2-port device measurements and associated topics.

應用手冊 2018-02-22

What is the difference between an equivalent time and a real-time oscilloscope? - Application Note
This document will discuss how each type of oscilloscope samples the incoming waveform and explain the trigger requirements.

應用手冊 2017-12-05

The Application of Handheld Spectrum Analyzers in Interface Testing - Application Note

應用手冊 2017-12-05

Optimizing RF and Microwave Spectrum Analyzer Dynamic Range - Application Note
This application note defines the elements of spectrum analyzer measurement speed and shows how to choose solution bandwidth and data output format for fast measurements.

應用手冊 2017-12-01

Demystifying RCRC and RC probes - Application Note
An ideal probe would provide an exact replica of a signal being probed. However, the probe becomes a part of the circuit under test, because the probe introduces probe loading to the circuit.

應用手冊 2017-12-01

PDF PDF 1.27 MB

1 2 3 4 5 6 下一頁