这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-15 / 15

排序:
为设计和测试工程师扫除上市时间障碍
为设计和测试工程师扫除上市时间障碍

应用说明 2019-08-14

TestOps 如何加速电子设计和测试
TestOps 如何加速电子设计和测试

应用说明 2019-07-17

Extensible VEE Object (EVO) Developer's Guideline - Application Note
Keysight VEE provides a way to extend Keysight VEE functionality by introducing Extensible VEE Object (EVO). Each EVO has its own GUI control and execution behavior, and is similar to generic VEE object.

应用说明 2019-01-28

PDF PDF 1.43 MB
Using MATLAB to Create Keysight Signal and Spectrum Analyzer Applications - Application Note
Learn to use MATLAB software to configure, control, and acquire data from X-Series signal and spectrum analyzers, and then use scripts to create, modify and execute custom analyzer applications.

应用说明 2017-12-01

PDF PDF 9.69 MB
FPGA Implementation of a LUT-Based Digital Pre-Distortion - Application Note
This application note demonstrates the implementation of a signal transformation using a lookup table (LUT). This program transforms a sawtooth signal into a sinusoidal.

应用说明 2017-12-01

FPGA Implementation of a LUT-Based Input Processing - Application Note
This application note demonstrates the implementation of a signal transformation using a lookup table (LUT). It implements a piecewise first-order linear approximation of a nonlinear function.

应用说明 2017-12-01

FPGA Implementation of a Digital-PLL Using FPGAflow - Application Note
This application note demonstrates the capabilities of Keysight M3300A AWG and digitizer PXIe combo module to implement closed-loop controls

应用说明 2017-01-05

Creating Hardware Handler in C/C++ for Keysight TestExec SL
A hardware handler enhances the Keysight TestExec SL's ability to control devices by communicating directly with the instrument's driver. This application note describes how to create hardware handlers for the TestExec SL.

应用说明 2009-09-10

PDF PDF 181 KB
Configuring Signal and Load Switching Using Keysight TestExec SL
This application note describes how users of the Keysight TestExec SL software can easily configure and set up switching for the increasing number of channels on units under test with the Switch Manager feature in the software.

应用说明 2009-08-13

PDF PDF 286 KB
Database Connectivity Guide for TestExec SL
This application note outlines the importance of proper data logging in a database and discusses best practices to import extensible markup language (XML) files from TestExec into a database.

应用说明 2009-07-16

PDF PDF 434 KB
Customizing the Keysight TestExec SL Operator Interface using Visual Basic
This application note describes how users of the Keysight TestExec SL software can customize the operator user interface using Visual Basic.

应用说明 2009-07-07

PDF PDF 312 KB
Automotive Power Window Regulator Testing - Application Note
Automotive power window regulator tests require the use of accurate data acquisition devices, as they cover a wide range of parameters such as window movement, acceleration of the window movement in both directions, maximum range of movement, torque exerted at the start, the end stall torque, and motor load characteristics.

应用说明 2008-06-30

PDF PDF 280 KB
Small Engine Dynamometer Testing - Application Note
Performing Dynamometer Testing on Combustion Engines

应用说明 2008-06-01

PDF PDF 443 KB
Strain Measurement Application Using U2300A Series with Keysight VEE Pro - Application Note
This application note describes how users can make strain and vibration measurements using the Keysight USB DAQ for reliability and strength characterization of concrete and metal structures.

应用说明 2007-05-18

PDF PDF 208 KB
Speeding Production Line Test Development and Execution at Motorola AEIG
This application note documents use of TestExec SL to decrease test development time and increase throughput in a case study with Motorola.

应用说明 2004-02-11

PDF PDF 214 KB