这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-25 / 158

排序:
Low-Cost Power Sources Meet Advanced ADC and VCO Characterization Requirements – Application Note
This application note shows how the low-cost Keysight B2961A/B2962A 6.5 digit power sources can characterize 14-bit ADC circuits and VCOs requiring a 10 microvolt RMS noise floor.

应用说明 2020-05-27

PDF PDF 3.08 KB
Evaluating Battery Run-Down with the N6781A/N6785A Source/Measure Unit and the BV9200B Software
This application note will describe in detail the procedure on evaluating battery run down to easily and accurately evaluate the battery and battery-powered device.

应用说明 2020-02-02

如何最大限度地延长便携式物联网设备的电池续航时间
如何最大限度地延长便携式物联网设备的电池续航时间

应用说明 2019-12-09

When Testing a Device at Multiple Voltages - Use an Output LIST - Application Note
When you need to test a device over a range of power levels, consider using an output LIST. An output LIST allows you to specify a series of steps that change the power supply’s output. Each step controls the output for a set length of time before moving on to the next step.

应用说明 2019-12-02

PDF PDF 2.22 MB
The Power of Emulation - Part 2: Ensuring Electric Cars Perform Flawlessly with Emulation
Design and test engineers are turning to emulation technology to reduce the design verification cycle time and reduce the cost of test to help speed up the transition to EVs.

应用说明 2019-08-28

PDF PDF 3.30 MB
选择和购买台式电源
选择和购买台式电源

应用说明 2019-07-26

是德科技用于太阳能电池和模块测试的温度测量解决方案
是德科技用于太阳能电池和模块测试的温度测量解决方案

应用说明 2019-07-10

Higher Current at at More Voltages Autoranging, Auto-series, and Auto-parallel
Take advantage of autoranging, auto-series, and auto-parallel to provide higher current at more voltages. These capabilities allow a smaller, quieter supply to take the place of a higher power supply.

应用说明 2019-07-10

PDF PDF 2.10 MB
是德科技新兴混动汽车和电动汽车直流对直流转换器设计和测试解决方案
是德科技新兴混动汽车和电动汽车直流对直流转换器设计和测试解决方案

应用说明 2019-07-08

是德科技使用数据记录轻松创建电源输出顺序
是德科技使用数据记录轻松创建电源输出顺序

应用说明 2019-07-05

是德科技自动并联功能如何扩展台式电源的输出范围
是德科技自动并联功能如何扩展台式电源的输出范围

应用说明 2019-07-05

能源生态系统 技术推动电动交通的未来
能源生态系统 技术推动电动交通的未来

应用说明 2019-07-03

电子负载基础知识
电子负载基础知识

应用说明 2019-06-25

在工作台或系统中获得更多可用功率
在工作台或系统中获得更多可用功率

应用说明 2019-06-25

从 μΩ 到 PΩ 的广泛电阻测量解决方案
从 μΩ 到 PΩ 的广泛电阻测量解决方案

应用说明 2019-05-16

How to Create Arbitrary Power Waveforms - Application Note
Creating arbitrary power waveforms, demonstrated with Python and sockets

应用说明 2019-04-15

System Power Supply Programming Using SCPI Commands - White Paper
Learn how to construct a program to send SCPI commands. The example provided uses sockets and Python.

应用说明 2019-04-08

如何使用 Keysight N6790 系列 优化电源测试
如何使用 Keysight N6790 系列 优化电源测试

应用说明 2019-03-25

Improve Voltage Regulation Using Remote Sense - White Paper
Learn how to use remote sense to improve load regulation. Most measurements assume steady load regulation.

应用说明 2018-11-02

PDF PDF 1.01 MB
Avoid Power Related Damage Using Overcurrent Protection with a Multiple Output Power Supply
When multiple voltages power a device, it is often desirable to turn off all the power supply outputs when a fault occurs. If using more than one power supply, daisy chain the digital IO ports such that all outputs, even across mainframes, will be shut down on an overcurrent event. Provide additional protection for a device by using these three functions together - OCP, fault-out and the inhibit function - to shut down all the outputs.

应用说明 2018-10-10

PDF PDF 1.65 MB
Bench-Top Test and Debug of Power Transient Issues for Automotive and Aerospace/Defense Applications
Using the N6705A for bench-top test and debug of power transient issues for automotive and aerospace/defense

应用说明 2018-09-19

Practical Tips to Help You Get the Most Out of the E36300 Series Bench Power Supplies
This application note provides practical tips to get the most out of the E36300 series bench power supplies.

应用说明 2018-08-20

Practical Tips to Help You Get the Most Out of the E36300 Series Bench Power Supplies
This application note provides practical tips to get the most out of the E36300 series bench power supplies.

应用说明 2018-08-20

Save Energy in your High-Power Test Applications - White Paper
This paper discusses on The definition of regenerative power supply and why it matters and also the operation of power supply.

应用说明 2018-08-01

PDF PDF 376 KB
Network analyzer evaluation of RF amplifier using 2961A/62A - Application Brief
This 2-page introduces the Keysight B2961A/62A Power Source and how to perform MMIC RF amplifier S-parameter measurements using it as the DC bias source.

应用说明 2018-03-15

PDF PDF 1.19 MB

1 2 3 4 5 6 7 下一页