这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-25 / 132

排序:
《测试对于自动驾驶汽车的推广至关重要》
《测试对于自动驾驶汽车的推广至关重要》

应用说明 2019-10-22

Next Generation of Test Automation and Systems - Application Note
Application note covering test automation using PathWave Test Automation Software

应用说明 2019-09-23

PDF PDF 1.06 MB
HP8920 Mode on the M8920A - Application Note
HP8920A to M8920A SCPI Compatibility Mode - BETA Release

应用说明 2019-07-11

PDF PDF 563 KB
是德科技如何缩短锂电池自放电测试时间?
是德科技如何缩短锂电池自放电测试时间?

应用说明 2019-07-03

Matching Response Times of Lithium-Ion Cell Self-Discharge Current Measurements
New system calibration method assures well-matched response times of self-discharge current measurements, enabling reliable classification of cells more quickly.

应用说明 2019-05-21

Removing Noise in Lithium-Ion Battery Cell Self-Discharge Data Sets
Li-Ion self discharge measurement data shows significant noise, complicating interpretation. This application note presents a series of algorithms that can effectively remove most of this noise, which improves the reliability of cell classification.

应用说明 2019-05-21

为什么自动驾驶系统将会需要车载以太网
为什么自动驾驶系统将会需要车载以太网

应用说明 2019-04-15

Noise Figure Measurement Accuracy - The Y-Factor Method - Application Note
Specific to instruments that use the Y-factor method for noise figure measurements, this app note discusses measurement basics, avoidable errors, loss and temperature corrections, and uncertainties.

应用说明 2019-03-19

车载毫米波雷达如何增强 先进驾驶辅助系统(ADAS)和自动驾驶
车载毫米波雷达如何增强 先进驾驶辅助系统(ADAS)和自动驾驶

应用说明 2019-03-19

USB 2.0 Compliance Testing with Infiniium Oscilloscopes - Application Note
This Application Note discusses the solution for the USB 2.0 test suite. The Keysight solution is the only one-box solution that uses the official USB-IF scripts for precompliance ans compliance testing.

应用说明 2019-01-29

Testing Automotive DC-DC converter with Keysight TS-8989 - Application Note
This paper discusses emulation of input signals, load simulations and measurements for testing high-power automotive DC-DC converter electronic control units and the TS-8989 functional tester.

应用说明 2018-04-12

PDF PDF 781 KB
Increasing Manufacturing Throughput of Automotive Controllers - Application Note
This application note describes how automotive manufacturers can boost throughput using the Keysight TS-5400 Series 3 high performance PXI function test system for multiple devices under test.

应用说明 2018-02-15

PDF PDF 757 KB
TS-8989 System Integration Guide - Application Note
In today’s manufacturing environment, floor space is an increasingly invaluable variable in the cost of test equation.

应用说明 2017-12-12

PDF PDF 2.69 MB
Measure Lithium Ion Self-Discharge of Cells in a Fraction of the Time Traditionally Required
This new way to determine a cell’s self-discharge by measuring its self-discharge current allows cells with excessively high self-discharge to be identified and isolated much quicker vs traditional open-circuit voltage approaches.

应用说明 2017-12-08

Accelerating Spurious Emission Measurements Using Fast-Sweep Techniques - Application Note
Searching for spurious emissions can be especially difficult and time-consuming. Learn about techniques you can use to optimize and speed your measurements.

应用说明 2017-12-05

Optimizing Power Product Usage to Speed Design Validation Testing - Application Note
This application note is for design validation engineers who need to conduct complex and/or time-consuming tests using power products. It presents methods and techniques to decrease setup time and test time. It is also useful to the manufacturing engineer, as these methods can be beneficial for manufacturing tests.

应用说明 2017-12-05

Right Load Switching and Simulation Design Choices for High Current and Mechatronic Functional Tests
Key considerations for designing a cost-effective high-power switching and load management automotive functional test solution.

应用说明 2017-12-01

PDF PDF 664 KB
The Benefits of Using LXI in Automotive Functional Test
LXI can help maximize performance, minimize cost and extend capital investments into the future. This whitepaper explores the benefits associated with using LXI in Automotive Functional test.

应用说明 2017-12-01

PDF PDF 1.26 MB
是德科技使用 PNA-X 系列网络分析仪精确地测量噪声系数
是德科技使用 PNA-X 系列网络分析仪精确地测量噪声系数

应用说明 2017-11-30

是德科技使用CVI Labwindows在TS-5400 PXI 系列上开发测试程序
是德科技使用CVI Labwindows在TS-5400 PXI 系列上开发测试程序

应用说明 2017-11-29

是德科技使用 Keysight TS-8989 PXI 功能测试系统测试汽车(电子驻车制动) EPB 控制系统
是德科技使用 Keysight TS-8989 PXI 功能测试系统测试汽车(电子驻车制动) EPB 控制系统

应用说明 2017-11-24

Keysight EEsof EDA 使用 3D 场景建模框架的汽车 FMCW 雷达系统设计
Keysight EEsof EDA 使用 3D 场景建模框架的汽车 FMCW 雷达系统设计

应用说明 2017-11-24

是德科技汽车串行总线测试
是德科技汽车串行总线测试

应用说明 2017-11-23

是德科技使用 FieldFox 手持式分析仪进行汽车射频/微波系统验证和故障诊断测试
是德科技使用 FieldFox 手持式分析仪进行汽车射频/微波系统验证和故障诊断测试

应用说明 2017-09-27

Fundamentals of RF and Microwave Noise Figure Measurements - Application Note
This 32-page, black-and-white application note providesinformation on RF and Microwave noise figure measurementts. Topics include noise figure and temperature, noise characteristics of two-port networks, and the measurement of noise figure.

应用说明 2017-09-06

1 2 3 4 5 6 下一页