기술 지원
전자 측정
176-200 / 1602
Virtual Panel for V3500A Handheld RF Power Meter
Virtual Panel for V3500A Handheld RF Power Meter.
프로그램 예제 2012-04-13 |
![]() |
N4916B GUI Example Extended to 14.2G
Stand-alone GUI that supports bit rates up to 14.2 Gb/s.
프로그램 예제 2012-04-04 |
![]() |
33220A 20 MHz Function/Arbitrary Waveform Generator Programming Examples
This document contains 33220A example programs in VB 6.0, Visual C++, VEE, LabView, and Microsoft (R) Excel.
프로그램 예제 2012-02-10 |
|
Library of Waveforms for Trueform Waveform Generators
The 33500 Series and 33600 Series of Trueform waveform generators with built-in arbitrary waveform generators (33511B/33512B/21B/33522B/33611A/33612A /33621A/33622A ) come preloaded with several popular waveforms; Cardiac, exponential fall, exponential rise, Gaussian pulse, Haversine, Lorentz, D-Lorentz, negative ramp, sinc.
프로그램 예제 2012-02-10 |
|
Extensible VEE Object (EVO) Code Sample
An EVO that accepts Y-Expression then generates waveform data points.
프로그램 예제 2012-02-10 |
![]() |
[VBA Sample Program] ENA Control Tool
This program is a intuitive GUI library that enables you to operate the E5071C easily.
프로그램 예제 2012-01-22 |
|
E5071C-TDR HDMI Cable Assembly Test Package
프로그램 예제 2012-01-16 |
![]() |
ENAControlTool_0100.zip
프로그램 예제 2012-01-13 |
![]() |
[VBA Sample Program] Band Pass Filter (BPF) Test Demo VBA for E5061B/E5071C/E5072A
프로그램 예제 2011-11-10 |
|
BPF_TEST_DEMO_E507x_0100.vba
프로그램 예제 2011-10-26 |
![]() |
MultiportControl_E5061B_0100.vba
프로그램 예제 2011-10-24 |
![]() |
SW_Config_E5061B.csv
프로그램 예제 2011-10-24 |
![]() |
4294A Data Transfer Program (Excel VBA) Rev.03.10
For Excel 2007/2010. Download this on your PC. See the 4294A Data Transfer Program Operation Manual.
프로그램 예제 2011-10-07 |
![]() |
4294A Data Transfer Program (Excel VBA)
This program (a VBA macro for Microsoft Excel) transfers the measurement data and the display image from the 4294A to a PC.
프로그램 예제 2011-10-06 |
|
Programming Example: X-Series Screen Capture with Labview
Programming Example: X-Series Screen Capture with Labview
프로그램 예제 2011-09-19 |
![]() |
Band_Pass_Filter_Test_VBA_0100.pdf
프로그램 예제 2011-09-09 |
![]() |
BPF_TEST_DEMO_E5061B_0100.vba
프로그램 예제 2011-09-09 |
![]() |
E5071C CalKit Definition File for USB3.0 Official Calibration Standards with SN01XXX and SN02XXX
For Calibration Standards with Serial Number Starting from SN01XXX or SN02XXX.
프로그램 예제 2011-09-01 |
![]() |
SCPI Learning Page
About half of all test engineers still use the SCPI programming directly to achieve maximum flexibility and performance from their Keysight or other vendor products.
프로그램 예제 2011-08-25 |
|
B2900A Program Examples included in B2900 Product Reference CD-ROM
The sample programs for the Keysight B2900 series Precision Source/Measure Unit including three sweep measurement sample programs written in the following programming languages, Microsoft® Visual C#®, Excel VBA and National Instruments LabVIEW.
Microsoft and Visual C# are trademark or registered trademarks of Microsoft Corporation in the United States and/or other countries.
프로그램 예제 2011-07-25 |
|
[VBA Sample Program] B2900A Forward Biased IV Measurement of Photovoltaic Cells
A Sample VBA program for Microsoft® Excel enables the B2900A Series user to make a forward biased IV measurement and estimate the basic static parameters of photovoltaic cells.
Microsoft is a trademark or registered trademark of Microsoft Corporation in the United States and/or other countries.
프로그램 예제 2011-07-24 |
|
E5071C-TDR VBA File for HDMI 1.4a Cable Assembly Test
프로그램 예제 2011-06-01 |
![]() |
E5071C-TDR State File for HDMI 1.4a Cable Assembly Test (Option 4D5/4K5)
프로그램 예제 2011-06-01 |
![]() |
M9392A Example Programs
Example programs for the M9392A PXI Vector Signal Analyzer. These programs are also provided in the general software installer. Includes sample programs in Visual Studio.net, LabVIEW, MATLAB, LabWindows, and Keysight VEE Pro.
프로그램 예제 2011-05-19 |
![]() |
[VBA 샘플 프로그램] ENA 셋업 마법사 VBA
프로그램 예제 2011-05-12 |
|