Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discutez avec un expert

Support technique

Mesure Electronique

Support by Product Model Number:

Affiner la liste

Par industrie/technologie

Par type de contenu

Par catégorie de produit

126-150 sur 1182

Tri:
5G NR Technology Overview
Slides

Présentation de séminaire 2019-05-01

PDF PDF 5.52 MB
Counter Interferences with Over-the-Air Signal Characterization
Learn how to troubleshoot interferences issues with different workflows and test equipment effectively.

Webcast 2019-04-26

JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013074&CC=US&LC=ENG JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013074&CC=US&LC=ENG
Signal Integrity and Power Integrity Hands-on Workshop with ADS 2017, SIPro and PIPro
It has become much more important to get higher frequency s-parameters for PCB accurately due to ever increasing data rates.

Séminaire

Test Solutions for the Entire EV and EVSE Ecosystem
The HEV/EV market is growing rapidly and the requirements on quality, reliability, and safety are demanding. Learn how to test each component independantly and as a system.

Webcast 2019-04-10

JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013092&CC=US&LC=ENG JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013092&CC=US&LC=ENG
Fundamentals of Sensor Measurements Using a DMM
Learn the critical parameters to test across all sensor types; whether the sensor measures temperature, pressure, flow, strain, light intensity, microwave power, or acoustic level.

Webcast 2019-04-10

JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3015789&CC=US&LC=ENG JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3015789&CC=US&LC=ENG
Modern Network Analyzer Calibration Techniques
Analyze the various calibration methods and learn expert tips to help you select the appropriate calibration method based on the type of measurement and overall measurement needs.

Webcast 2019-04-10

JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013074&CC=US&LC=ENG JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013074&CC=US&LC=ENG
High Speed Digital Design Seminar: New features and capabilities of ADS 2019 U1 for DDR and SerDes
High Speed Digital Design Seminar: New features and capabilities of ADS 2019 Update 1 for DDR and SerDes

Présentation de séminaire 2019-04-10

Keysight EEsof EDA Customer Education and Services
Brief overview of Keysight EDA Customer Education and Services.

Matériel de formation 2019-04-06

Go Green: Reduce Your Product's Power Consumption
Wireless transmissions are often the biggest single consumer of battery charge. Learn how to extend the battery life by optimizing the trade-off between download power and packet error rate.

Webcast 2019-04-05

JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013079&CC=US&LC=ENG JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013079&CC=US&LC=ENG
Redefining Drive Test for 5G
5G NR deployments in 3.5 GHz and 28–29 GHz frequency ranges change testing, impacting drive test coverage measurements and QoE assessments. Learn about 5G NR field measurement and drive test that can be used to optimize 5G QoE.

Webcast 2019-04-04

JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013083&CC=US&LC=ENG JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013083&CC=US&LC=ENG
Fundamentals of Bit Error Ratio Testing
This section covers receiver testing using a Bit Error Ratio Tester (BERT), the typical applications to use a BERT, and what are the key specification to take into consideration when configuring one. In addition, we will be covering the test setup, how to run a typical receiver test, and how the data test pattern is stressed.

Présentation de séminaire 2019-04-03

PDF PDF 1.51 MB
Fundamentals of Arbitrary Waveform Generation
This section gives an overview of the use and importance of an Arbitrary Waveform Generator and how to make sure you have the right Sampling Rate and Memory depth to meet your measurement needs when choosing an AWG. Topics will include key specifications of Arbitrary Waveform Generation, the importance of considering filtering and sampling rate, overview about generating signal impairments and customization of your signal with an AWG.

Présentation de séminaire 2019-04-03

PDF PDF 4.05 MB
High-Speed Oscilloscope Fundamentals
This section will focus on becoming familiarized with oscilloscopes and probing technology from the ground up. Topics will cover sampling rates, bandwidth and aliasing, triggering, waveform visualization tools, waveform update rate, and probing tips and tricks.

Présentation de séminaire 2019-04-03

PDF PDF 2.99 MB
Signal Integrity Measurements and Network Analysis
This section will briefly touch on transmission line fundamentals and then focus on practical ways to troubleshoot and improve physical layer components inside the internet infrastructure. Topics will include differential s-parameters, how mode conversion relates to crosstalk, practical de-embedding methods to increase accuracy and finally a backplane design case study demonstration using a multiport VNA.

Présentation de séminaire 2019-04-03

PDF PDF 5.45 MB
Get Your Game On for Next Generation DRAM: DDR5 and LPDDR5
This presentation will show you how to get your game on so you can master a whole new generation of DRAM.

Présentation de séminaire 2019-04-02

PDF PDF 1.20 MB
Terabit Communication Research with Coherent Optical Modulation Tools
If you plan to use coherent modulation for higher bit rates, this presentation introduces you to the basic concepts of coherent signal measurements, new advanced tools, and provides examples of measurements.

Présentation de séminaire 2019-04-02

PDF PDF 2.67 MB
A Practical Guide to Signal Integrity: From Simulation to Measurement
If you are new to signal integrity, this presentation will give you a head start on your journey, including complimentary example files for continuing your learning. For experienced SI engineers, this presentation is an excellent refresher on the fundamental SI analyses and concepts in both simulation and measurement.

Présentation de séminaire 2019-04-02

PDF PDF 3.89 MB
PCI Express 5.0: Full Speed Ahead! Phy Layer Testing Challenges at 32GT/s
In this presentation, you'll learn not only what's new with the PCIe 5.0 standard but also what to look for as you evaluate tools to help you validate your transmitter and receiver circuits.

Présentation de séminaire 2019-04-02

PDF PDF 2.09 MB
400G: Looking Forward to 800G
Most of the work on the '400G Class' Standards is complete, and new projects are starting to define the electrical links that will enable the next '800G Class' of optical and electrical standards. The low margins we see today will be even smaller or non-existent in the next generation. Verifying compliance for 400G requires careful attention to test setup and execution and will likely require even more discipline moving forward. This session will cover practical techniques to minimize some of the problem areas users are experiencing today in validating compliance in 400G links, and what challenges we may see as the '800G Class' Standards begins to take shape.

Présentation de séminaire 2019-04-02

PDF PDF 1.87 MB
TDECQ for PAM4 Optical Transmitters: Does it Really Work?
The use of PAM4 and forward error correction led to dramatic changes in the test methods used to characterize optical transmitters used in digital communications systems. TDECQ (transmitter dispersion and eye closure quaternary) is the primary example of this change. Does the measurement really provide the results it was intended to yield, specifically the power penalty metric needed to predict how well a transmitter will operate in a real system? This paper will try to document when it does and when it does not.

Présentation de séminaire 2019-04-02

PDF PDF 2.38 MB
Get More Out of Your Instruments with FPGAs
Learn how to easily program FPGAs to experiment with new protocols or envelope tracking values, customize Doppler, delay functions, accelerate a CPU intensive test, and more.

Webcast 2019-03-28

JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013072&CC=US&LC=ENG JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013072&CC=US&LC=ENG
9 Best Practices for Optimizing Your Signal Generator
Watch “9 Best Practices for Optimizing Your Signal Generator” to learn how to make accurate and consistent measurements to optimize your signal generator’s performance for a variety of test applications.

Webcast 2019-03-28

JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013074&CC=US&LC=ENG JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013074&CC=US&LC=ENG
IoT Insights Using an Oscilloscope
As the internet of things (IoT) continues to grow, so does the demand for accuracy in devices. In this webinar, you will learn about common IoT test challenges and how your benchtop oscilloscope can address them.

Webcast 2019-03-28

JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013079&CC=US&LC=ENG JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013079&CC=US&LC=ENG
Accelerating Test Automation Development
Test engineers are under constant pressure to reduce the total cost of test, and at the same time, get products through testing faster. Learn steps that will accelerate your test workflow.

Webcast 2019-03-28

JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013072&CC=US&LC=ENG JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013072&CC=US&LC=ENG
Addressing FEC Challenges on Your 400G Device
Forward error correction (FEC) is a necessity in the 400G world but introduces new test challenges. In this webcast, you will discover tools for debugging and solving your FEC test challenges.

Webcast 2019-03-28

JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013087&CC=US&LC=ENG JSPX?ACTION=REF&CNAME=EDITORIAL&CKEY=3013087&CC=US&LC=ENG

Précédente 1 2 3 4 5 6 7 8 9 10 ... Page suivante