这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

按主题

行业/技术

按内容类型

按产品类别

226-250 / 8103

排序:
Can the U4431A MIPI M-PHY protocol analyzer be controlled from an external PC via the AXIe mainframe's USB port?
Yes, the USB connected chassis option (M9502A-U20/M9505A-U20) is a viable connection strategy when using the U4431A M-PHY Protocol Analyzer instrument.

FAQ 2016-07-08

What termination model (Balanced vs. Unbalanced) should I use for my M8000 BERT?
For M8000 (M8041A/51A/61A/62A) BERT data outputs, a Termination Model must be selected in the Amplifier section of the Parameters window, Balanced or Unbalanced.

FAQ 2016-07-08

EXM Instrument Software Downgrade Procedure
Step by step instructions for how to downgrade your instrument software

FAQ 2016-06-21

PDF PDF 300 KB
Where can I apply for a Free Trial of Keysight EEsof EDA software?
To apply for a free trial of Keysight EDA software, go to: http://www.keysight.com/find/eesof-evaluation

FAQ 2016-06-14

30-Day Free Trial for X-Series Measurement Applications for X-Series Modular Instruments
30-day trial license available for the X-Series measurement applications for X-Series modular signal analyzers.

FAQ 2016-06-09

哪里有合适的教学工具辅助我学习使用 M9018A?
请下载 PXI 机箱交互式方框图,并使用 Adobe Acrobat 软件进行查看。

FAQ 2016-06-06

Keysight Oscilloscope Mobile FAQ
Frequently asked questions about the Keysight Oscilloscope Mobile application.

FAQ 2016-04-21

从哪里可以下载 M9195B 的机械制图?
文件可以导入到您的建模应用软件中。

FAQ 2016-04-19

如何设置 M9485A,使它适用于非是德科技机箱?
需要触发例程。

FAQ 2016-04-19

从哪里可以下载 Y1270A 的机械制图?
文件可以导入到您的建模应用软件中。

FAQ 2016-04-18

What comes standard or pre-configured in my NFA X-Series analyzer and what options are available at the time of initial purchase?
See the list by selecting the link...

FAQ 2016-04-08

配有 E5053A 和 11970 混频器的 E5052B 的相位噪声连续性如何?
请参见此文档。

FAQ 2016-03-29

Where can I find PNA/PNA-L/PNA-X Upgrade Options detail?
This is the link to the CTD external server for PNA family Upgrade option detail

FAQ 2016-03-28

N9010AK-R2C and N9020AK-R2C, Revise to Current Information
N9010AK-R2C and N9020AK-R2C, Revise to Current Information

FAQ 2016-03-22

E8257D and E8267D Option R2C, Revise to Current Information
What option R2C provides

FAQ 2016-03-22

N9030AK Option R2C, Revise to Current Information
N9030AK Option R2C, Revise to Current Information

FAQ 2016-03-22

N9000AK Option R2C, Revise to Current Information
N9000AK Option R2C, Revise to Current Information

FAQ 2016-03-22

Can I make my golden sample’s characteristic trace as the limit for others?
Yes

FAQ 2016-03-17

Does N9322C provide CISPR band presets?
Not exactly

FAQ 2016-03-15

Can N9322C record spectrum over time?
Yes

FAQ 2016-03-15

Does N9322C offer window limit as the N9320B’s?
Yes

FAQ 2016-03-15

In the channel scanner mode, are there any pre-defined standards?
yes

FAQ 2016-03-15

How to edit amplitude correction factor?
correction factor

FAQ 2016-03-15

What does “FSK error” mean in option DMA (ASK/FSK demodulation analysis)?
modulation signal quality

FAQ 2016-03-15

Does N9322C provide CISPR filters and quasi-peak detector?
Yes

FAQ 2016-03-15

以前 1 2 3 4 5 6 7 8 9 10 ... 下一页