Aqui está a página que achamos que você queria. Veja o resultado da pesquisa ao invés de:

 

Contact an Expert

Suporte técnico

Medição Eletrônica

Support by Product Model Number:

Refine the List

By Topic

Mercado/Tecnologia

By Type of Content

Categoria de Produto

126-150 de 8115

Sort:
89601B VSA software and X-Series signal analyzer software compatibility matrix
Supported versions listed here

FAQ 2018-03-20

How Do I Measure the Bit Error Rate (BER) to a Given Confidence Level on the J-BERT M8020A and the M8040A High-Performance BERT?
How do I measure Bit Error Rate (BER) to a given confidence level on J-BERT M8020A and M8040A high-performance BERT?

FAQ 2018-03-01

How do I get replacement parts for individual items in the training kit?
Here are the parts that need to be purchased from Keysight at www.keysight.com/find/parts

FAQ 2018-02-26

5G New Radio Insights to Help You Win in 5G
New 5G communications, such as new radio, mean your designs need to accommodate millimeter wave frequencies, massive MIMO and beamforming, coexistence with LTE and more. See solutions that will help you can innovate, transform, and win in 5G.

FAQ 2018-02-21

Keysight's product portfolio enhanced by Scienlab test solutions for EV and HEV

FAQ 2018-02-12

IO Libraries Suite: What is the latest version? IO Libraries Suite 2018 Update 0.2
IO Libraries Suite 2018 Update 0.2, available online.

FAQ 2018-01-31

What software and options do I need to access the FPGA sandbox in my high-speed digitizer?
Digitizer option FDK enables programming access to the on-board FPGA. Click on the question for additional information.

FAQ 2018-01-18

Where can I find the user documentation for the U5340A FPGA Development Kit (FDK)?
The user documentation is installed on your computer with the software.

FAQ 2018-01-18

How do I downgrade my Infiniium oscilloscope from Windows 10 to Windows 7?
If you bought an Infiniium oscilloscope running Windows 10 and you want to run Windows 7 instead, this document explains how to do so.

FAQ 2017-12-14

M8040AU Upgrades for M8040A 64Gbaud high-performance BERT
M8020A/M8040A Post Purchase Upgrade Option

FAQ 2017-12-13

M8020AU Upgrades for J-BERT M8020A high-performance BERT
M8020A/M8040A Post Purchase Upgrade Option

FAQ 2017-12-13

Signal Analyzer LabVIEW Instrument Drivers
Supported models: N9000A, N9000B, N9010A, N9010B, N9020A, N9020B, N9030A, N9030B, N9038A, M9290A, N9040B, N9041B, M9420A, M9421A, N8973B, N8974B, N8975B, N8976B, M8920A

FAQ 2017-12-01

What is the Embedded Controller Default Password? Answer: Keysight4u!
The default password is “Keysight4u!” for the Administrator account for Windows 10 Enterprise 2016 LTSB. We recommend that you change the password for improved security, because the default password is public knowledge.

FAQ 2017-11-14

Can the state of channel be stored while it is still being actively monitored?
No. The instrument can store the configuration for all channels only while monitoring is OFF. Only measurement attributes of the currently-selected functions (range, resolution, etc) will be preserved in the stored states. If channel monitoring is ON during store / auto-recall execution, the instrument will not function correctly. To restore the instrument back to its initial working state, all modules slotted into the instrument must be removed and the auto-recall function turned OFF. Please refer to the user manual / service manual regarding the usage of the store/auto-recall function.

FAQ 2017-11-13

Free Trial Licenses
Overview of & links to all trial licenses within the N6841A

FAQ 2017-09-28

What are the differences between N6141A/C EMI measurement application and Option EMC?

FAQ 2017-09-28

Is 4338B Adjustment Program still available?
The 4338B adjustment program (04338-65005) that could be found in 4338B Service Manual no longer available…

FAQ 2017-09-26

Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B, N9038A, M9420A, N9000B, N9010B, N9020B, N9030B, N9040B, M9290A, M9420A, M9421A, SPN9026A, SPN9003A, N9041B, M90XA

FAQ 2017-09-21

How to measure output frequency of E4981A Capacitance Meter?
To measure the output frequency of E4981A Capacitance Meter, interface box (Keysight part number: 04294-61002) is required…

FAQ 2017-09-20

Get to Market Faster with a Technology Refresh
Maximize test asset value while lowing cost, securing the right technology, and getting to market on time

FAQ 2017-09-05

Where can I find PNA/PNA-L/PNA-X Firmware, Software and Support information?
This is the link to the CTD external website for PNA Firmware, Software, and other support information

FAQ 2017-08-31

PNA Manual, Firmware, Upgrades, and Support
PNA-L, PNA, and PNA-X Manual, firmware, software, upgrade, and support information. Also available are PNA software utilities, and calibration kit and verification kit data.

FAQ 2017-08-29

What are the recommended power supplies used for U9391C/F/G?
Power supply

FAQ 2017-08-07

Can the B01 bundle for the M9703B digitizer support 1 GHz of bandwidth?
No, the AXIe carrier board in the B01 bundle contains different assemblies than the standard M9703B board. Click on the link for additional information.

FAQ 2017-08-01

Where can I find Signal Integrity, Power Integrity and EMC/EMI resources for high-speed digital designs?
Signal Integrity & Power Integrity Resources from Keysight EEsof EDA at http://www.keysight.com/find/eesof-ads-sipi-resources

FAQ 2017-07-28

Voltar 1 2 3 4 5 6 7 8 9 10 ... Avançar