Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

По теме

По Отрасли/Технологии

По типу содержания

По типу оборудования

226-250 из 8116

Упорядочить:
XY Display Mode Example
The XY time mode converts the oscilloscope from a volts-versus-time display to a volts-versus-volts display using two input channels.

FAQ 2017-02-24

How do I create an amplitude correction file in Excel and load it into my X-Series Analyzer?
Details using Excel can be found here...

FAQ 2017-02-08

Looking for the best cheap oscilloscope?
Professional quality, low cost oscilloscope. Keysight 1000 X-Series oscilloscope proves a cheap oscilloscope doesn't have to be low quality.

FAQ 2017-02-07

Why does my E6640A EXM not have a calibration certificate?
Details can be found here...

FAQ 2017-02-06

Why does the FPGA Configuration Window appear upon boot up?
Information on why the FPGA Configuration Window appears...

FAQ 2017-02-02

Where do I download the mechanical drawings for the M9018B?
Files can be imported into your modeling application.

FAQ 2017-02-01

Where do I download the mechanical drawings for the M9010A?
Files can be imported into your modeling application.

FAQ 2017-02-01

Is there a 3D model of the Infiniium V-Series oscilloscopes?
Yes, see the Step format file downloads.

FAQ 2017-01-25

Комплексное решение по предоставлению услуг калибровки/поверки
Комплексное решение Keysight по предоставлению услуг калибровки/поверки является самым удобным способом, гарантирующим высокую точность, работоспособность и надежность всего парка вашего испытательного оборудования.

FAQ 2017-01-24

Is There a GPS Receiver for FieldFox?
GPS capability has been added to FieldFox starting from firmware revision A.05.33.

FAQ 2017-01-23

Keysight EEsof EDA Distinguished Authors
Keysight EEsof EDA Distinguished Author program.

FAQ 2017-01-20

What is the current rating of the Y113xA cables?
The Y1135A and Y1136A cables are 50 conductor, 24 AWG cables with 25 shielded twisted pairs with PVC insulation. They can be used with the 34921A, 23A, 25A, 31A, 32A, 33A, 37A, 38A, 51A, and 52A plug-in modules for the 34980A. However, they do not support the full rated total current of the 34937A and 34938A. The Y1137A and Y1138A cables are 78 conductor cables 28 AWG conductors with 39 shielded twisted pairs. They can be used with the 34922A, 24A, 34A, 39A, and 34950A plug-in modules.

FAQ 2016-12-13

What are the new Wave 2 features for Mobile WiMAX™ 802.16 system profiles?
Read about IO-MIMO and IO-BF (beamforming) profiles...

FAQ 2016-12-02

What is the maximum USB flash drive storage limit with FieldFox?
FF USB storage

FAQ 2016-11-28

Where do I download the mechanical drawings for the M9019A?
Files can be imported into your modeling application.

FAQ 2016-11-16

Where do I download the mechanical drawings for the M9502A?
Files can be imported into your modeling application.

FAQ 2016-11-16

How do I make the AXIe module show up when there is an empty slot between it and the controller?
If you leave an empty slot between the M9537A controller and an AXIe module, you might not be able to use the AXIe module and an error will show up in Windows Device Manager.

FAQ 2016-11-16

How do I setup for DisplayPort Hot Swap capability?
The M9537A has 3 DisplayPorts that are activated on boot-up. If you move a cable from one DisplayPort to another, you must reboot to activate the new configuration.

FAQ 2016-11-16

Where do I download the mechanical drawings for the M9537A?
Files can be imported into your modeling application.

FAQ 2016-11-16

34972A may freeze when LAN connection is under control after power-up
Yes. The first thing to remember is that the 34972A freeze because the user is trying to communicate with the instrument right after power-up. During that time, the instrument is not yet in ready mode. To prevent the problem, please set a delay (approximately 20s or more time until the instrument boot up completely) after power-up before attempting the LAN communication.

FAQ 2016-11-01

34972A with USB data logging may eventually freeze. How to prevent?
Yes, experience has shown that using a powered USB 2.0 Hub between the 34972A and the PC usually eliminates the problem.Using LAN instead of USB is the recommended solution if possible.

FAQ 2016-10-26

IO Libraries Suite: What has changed in IO Libraries Suite 17.0, 17.1, 17.2, 17.2 Update 1, 17.2 Update 2, 17.3?
Keysight IO Libraries Suite 17 marks a significant update in the architecture of the IO Libraries Suite infrastructure, as well as an all-new Connection Expert...

FAQ 2016-10-26

How do I use myKeysight Keysight Software Manager
Depending on what you want to do, the myKeysight/KSM can help you perform actions such as redeeming an order, resetting your password, viewing, renewing, upgrading or re-hosting a license.

FAQ 2016-10-12

Torque Wrench used with M1971E

FAQ 2016-10-01

Take the Lead in 5G Wireless Technology
Being first and best in 5G wireless communication depends on tools that let you explore new signals, scenarios and topologies. Keysight’s 5G solutions are ready to enable deeper insights as you, and we, evolve with the standard.

FAQ 2016-09-28

Назад 1 2 3 4 5 6 7 8 9 10 ... Следующие