이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

상세 분류

주제별

산업/기술

분야별 검색결과

제품 카테고리별

226-250 / 8143

정렬방식:
What is the dimension and connector location of each modules of the M9485A?

FAQ 2017-05-19

PXI, PXIe 및 AXIe의 데이터 전송 속도는 어떻게됩니까?
PXI-1에는 두가지 경우가 있습니다.

FAQ 2017-05-17

Why is sensor with internal calibration capability not measuring 0dBm after performing zero & calibration process?
Power sensors with internal calibration capability( eg. N192XA, U848x, U2020XA, U2040XA) use its built in reference when performing a zero and calibration.

FAQ 2017-05-05

Is there a 3D model of the InfiniiVision 4000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2017-05-05

89600 VSA Software install fails
Instructions provided to correct this failure

FAQ 2017-04-25

BenchVue 2017 소프트웨어란 무엇입니까?
BenchVue 2017 소프트웨어에 대한 추가 정보.

FAQ 2017-04-25

키사이트 EEsof EDA 판매 지원 팀에 지원을 요청하는 방법
본 FAQ에서 제공된 양식을 이용해서 문의 정보를 제출하십시오.

FAQ 2017-04-24

M9018B와 M9018A의 유사점과 차이점은 무엇인가?
M9018B와 M9018A의 유사점과 차이점

FAQ 2017-04-12

E1407A에 대한 계측기 보안 절차 (영어)

FAQ 2017-04-05

Where can I find product documentation for MBP and MQA?
Product documentation for Model Builder Program (MBP) and/or Model Quality Assurance (MQA) can be found in the Knowledge Center.

FAQ 2017-04-03

Where can I get current and previous software versions as well as updates of MBP and/or MQA?
Current and previous software versions of Model Builder Program (MBP) and/or Model Quality Assurance (MQA) can be found in the Knowledge Center.

FAQ 2017-04-03

How do I renew an expired MBP or MQA license?
General information on renewing an expired Model Builder Program (MBP) or Model Quality Assurance (MQA) license.

FAQ 2017-04-03

How to perform cal factor correction when using 8480 series power sensor ( with cal factor below 85% or above 100%) with old power meters (HP435B/HP43
If you are using an HP435B or HP436A, the minimum cal factor setting is 85% and the maximum is 100%.

FAQ 2017-03-30

Why is the linearity of E441x, E930x, E932x and E/V/W8486A Power Sensors not tested per sensor’s dynamic range?
In actuality, there is little necessity to test linearity of the E4412A and E4413A Power Sensors below -20dBm….

FAQ 2017-03-29

Why is the accuracy of U200x Power Sensors not tested per sensor’s dynamic range?
The accuracy of those sensors is essentially a combination of linearity, instrumentation accuracy and traceability to absolute accuracy at 50MHz, 0dBm.

FAQ 2017-03-29

Is there a 3D model of the M924xA PXIe modular oscilloscopes?
Yes, see the IGES, SAP, Step, EASM, PKG, and PDF format file downloads.

FAQ 2017-03-23

How to maintain 16195B?
The 16195B which consists of Open, Short, 50 Ω Load and Low-loss Capacitor terminations is calibration kit for LCR Meter/Impedance Analyzer and Network Analyzer (NA). The 16195B itself does not have warranted specification as independent product. Maintenance of the 16195B depends on what instrument you calibrate with 16195B.

FAQ 2017-03-15

M9005A의 기계 도면은 어디에서 다운로드할 수 있습니까?
파일을 모델링 어플리케이션으로 가져올 수 있습니다.

FAQ 2017-03-10

All M9301A Synthesizer Instrument Drivers
Supported models: M9301A

FAQ 2017-03-09

All M9214A Digitizer Instrument Drivers
Supported models: M9214A

FAQ 2017-03-09

Can I use Command Expert with non-Keysight instruments?
Yes, you can use Command Expert with any SCPI instrument that follows the SCPI-99 standard, or has an IVI-COM, IVI-C, or IVI.NET driver

FAQ 2017-03-08

XY Display Mode Example
The XY time mode converts the oscilloscope from a volts-versus-time display to a volts-versus-volts display using two input channels.

FAQ 2017-02-24

How do I create an amplitude correction file in Excel and load it into my X-Series Analyzer?
Details using Excel can be found here...

FAQ 2017-02-08

가장 저렴한 오실로스코프를 찾으십니까?
키사이트 1000 X-시리즈 오실로스코프는 믿을 수 없을 정도로 저렴한 가격대에 전문가급 기능성을 지원합니다.

FAQ 2017-02-07

Why does my E6640A EXM not have a calibration certificate?
Details can be found here...

FAQ 2017-02-06

이전 1 2 3 4 5 6 7 8 9 10 ... 다음