이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

상세 분류

주제별

산업/기술

분야별 검색결과

제품 카테고리별

126-150 / 8123

정렬방식:
Keysight I / CV에는 B1500A 드라이버가 있습니까?
아니요.

FAQ 2017-10-31

B1500A는 스위칭 메트릭스 드라이버가 있습니까?

FAQ 2017-10-31

U2651A / U2652Ar에서 디지털 입력 전압 <24V를 지원할 때 28V 디지털 신호를 U2651A / U2652A에 어떻게 입력 할 수 있습니까?
전압 분배기를 연결...

FAQ 2017-10-25

B1500A에 장착 가능한 Capacitor measurement unit(MFCMU)은 몇개인가요?
한개의 MFCMU 장착가능

FAQ 2017-10-25

두 개의 HPSMU를 2채널 메인프레임에 장착 가능한가요?
아니요...

FAQ 2017-10-25

B1500A에서 커브트레이서 모드를 사용 할 수 있나요?
네.. EasyExpert...

FAQ 2017-10-25

What are the differences between N6141A/C EMI measurement application and Option EMC?

FAQ 2017-09-28

Is 4338B Adjustment Program still available?
The 4338B adjustment program (04338-65005) that could be found in 4338B Service Manual no longer available…

FAQ 2017-09-26

Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B, N9038A, M9420A, N9000B, N9010B, N9020B, N9030B, N9040B, M9290A, M9420A, M9421A, SPN9026A, SPN9003A, N9041B, M90XA

FAQ 2017-09-21

How to measure output frequency of E4981A Capacitance Meter?
To measure the output frequency of E4981A Capacitance Meter, interface box (Keysight part number: 04294-61002) is required…

FAQ 2017-09-20

새로운 MD2 드라이버 버전을 설치할 때 FPGA 업그레이드가 필요합니까?
새로운 MD2 소프트웨어 버전을 설치한 후 디지타이저를 초기화할 때 에러 메시지가 표시될 경우 제공되는 지침

FAQ 2017-09-19

Where can I find PNA/PNA-L/PNA-X Firmware, Software and Support information?
This is the link to the CTD external website for PNA Firmware, Software, and other support information

FAQ 2017-08-31

PNA Manual, Firmware, Upgrades, and Support
PNA-L, PNA, and PNA-X Manual, firmware, software, upgrade, and support information. Also available are PNA software utilities, and calibration kit and verification kit data.

FAQ 2017-08-29

What are the recommended power supplies used for U9391C/F/G?
Power supply

FAQ 2017-08-07

Can the B01 bundle for the M9703B digitizer support 1 GHz of bandwidth?
No, the AXIe carrier board in the B01 bundle contains different assemblies than the standard M9703B board. Click on the link for additional information.

FAQ 2017-08-01

테크놀로지 리프레쉬로 출시 시간 단축
테스트 자산 가치를 극대화하는 동시에 비용을 줄이고 적합한 기술을 확보하며 출시 시간을 단축

FAQ 2017-08-01

Is there a 3D model of the InfiniiVision 1000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2017-07-28

What are the Keysight equivalent model numbers for Centellax BERT products and test accessories?
Click on the question for full details of the equivalent model numbers.

FAQ 2017-07-13

다양한 무선 기반IoT 테스트 문제 해결 - NB-IoT부터 NFC까지
교차 플랫폼 측정 알고리즘과 원 버튼 방식의 적합성 평가 소프트웨어를 이용하면 설계 검증부터 제조 및 적합성 테스트에 이르기까지 필요한 IoT 무선 통신 테스트가 간편해집니다.

FAQ 2017-07-05

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

I want to use multiple 2-port M9371A PXIe VNAs in my system. Is option 551 necessary?
If the modules are used as independent 2-port VNAs, no; however, option 551 is necessary to perform true, calibrated, multiport measurements. Click on the question for additional information.

FAQ 2017-06-28

Why has Keysight changed the N9069C licensing structure model?
The N9069C licensing structure model has been collapsed as a customer ordering convenience. Click on the question for additional information.

FAQ 2017-06-28

How do I send the UXM Error Logs to Keysight?
You can use the UXM’s Export Logs function to send the UXM platform log files to the Keysight support team. Click on the question for additional information.

FAQ 2017-06-28

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2017-06-28

Can the PNA-X be configured to install Windows updates as they are pushed out by Microsoft?
Yes, any Windows based machine can be configured to install Windows updates.

FAQ 2017-06-28

이전 1 2 3 4 5 6 7 8 9 10 ... 다음