Here’s the page we think you wanted. See search results instead:

 

Discutez avec un expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

Par sujet

By Industry/Technology

By Type of Content

Par catégorie de produit

176-200 of 8134

Sort:
Signal Analyzer LabVIEW Instrument Drivers
Supported models: N9000A, N9000B, N9010A, N9010B, N9020A, N9020B, N9030A, N9030B, N9038A, M9290A, N9040B, N9041B, M9420A, M9421A, N8973B, N8974B, N8975B, N8976B, M8920A

FAQ 2017-12-01

What is the Embedded Controller Default Password? Answer: Keysight4u!
The default password is “Keysight4u!” for the Administrator account for Windows 10 Enterprise 2016 LTSB. We recommend that you change the password for improved security, because the default password is public knowledge.

FAQ 2017-11-14

Can the state of channel be stored while it is still being actively monitored?
No. The instrument can store the configuration for all channels only while monitoring is OFF. Only measurement attributes of the currently-selected functions (range, resolution, etc) will be preserved in the stored states. If channel monitoring is ON during store / auto-recall execution, the instrument will not function correctly. To restore the instrument back to its initial working state, all modules slotted into the instrument must be removed and the auto-recall function turned OFF. Please refer to the user manual / service manual regarding the usage of the store/auto-recall function.

FAQ 2017-11-13

Free Trial Licenses
Overview of & links to all trial licenses within the N6841A

FAQ 2017-09-28

What are the differences between N6141A/C EMI measurement application and Option EMC?

FAQ 2017-09-28

Is 4338B Adjustment Program still available?
The 4338B adjustment program (04338-65005) that could be found in 4338B Service Manual no longer available…

FAQ 2017-09-26

Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B, N9038A, M9420A, N9000B, N9010B, N9020B, N9030B, N9040B, M9290A, M9420A, M9421A, SPN9026A, SPN9003A, N9041B, M90XA

FAQ 2017-09-21

How to measure output frequency of E4981A Capacitance Meter?
To measure the output frequency of E4981A Capacitance Meter, interface box (Keysight part number: 04294-61002) is required…

FAQ 2017-09-20

Get to Market Faster with a Technology Refresh
Maximize test asset value while lowing cost, securing the right technology, and getting to market on time

FAQ 2017-09-05

Where can I find PNA/PNA-L/PNA-X Firmware, Software and Support information?
This is the link to the CTD external website for PNA Firmware, Software, and other support information

FAQ 2017-08-31

PNA Manual, Firmware, Upgrades, and Support
PNA-L, PNA, and PNA-X Manual, firmware, software, upgrade, and support information. Also available are PNA software utilities, and calibration kit and verification kit data.

FAQ 2017-08-29

What are the recommended power supplies used for U9391C/F/G?
Power supply

FAQ 2017-08-07

Can the B01 bundle for the M9703B digitizer support 1 GHz of bandwidth?
No, the AXIe carrier board in the B01 bundle contains different assemblies than the standard M9703B board. Click on the link for additional information.

FAQ 2017-08-01

What are the Keysight equivalent model numbers for Centellax BERT products and test accessories?
Click on the question for full details of the equivalent model numbers.

FAQ 2017-07-13

Can the PNA-X be configured to install Windows updates as they are pushed out by Microsoft?
Yes, any Windows based machine can be configured to install Windows updates.

FAQ 2017-06-28

For signals requiring wider bandwidth, how can Keysight’s LTE Signal Studio waveform creation products be used to increase carrier spacing?
Set the FFT length to 8192 and a sample rate of 800 MHz. Subcarrier spacing = sampleRate/FFT size

FAQ 2017-06-28

Does M9393A work without M9300? If so, when using the M9393A with 100MHz reference on a pulse generator, what is the external reference input voltage?
When replacing the M9300 with a pulse generator, self-test and alignments may pass. Click on the question for additional information.

FAQ 2017-06-28

When using the DIQ application, what happens when I set the internal receiver to measure beyond the frequency range of my instrument?
Data for frequencies beyond the instrument hardware limitations is extrapolated from the hardware’s maximum and minimum limits. Click on the question for additional information.

FAQ 2017-06-28

Is it possible to develop specific macros for E5061B to support TRL cal or the unknown thru method under a 9-term calibration method?
Yes, it is possible to perform a user developed 8-term calibration, like TRL, using an external program for the E5061B. Click on the question for additional information.

FAQ 2017-06-28

How do I measure a pulsed RF signal output with a sampling oscilloscope?
There are two possible ways. Click on the question for additional information.

FAQ 2017-06-28

Why has Keysight changed the N9069C licensing structure model?
The N9069C licensing structure model has been collapsed as a customer ordering convenience. Click on the question for additional information.

FAQ 2017-06-28

Can the PNA-X support SSLT or SSST calibration techniques?
Yes; however, the Cal Kit must be defined properly to work. The Cal can be modified via Advanced Modify Cal Kit for Definitions under the Calibration menu.

FAQ 2017-06-28

Is it possible to add the N9080B-2TP with the N9080B-1FP installed on the X-Series Analyzer? Should the N9080B-2FP be used instead?
Yes, this is possible. A combination of fixed and transportable licenses can be used.

FAQ 2017-06-28

N9080B SEM measurement defaults seem to be different from 3GPP 36.141 V12.12.0 (2016-06). Is N9080B doing something it shouldn’t?
To make a “True RMS detection”, as requested by the 3GPP conformance testing, based on ITU-R SM.329, for a mix of noise-like & CW-like signals under test, use “Peak Detector with very narrow VBW”. Click on the question for additional information.

FAQ 2017-06-28

How do I send the UXM Error Logs to Keysight?
You can use the UXM’s Export Logs function to send the UXM platform log files to the Keysight support team. Click on the question for additional information.

FAQ 2017-06-28

Previous 1 2 3 4 5 6 7 8 9 10 ... Next