Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discutez avec un expert

Support technique

Mesure Electronique

Support by Product Model Number:

Affiner la liste

Par sujet

Par industrie/technologie

Par type de contenu

Par catégorie de produit

176-200 sur 8100

Tri:
What is the service (repair/calibration) support strategy?
The service (repair/calibration) support strategy of the M9485A is the module level. Only defective module can be returned, if it needs repair.

FAQ 2017-05-25

Which power meter is recommended for system power calibration?
U2000 Series USB Average Power Sensors or U8480 Series USB Thermocouple Power Sensors are recommended.

FAQ 2017-05-25

How many peripheral modules (M9379A, M9341A/B, M9161D, M9111A) are supported on M9485A?
M9485A supports one M9341A/B and up to 6 M9111A. There is no software limitation for M9379A and M9161D.

FAQ 2017-05-25

Can I use multiple M9485A with one controller?
Yes, but there are some limitations. Please refer to below.

FAQ 2017-05-25

How can I order custom configuration for M9485A?
You can order each module/accessory separately as you like. Please refer to below item list and startup guide for detail.

FAQ 2017-05-24

What is the part number of connector saver for the M9376A, M9378A/B?
The connector saver is an adapter of coaxial straight male-SMA female-SMA on the test port of the M9376A, M9378A/B. This adapter can be replaced easily if the connecter is broken or is worn down.

FAQ 2017-05-24

How should I stack 2 PXI chassis for M9485A 2-chassis configuration?
It is recommended to use M9485-60003 1U spacer kit which is included in cable kit for two chassis configurations.

FAQ 2017-05-24

What is the dimension and connector location of each modules of the M9485A?

FAQ 2017-05-19

Is there a 3D model of the InfiniiVision 4000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2017-05-05

Why is sensor with internal calibration capability not measuring 0dBm after performing zero & calibration process?
Power sensors with internal calibration capability( eg. N192XA, U848x, U2020XA, U2040XA) use its built in reference when performing a zero and calibration.

FAQ 2017-05-05

89600 VSA Software install fails
Instructions provided to correct this failure

FAQ 2017-04-25

How do I contact Keysight EEsof EDA Sales Support for help?
Use the form provided in this FAQ to submit your contact information.

FAQ 2017-04-24

Where do I download the mechanical drawings for the Y1271A?
Files can be imported into your modeling application.

FAQ 2017-04-21

Where can I find system requirements and supported platform information for GoldenGate?
For GoldenGate system requirements and supported platform information, refer to the Prerequisites section for your platform at http://www.keysight.comfind/eesof-goldengate-latest-downloads

FAQ 2017-04-06

Explore the Newest Release of GoldenGate and More
List of product-specific release information for GoldenGate

FAQ 2017-04-06

Instrument Security Procedures for E1407A

FAQ 2017-04-05

How do I renew an expired MBP or MQA license?
General information on renewing an expired Model Builder Program (MBP) or Model Quality Assurance (MQA) license.

FAQ 2017-04-03

Where can I find product documentation for MBP and MQA?
Product documentation for Model Builder Program (MBP) and/or Model Quality Assurance (MQA) can be found in the Knowledge Center.

FAQ 2017-04-03

Where can I get current and previous software versions as well as updates of MBP and/or MQA?
Current and previous software versions of Model Builder Program (MBP) and/or Model Quality Assurance (MQA) can be found in the Knowledge Center.

FAQ 2017-04-03

How to perform cal factor correction when using 8480 series power sensor ( with cal factor below 85% or above 100%) with old power meters (HP435B/HP43
If you are using an HP435B or HP436A, the minimum cal factor setting is 85% and the maximum is 100%.

FAQ 2017-03-30

Why is the linearity of E441x, E930x, E932x and E/V/W8486A Power Sensors not tested per sensor’s dynamic range?
In actuality, there is little necessity to test linearity of the E4412A and E4413A Power Sensors below -20dBm….

FAQ 2017-03-29

Why is the accuracy of U200x Power Sensors not tested per sensor’s dynamic range?
The accuracy of those sensors is essentially a combination of linearity, instrumentation accuracy and traceability to absolute accuracy at 50MHz, 0dBm.

FAQ 2017-03-29

What are the similarities and differences between M9018B and M9018A?
Similarities and differences between M9018B and M9018A

FAQ 2017-03-28

Is there a 3D model of the M924xA PXIe modular oscilloscopes?
Yes, see the IGES, SAP, Step, EASM, PKG, and PDF format file downloads.

FAQ 2017-03-23

How to maintain 16195B?
The 16195B which consists of Open, Short, 50 Ω Load and Low-loss Capacitor terminations is calibration kit for LCR Meter/Impedance Analyzer and Network Analyzer (NA). The 16195B itself does not have warranted specification as independent product. Maintenance of the 16195B depends on what instrument you calibrate with 16195B.

FAQ 2017-03-15

Précédente 1 2 3 4 5 6 7 8 9 10 ... Page suivante