Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

By Topic

By Industry/Technology

By Type of Content

By Product Category

226-250 of 8144

Sort:
When using the DIQ application, what happens when I set the internal receiver to measure beyond the frequency range of my instrument?
Data for frequencies beyond the instrument hardware limitations is extrapolated from the hardware’s maximum and minimum limits. Click on the question for additional information.

FAQ 2017-06-28

I am using an electronic load to draw current into my DUT, but when I draw current the voltage drops. Why is this happening?
A voltage drop will appear across this impedance as current flows through it in accordance with Ohm’s Law. Click on the question for additional information.

FAQ 2017-06-28

How do I send the UXM Error Logs to Keysight?
You can use the UXM’s Export Logs function to send the UXM platform log files to the Keysight support team. Click on the question for additional information.

FAQ 2017-06-28

Can the PNA-X support SSLT or SSST calibration techniques?
Yes; however, the Cal Kit must be defined properly to work. The Cal can be modified via Advanced Modify Cal Kit for Definitions under the Calibration menu.

FAQ 2017-06-28

When using OFDM mode in N7610B Signal Studio for Short Range Communications, is User File data supplied by an external file started with MSB or LSB?
The first bit in the file is used first. So this can be thought of as the MSB is used first.

FAQ 2017-06-28

Does the Maury Microwave MT7553B03 50 GHz Noise Receiver Module lower the effective noise figure of the N5245A beyond that of option 029?
Yes, the NF of the 50 GHz PNA-X is about 10 dB for most of its range while the typical NF from the MT7553B03 is 6 dB.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I display the mixer conversion loss of M1970 Series or M1971 Series Harmonic Mixer on an X-Series Signal Analyzer?
There is no way to display the conversion loss values from these mixers on screen. There is a hard copy of the conversion loss data supplied with each mixer that can be referenced.

FAQ 2017-06-28

Can the PNA-X be configured to install Windows updates as they are pushed out by Microsoft?
Yes, any Windows based machine can be configured to install Windows updates.

FAQ 2017-06-28

Why has Keysight changed the N9069C licensing structure model?
The N9069C licensing structure model has been collapsed as a customer ordering convenience. Click on the question for additional information.

FAQ 2017-06-28

Is calibration included in the 86100DU-WN7 Windows 7 upgrade?
86100DU-WN7 is a return to service center upgrade and does include calibration, in addition to a certificate of calibration and data.

FAQ 2017-06-28

When working with high power setups, is it valid to calibrate at low powers and then increase the power after calibration?
Yes, this is valid as long as the source attenuator setting does not change. Click on the question for additional information.

FAQ 2017-06-28

How do I measure a pulsed RF signal output with a sampling oscilloscope?
There are two possible ways. Click on the question for additional information.

FAQ 2017-06-28

Save Time with a Modern Bench Power Supply
The new low cost DC Bench Power Supply from Keysight has three independent outputs & built in data logger. See how a modern Bench Power Supply can help you.

FAQ 2017-06-20

Enabling the fastest path to 5G
Learn more about 5G technologies and the available 5G testing solutions spanning every stage of your design cycle.

FAQ 2017-06-16

How do you know the serial number and calibration date (Last Verification Date) of each module?
See “About NA” in the firmware or Use a tool to check the serial number and calibration date.

FAQ 2017-06-01

Do I require a Control FPGA firmware upgrade when installing a new MD2 software version?
Instructions provided if an error message occurs at the initialization of the digitizer after installing a new MD2 software version

FAQ 2017-05-31

Upgrading 89600 VSA Software
Adding new options, upgrading to new revisions, and adding additional applications is described in this document.

FAQ 2017-05-31

What is the difference of software options between M9485A and PNA/ENA series VNA?
There is no difference for option 007/009/010. There are some differences for options 025, 028, 086 and 551.

FAQ 2017-05-25

How do I install the cables and adapter for the M9485A?
The installation procedure is shown in the M9485A Start Up Guide.

FAQ 2017-05-25

Which PXI chassis is recommended for M9485A?
M9018A/18B and M9019A are recommended.

FAQ 2017-05-25

Which power meter is recommended for system power calibration?
U2000 Series USB Average Power Sensors or U8480 Series USB Thermocouple Power Sensors are recommended.

FAQ 2017-05-25

Is there any system level specification for the M9485A?
No, there is no system level specification.

FAQ 2017-05-25

What is the service (repair/calibration) support strategy?
The service (repair/calibration) support strategy of the M9485A is the module level. Only defective module can be returned, if it needs repair.

FAQ 2017-05-25

How many peripheral modules (M9379A, M9341A/B, M9161D, M9111A) are supported on M9485A?
M9485A supports one M9341A/B and up to 6 M9111A. There is no software limitation for M9379A and M9161D.

FAQ 2017-05-25

Previous 1 2 3 4 5 6 7 8 9 10 ... Next