您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

縮小範圍

依主題

依產業/技術

依內容類型

依產品分類

76-100 / 8110

排序:
How do I remove the root login password on the U3800A Intel Edison?
If the password is misplaced or lost, you will need to reflash Intel Edison firmware. Otherwise, you can remove the password from Edison’s system file.

FAQ 2018-07-25

CX3300 series Windows 10 support
CX3300 series Windows 10 support

FAQ 2018-07-18

PDF PDF 213 KB
Scienlab 的電動車和油電混合車測試解決方案增強了是德科技的產品組合

FAQ 2018-07-16

尋找適用於高速數位生態系統的關鍵解決方案
克服高速數位測試挑戰

FAQ 2018-07-04

增進毫米波頻率的測試
毫米波頻率的測試可能比您預期的難很多,許多在較低頻率下可忽略不計的因素,現在都成了影響成功與否的關鍵要素。了解如何避免對毫米波頻率量測影響甚鉅的主要缺陷。

FAQ 2018-07-03

How do I install the X8711A software?
Use the installation wizard to install the software, or see the supporting document for manual installation.

FAQ 2018-06-28

Manual Installation Instructions
It is recommended to use the installation wizard to install the software components. The installation wizard can be found at keysight.com/find/X8711A under Technical Support then the Drivers, Firmware & Software tab. There is both an on-line and off-line installation download available. If there is a need to manually install the software components, refer to the instructions.

FAQ 2018-06-28

PDF PDF 337 KB
Signal Generator (Signal Source) Upgrade Center
Information to perform a signal generator upgrade or signal source upgrade.

FAQ 2018-06-19

Where can I find software downloads for PathWave Test?
Go to http://www.keysight.com/find/pathwave-test-latest-downloads

FAQ 2018-06-12

How to upgrade your Embedded Controller to Windows 10
You can easily update your Embedded Controller to Windows 10 by swapping out the SSD with a new Windows 10 SSD.

FAQ 2018-06-07

How to upgrade M9036A WES 7 64bit to the PXIe Chassis Family Driver.
If you install the PXIe Chassis Family Driver on M9036A WES 7 64bit and get an error, follow these instructions.

FAQ 2018-06-06

了解最新版 IC-CAP 及其他資訊
詳列不同 IC-CAP 軟體版本資訊。

FAQ 2018-04-28

Why 8990B keep showing disconnected when I connect it through LAN connection?
User need to turn off 8990B firewall, then add LAN instrument at Keysight Connection Expert, and set Instrument Identification to '*IDN query'.

FAQ 2018-04-26

DOC DOC 776 KB
What are the Memory Information and Procedures of the E8404A ?

FAQ 2018-04-19

輕鬆進行頻譜分析,將創意構想化為實際設計
提升頻譜和信號分析技能,貢獻一己之力

FAQ 2018-03-26

89601B VSA software and X-Series signal analyzer software compatibility matrix
Supported versions listed here

FAQ 2018-03-20

How do I get replacement parts for individual items in the training kit?
Here are the parts that need to be purchased from Keysight at www.keysight.com/find/parts

FAQ 2018-02-26

5G NR 洞察力助您贏得 5G 競賽
新的 5G 通訊,例如新空中介面(new radio),要求您的設計必須能同時支援毫米波頻率、大規模 MIMO 和波束成形技術,並與 LTE 共存。請查看有助於您在 5G 中實現創新 、轉型並獲得勝利的解決方案。

FAQ 2018-02-21

IO Libraries Suite: What is the latest version? IO Libraries Suite 2018 Update 0.2
IO Libraries Suite 2018 Update 0.2, available online.

FAQ 2018-01-31

What software and options do I need to access the FPGA sandbox in my high-speed digitizer?
Digitizer option FDK enables programming access to the on-board FPGA. Click on the question for additional information.

FAQ 2018-01-18

Where can I find the user documentation for the U5340A FPGA Development Kit (FDK)?
The user documentation is installed on your computer with the software.

FAQ 2018-01-18

How do I downgrade my Infiniium oscilloscope from Windows 10 to Windows 7?
If you bought an Infiniium oscilloscope running Windows 10 and you want to run Windows 7 instead, this document explains how to do so.

FAQ 2017-12-14

嵌入式控制器的預設密碼為何?答案:Keysight4u!
Windows 10 企業版 2016 LTSB 管理人員帳號的預設密碼是「Keysight4u!」。我們建議您改變密碼以提高安全性,因為預設密碼是公開的。

FAQ 2017-12-14

M8040AU Upgrades for M8040A 64Gbaud high-performance BERT
M8020A/M8040A Post Purchase Upgrade Option

FAQ 2017-12-13

M8020AU Upgrades for J-BERT M8020A high-performance BERT
M8020A/M8040A Post Purchase Upgrade Option

FAQ 2017-12-13

上一個 1 2 3 4 5 6 7 8 9 10 ... 下一頁