这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

行业/技术

按内容类型

按产品类别

按其他类别

251-275 / 1060

排序:
Keysight Technologies Unveils Significant FEM Simulation Speed Increase in Latest 3-D EM Simulation
Keysight announces the latest release of Electromagnetic Professional (EMPro) software, its 3-D electromagnetic simulation software.

新闻资料 2014-12-02

Keysight Demonstrates LTE-A 450 Mbps End-to-End IP Data Throughput with UXM
The E7515A UXM wireless test set provides verification of three component carrier (3CC) end-to-end IP data throughput.

新闻资料 2014-11-18

New Expanded Multi-Vendor Services Capability - Newsroom
Keysight Technologies introduces new expanded multi-vendor services capability

新闻资料 2014-11-14

PCIe® Gen3 Protocol Analysis Test Solution – Press Release

新闻资料 2014-11-06

Keysight Announces Unique Ability to Extend Frequency Range of Existing X-Series Signal Analyzers

新闻资料 2014-11-05

Keysight Technologies Supports B4G/5G Technology Development at National Taiwan University’s
Keysight Supports B4G/5G Technology Development at National Taiwan University’s High-Speed Radio Frequency and mmWave Center

新闻资料 2014-10-24

Keysight to Demonstrate Hardware and Electronic Design Automation Software Solutions at EPEPS 2014
Keysight Technologies announces it will demonstrate its latest hardware and electronic design automation software solution releases at EPEPS 2014, Embassy Suites Portland, Portland, Oregon, Oct. 26-29. Keysight is a silver-level sponsor of the event.

新闻资料 2014-10-23

E6650A EXF One-Box Tester Scales with Volume Growth, Lowers Cost of Test in Femtocell Mfg
Keysight announces the E6650A EXF wireless test set, the industry's first one-box tester dedicated to femtocell manufacturing. Delivering speed, performance and scalability needed to ramp up production and lower the cost of test. Validation with the latest cellular and WLAN chipsets reduces start-up time.

新闻资料 2014-10-21

是德科技推出首款 5G 探测程序库
是德科技推出 Keysight EEsof EDA W1903BEL 5G 基带探测程序库。

新闻资料 2014-10-21

Keysight to Demonstrate Latest RF Circuit, System and 3D EM Design and Simulation Solutions at CSICS
Keysight announces it will demonstrate its latest RF circuit, system and 3D electromagnetic design and simulation solutions at the Compound Semiconductor IC Symposium (CSICS 2014), Hyatt Regency La Jolla at Aventine, San Diego, California, Oct. 19-22. Keysight EEsof EDA is a silver-level sponsor of the event.

新闻资料 2014-10-14

Keysight Technologies Demonstrates Simulation, Debug, Validation and Test Solutions at MemCon
Keysight announces it will demonstrate solutions that provide simulation, debug, validation and test for the fastest speed memory designs at MemCon, Santa Clara Convention Center, Booth102, Santa Clara, Calif., Oct. 15.

新闻资料 2014-10-13

Keysight’s UXA signal analyzer delivers industry-best phase noise, real-time and analysis bandwidth

新闻资料 2014-10-10

Keysight Technologies announces expanded TRX module and EXM wireless test set enhancements
Keysight Technologies Announces Expanded TRX Module and EXM Wireless Test Set Enhancements

新闻资料 2014-10-01

New Agile Signal Generator Delivers Fast, Reliable Switching in Complex Multi-Emitter Simulations

新闻资料 2014-10-01

Keysight Introduces DDR Bus Simulator to Solve the Bit-Error-Rate Contour Simulation Challenge
Keysight Technologies introduces the DDR Bus Simulator; the industry’s first tool to generate accurate Bit-Error-Rate (BER) contours for the JEDEC DDR memory bus specification.

新闻资料 2014-09-30

Keysight Technologies Enters into Manufacturing Test License (MTL) Agreement with Broadcom

新闻资料 2014-09-21

Keysight and Stanford University Work to Streamline Engineering Students’ Experience

新闻资料 2014-09-18

Keysight Expands Functional Test Capabilities, Delivers Greater RF Design Confidence
The E7515A UXM wireless test set includes support for LTE-A category 7 data throughput, expanded functional test capabilities, and in-depth RF performance verification using the X-Series measurement applications.

新闻资料 2014-09-18

Keysight Introduces Industry's First PXIe Signal Analyzer to Provide Swept & FFT Capabilities

新闻资料 2014-09-16

Keysight Technologies' New, Full Two-port 26.5 GHz Vector Network Analyzers Fit in Just One PXI Slot

新闻资料 2014-09-15

Keysight Technologies Introduces Industry's Most Comprehensive Reference Solution for Full Character
Keysight Technologies, Inc. today announced a new PXI Reference Solution for RF power amplifier (PA) characterization and test. The Reference Solution, which performs S-parameter, harmonic distortion, power and demodulation measurements, enables rapid, full characterization of next-generation power amplifier modules, such as a power amplifier-duplexer (PAD).

新闻资料 2014-09-15

Keysight Technologies Introduces 65-GSa/s High-Speed Arbitrary Waveform Generator
Keysight Technologies, Inc. today added a 65-GSa/s, 20-GHz modular instrument to its portfolio of arbitrary waveform generators. The new high-speed, wide-bandwidth M8195A arbitrary waveform generator allows engineers to generate digital, multilevel (e.g. PAM4, MIPI C-PHY) signal scenarios and test their electrical and optical links with complex modulated signals up to 32 GBaud and beyond. This makes the M8195A the most versatile signal generator in the industry.

新闻资料 2014-09-10

M8195A 65GSa/s AWG – Press Release
Introduces 65-GSa/s High-Speed Arbitrary Waveform Generator

新闻资料 2014-09-10

FieldFox 手持式分析仪为卫星地面站提供精确和全面的解决方案

新闻资料 2014-09-09

Keysight Technologies Introduces Logic Analyzer that Captures Industry's Highest Data Rates
Keysight Technologies, Inc. today introduced the industry's highest-data-rate state-mode logic analyzer (up to 4 Gb/s), the industry's first solution for validating simultaneous read and write DDR4 traffic across all byte lanes captured from a DDR4 DIMM operating at data rates of more than 2.5 Gb/s.

新闻资料 2014-09-03

以前 ... 11 12 13 14 15 16 17 18 19 20 ... 下一页