Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По Отрасли/Технологии

По типу содержания

По типу оборудования

По другим категориям

501-525 из 1011

Упорядочить:
Agilent Technologies Introduces Signal Processing Libraries for 802.11ac WLAN and 60-GHz 802.11ad
Agilent Technologies Inc. (NYSE: A) today released SystemVue 2011.10, the latest update to the leading design environment for wireless physical-layer architects.

Материалы для прессы 2011-11-16

Agilent Technologies Introduces Signal Processing Libraries for 802.11ac WLAN and 60-GHz 802.11ad
The release provides new digital signal processing reference libraries for emerging connectivity standards IEEE 802.11ac and 802.11ad, and delivers updates for 4G-LTE, 3G-HSPA and wideband digital predistortion libraries.

Материалы для прессы 2011-11-16

Agilent Technologies Introduces Signal Processing Libraries for 802.11ac WLAN and 60-GHz 802.11ad
Libraries Accelerate R&D Validation and Enable Simulation-to-Test Continuity

Материалы для прессы 2011-11-16

Agilent Technologies Introduces Innovative Multi-Measurement Signal Analyzer Capability for Wireless
Agilent Technologies Inc. (NYSE:A) today announced that an innovative, new multi-measurement capability is being added to its 89600 VSA software, enabling simultaneous signal analysis of multiple carriers and signal formats for more efficient testing and deeper signal insight in wireless test.

Материалы для прессы 2011-11-15

Agilent Technologies to Demonstrate Solutions at MILCOM
Agilent announces it will demonstrate its latest military communications test technologies and tools at MILCOM, Nov. 7-10, at the Baltimore Convention Center (Booth 1201) in Baltimore.

Материалы для прессы 2011-11-01

World’s First WiGig Technology Plugfest - Press Material
Ron Nersesian, President of Agilent’s Electronic Measurement Group, shares Agilent’s product contributions to support the first annual WiGig Technology Plugest with baseband, RF and mmWave signal generation and analysis capability.

Материалы для прессы 2011-10-24

Agilent Technologies Introduces Industry's First 3GPP Release 9 Compliant MSR Signal
Ideal for engineers manufacturing base stations and base-station components, the MSR measurement application enables one-button, standards-based testing per the RF requirements defined in the TR 37 series of the 3GPP Release 9 standard. It is the first and only 3GPP-compliant one-button measurement application on the market today to quickly and easily manufacture MSR base stations and base-station components.

Материалы для прессы 2011-10-19

Enhancements for Ease of Use, Wider Functionality on Handheld Spectrum Analyzers

Материалы для прессы 2011-10-19

Agilent Technologies Introduces 2.8-Gb/sec Entry-Level Option for Industry's Fastest Logic Analyzer
Agilent Technologies Inc. (NYSE: A) today introduced a new lower-priced entry-level 1.4-Gb/sec state mode option for the industry's fastest logic analyzer, the Agilent U4154A.

Материалы для прессы 2011-10-18

Agilent Technologies Introduces World's First 67-GHz Nonlinear Vector Network Analyzer
Using this hardware, designers can easily characterize and model components accurately up to frequencies of 67 GHz. In addition, X-parameters can be measured up to 67 GHz, providing an accurate model of linear and nonlinear component behavior at very high frequencies and wide bandwidth.

Материалы для прессы 2011-10-17

Agilent Technologies Introduces Wireless Link Analysis Software Accelerates Troubleshooting

Материалы для прессы 2011-10-10

Agilent Technologies Introduces First Complete and Compliant 60-GHz Wireless Test Solution
Agilent Technologies Introduces First Complete and Compliant 60-GHz Wireless Test Solution

Материалы для прессы 2011-10-10

Latest RF Design and 3-D EM Simulation Platforms Enhance Multi-technology Design, Speed Simulation
Agilent announces new versions of Advanced Design System (ADS) and Electromagnetic Professional (EMPro) software.

Материалы для прессы 2011-10-10

Agilent Technologies Introduces First Complete and Compliant 60 GHz Wireless Test Solution
Agilent announces the first complete and compliant test solution for 60-GHz wireless devices, including WiGig, WirelessHD and IEEE 802.11ad devices.

Материалы для прессы 2011-10-10

TowerJazz Expands its High Speed SiGe, SOI and RF CMOS Design Kits for use with ADS 2011
TowerJazz Press Release

Материалы для прессы 2011-10-06

PDF PDF 104 KB
Agilent Introduces First-to-Market Functional Test Solution for MIPI D-PHY Standard Interconnects

Материалы для прессы 2011-10-04

Agilent Technologies' All-in-One MIPI D-PHY Test Platform Selected by ST Microelectronics

Материалы для прессы 2011-10-04

Agilent Launches Industry's First Complete MIPI M-PHY Test Suite

Материалы для прессы 2011-10-04

Agilent Technologies Announces Industry's First MIPI M-PHY Transmitter Compliance Test Software
Agilent today announced the industry's first MIPI M-PHY compliance test software package for transmitter validation.

Материалы для прессы 2011-09-28

Agilent to Demonstrate Newest Test Solutions for MW, RF, Wireless, Radar at European Microwave Week
Agilent announces that it will show its newest test and measurement solutions in microwave, RF, wireless and radar for telecommunications, transportation and medical markets at European Microwave Week.

Материалы для прессы 2011-09-27

N6700 Modular Power System Adds Application-Specific Modules for Battery Test, Mobile Device Mfg

Материалы для прессы 2011-09-27

Agilent Technologies Debuts PXI-Based Digital Multimeters

Материалы для прессы 2011-09-27

Agilent Technologies Expands PXI Digital Multimeter Offering with Low-Cost PXI Digital Multimeter

Материалы для прессы 2011-09-27

Agilent’s PXA Signal Analyzer Now Enables Wideband Measurement with up to 900 MHz of Bandwidth

Материалы для прессы 2011-09-21

IHP Expands its SiGe Process Design Kit Offerings for Use with ADS 2011 Software Release
Innovations for High Performance Microelectronics (IHP) announces the availability of leading-edge ADS PDKs for its 0.25 μm SiGe process (SG25H3) and 0.13 μm SiGe process (SG13S).

Материалы для прессы 2011-09-20

PDF PDF 115 KB

Назад ... 21 22 23 24 25 26 27 28 29 30 ... Следующие