Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По Отрасли/Технологии

По типу содержания

По типу оборудования

По другим категориям

251-275 из 1011

Упорядочить:
Keysight Technologies and Kwangwoon University Radio Research Center Co-host 5G and mmWave Workshop
Keysight Technologies co-hosted a 5G and millimeter-Wave (mmWave) workshop with Kwangwoon University Radio Research Center, Seoul, South Korea. The 5G event, held in October, was the first co-hosted event in the region with over 190 in attendance.

Материалы для прессы 2014-12-04

Keysight Technologies and Kwangwoon University Radio Research Center Co-host 5G and mmWave Workshop
Keysight co-hosted a 5G and millimeter-Wave workshop with Kwangwoon University Radio Research Center, Seoul, South Korea

Материалы для прессы 2014-12-04

Keysight Technologies Unveils Significant FEM Simulation Speed Increase in Latest 3-D EM Simulation
Keysight announces the latest release of Electromagnetic Professional (EMPro) software, its 3-D electromagnetic simulation software.

Материалы для прессы 2014-12-02

Keysight Demonstrates LTE-A 450 Mbps End-to-End IP Data Throughput with UXM
The E7515A UXM wireless test set provides verification of three component carrier (3CC) end-to-end IP data throughput.

Материалы для прессы 2014-11-18

New Expanded Multi-Vendor Services Capability - Newsroom
Keysight Technologies introduces new expanded multi-vendor services capability

Материалы для прессы 2014-11-14

PCIe® Gen3 Protocol Analysis Test Solution – Press Release

Материалы для прессы 2014-11-06

Keysight Announces Unique Ability to Extend Frequency Range of Existing X-Series Signal Analyzers

Материалы для прессы 2014-11-05

Keysight Technologies Supports B4G/5G Technology Development at National Taiwan University’s
Keysight Supports B4G/5G Technology Development at National Taiwan University’s High-Speed Radio Frequency and mmWave Center

Материалы для прессы 2014-10-24

Keysight to Demonstrate Hardware and Electronic Design Automation Software Solutions at EPEPS 2014
Keysight Technologies announces it will demonstrate its latest hardware and electronic design automation software solution releases at EPEPS 2014, Embassy Suites Portland, Portland, Oregon, Oct. 26-29. Keysight is a silver-level sponsor of the event.

Материалы для прессы 2014-10-23

Keysight Technologies Introduces Industry's First 5G Exploration Library
Keysight introduces the Keysight EEsof EDA W1903BEL 5G Baseband Exploration Library.

Материалы для прессы 2014-10-21

E6650A EXF One-Box Tester Scales with Volume Growth, Lowers Cost of Test in Femtocell Mfg
Keysight announces the E6650A EXF wireless test set, the industry's first one-box tester dedicated to femtocell manufacturing. Delivering speed, performance and scalability needed to ramp up production and lower the cost of test. Validation with the latest cellular and WLAN chipsets reduces start-up time.

Материалы для прессы 2014-10-21

Keysight to Demonstrate Latest RF Circuit, System and 3D EM Design and Simulation Solutions at CSICS
Keysight announces it will demonstrate its latest RF circuit, system and 3D electromagnetic design and simulation solutions at the Compound Semiconductor IC Symposium (CSICS 2014), Hyatt Regency La Jolla at Aventine, San Diego, California, Oct. 19-22. Keysight EEsof EDA is a silver-level sponsor of the event.

Материалы для прессы 2014-10-14

Keysight Technologies Demonstrates Simulation, Debug, Validation and Test Solutions at MemCon
Keysight announces it will demonstrate solutions that provide simulation, debug, validation and test for the fastest speed memory designs at MemCon, Santa Clara Convention Center, Booth102, Santa Clara, Calif., Oct. 15.

Материалы для прессы 2014-10-13

Keysight’s UXA signal analyzer delivers industry-best phase noise, real-time and analysis bandwidth

Материалы для прессы 2014-10-10

Keysight Technologies announces expanded TRX module and EXM wireless test set enhancements
Keysight Technologies Announces Expanded TRX Module and EXM Wireless Test Set Enhancements

Материалы для прессы 2014-10-01

New Agile Signal Generator Delivers Fast, Reliable Switching in Complex Multi-Emitter Simulations

Материалы для прессы 2014-10-01

Keysight Introduces DDR Bus Simulator to Solve the Bit-Error-Rate Contour Simulation Challenge
Keysight Technologies introduces the DDR Bus Simulator; the industry’s first tool to generate accurate Bit-Error-Rate (BER) contours for the JEDEC DDR memory bus specification.

Материалы для прессы 2014-09-30

Keysight Technologies Enters into Manufacturing Test License (MTL) Agreement with Broadcom

Материалы для прессы 2014-09-21

Keysight Expands Functional Test Capabilities, Delivers Greater RF Design Confidence
The E7515A UXM wireless test set includes support for LTE-A category 7 data throughput, expanded functional test capabilities, and in-depth RF performance verification using the X-Series measurement applications.

Материалы для прессы 2014-09-18

Keysight and Stanford University Work to Streamline Engineering Students’ Experience

Материалы для прессы 2014-09-18

Keysight Introduces Industry's First PXIe Signal Analyzer to Provide Swept & FFT Capabilities

Материалы для прессы 2014-09-16

Keysight Technologies' New, Full Two-port 26.5 GHz Vector Network Analyzers Fit in Just One PXI Slot

Материалы для прессы 2014-09-15

Keysight Technologies Introduces Industry's Most Comprehensive Reference Solution for Full Character
Keysight Technologies, Inc. today announced a new PXI Reference Solution for RF power amplifier (PA) characterization and test. The Reference Solution, which performs S-parameter, harmonic distortion, power and demodulation measurements, enables rapid, full characterization of next-generation power amplifier modules, such as a power amplifier-duplexer (PAD).

Материалы для прессы 2014-09-15

Keysight Technologies Introduces 65-GSa/s High-Speed Arbitrary Waveform Generator
Keysight Technologies, Inc. today added a 65-GSa/s, 20-GHz modular instrument to its portfolio of arbitrary waveform generators. The new high-speed, wide-bandwidth M8195A arbitrary waveform generator allows engineers to generate digital, multilevel (e.g. PAM4, MIPI C-PHY) signal scenarios and test their electrical and optical links with complex modulated signals up to 32 GBaud and beyond. This makes the M8195A the most versatile signal generator in the industry.

Материалы для прессы 2014-09-10

M8195A 65GSa/s AWG – Press Release
Introduces 65-GSa/s High-Speed Arbitrary Waveform Generator

Материалы для прессы 2014-09-10

Назад ... 11 12 13 14 15 16 17 18 19 20 ... Следующие