这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

行业/技术

按内容类型

按产品类别

51-75 / 880

排序:
University Uses ADS to Create an Impedance Matching Method for Wireless Battery Charging
Learn how NCKU created an impedance matching method for wireless battery charging using Keysight ADS.

案例分析 2019-03-14

PDF PDF 2.27 MB
4 种方法打造专属电源使用技巧
4 种方法打造专属电源使用技巧

电子书 2019-03-12

PDF PDF 2 MB
How to Resolve the Evaluation and Validation Challenge in Mobile Devices - Case Study
As mobile devices get faster and sport more functions and features, they run up against battery limits. This outlines how mobile device/circuit design engineer uses a device current waveform analyzer to solve their power distribution network implementation challenges.

案例分析 2019-02-19

PDF PDF 3.51 MB
5G NR Device Manufacturer Doubles Test Capacity
A leading 5G new radio device manufacturer doubles text capacity with zero additional CapEx through Keysight Financial Services.

案例分析 2019-02-19

PDF PDF 3.46 MB
Successful Deployment of eCall Live Crash Test - Case Study
Car maker successfully emulates over-the-air environments in live crash test for their emergency call in-vehicle systems, with the eCall/ERA-GLONASS conformance test solution from Keysight.

案例分析 2018-12-13

PDF PDF 5.10 MB
Fast Thermal Characterization and Testing on Your Electronic Devices - White Paper

文章 2018-12-11

PDF PDF 3.89 MB
Coherent Optical Component Test Enables 1.2 Terabit Applications - Case Study
Using Keysight’s state-of-the-art test equipment, NeoPhotonics successfully validated the performance of its 64 GBaud components, including its new 400ZR COSA, almost one year before the availability of DSP silicon for the transceivers. Without Keysight equipment, NeoPhotonics had no way of testing and assessing the performance of their components.

案例分析 2018-12-11

PDF PDF 2.06 MB
Pushing the Boundaries to Achieve Ultra-broadband Communications at True Terahertz Frequencies
See how researchers at the University at Buffalo achieved the first ever system to transmit and receive communications at 1.025 terahertz.

内部通讯 2018-12-10

PDF PDF 23 KB
Electronics OEM Taps Keysight Automotive Radar Solution to Support Autonomous Driving R&D
Electronics manufacturer jumpstarts automotive radar application design and test efforts with Keysight solution, saving test development time and improving initial test coverage by over 50 percent.

案例分析 2018-11-26

PDF PDF 2.97 MB
Putting the Future in Motion with Automotive Ethernet
Continental adopts Keysight's automotive Ethernet test solution for 100BASE-T1, 1000BASE-T1, DDR memory, and USB connectivity compliance testing.

案例分析 2018-11-16

PDF PDF 3.30 MB
Protecting Government Wireless Systems with Detailed Signal Emulation and Interference Analysis
Agency researchers were asked to investigate signal interference and spectral coexistence related to the performance of government systems in the presence of commercial wireless signals. Much of the work was to be completed in a laboratory setting, and this suggested the use of an advanced solution for signal creation, emulation, measurement and analysis.

案例分析 2018-11-14

PDF PDF 4.48 MB
Water Meter Manufacturer Reduces Development Cycle by Two Months - Case Study
Using the X8712A IoT Device Battery Life Optimization Solution, one large water meter manufacturer in China was able to shave two months off their development and test time, and improved their design, extending battery life to over 10 years. This case study explained how the manufacturer was able to achieve their design excellence.

案例分析 2018-10-17

PDF PDF 3.57 MB
A Leading AR/VR Solution Provider Saves 60% of Time While Optimizing Battery Life
Case study reveals how a leading provider saved 60% of test development and testing time during design validation and significantly improved battery life, solving the issue with the heavy battery pack.

案例分析 2018-09-19

PDF PDF 2.64 MB
Keysight One-Stop Calibration Capabilities - Asia (Australia)
Keysight One-Stop Calibration Capabilities - Asia (Australia)

文章 2018-09-19

Different Strategies for Preparing Students to Tackle the RF Engineering Challenges of Tomorrow
Panel universities discuss the positive impact of leveraging Keysight’s RF and Microwave Education Programs to develop next generation RF industry-ready engineers.

文章 2018-09-04

PDF PDF 2.40 MB
A Pilot Program in Internet-of-things with University and Industry Collaboration
University of New Haven in collaboration with Keysight Technologies have embarked on offering a sequence of two IoT courses to teach the concepts and functionalities of the IoT technologies.

文章 2018-09-04

PDF PDF 2.10 MB
4 More Ways to Build Your Power Supply Skill Set: Part 2
Today's designs place higher demands on the systems that power them, and more design problems are being caused by these power systems. This eBook supplements the first set of power skills and provides four additional tips to build your power supply skill set.

电子书 2018-08-28

PDF PDF 2.89 MB
Using Arduino in Engineering Education: Motivating Students to Grow from a Hobbyist to Professional
Keysight Technologies in collaboration with top US engineering schools have developed Arduino-based projects as motivators for advanced electronic engineering education in industrial setting.

文章 2018-08-27

PDF PDF 4.37 MB
Extending the Operating Life of IoT Devices with a Wireless Energy-Harvesting - Case Study
Geneva-based STMicroelectronics and French university Ecole Supérieure d’Electronique de l’Ouest (ESEO) collaborated on the development of “energy harvesting” circuits capable of transforming RF energy into DC power. STMicroelectronics and ESEO chose Keysight Advanced Design System (ADS) and its co-simulation capabilities to accurately design and simulate the rectifying circuit for the energy harvesting solution. The design team successfully created an energy-harvesting system that transformed ambient 2.45-GHz wireless signals into DC power.

案例分析 2018-08-20

PDF PDF 1.41 MB
Portable RADAR Testing Saves Time on the Assembly Line - Case Study
Automotive radar technology is an indispensable part of the advanced driver-assistance systems (ADAS) that not only adds convenience but helps save lives. ADAS-connected radar modules must be precisely validated on the assembly line to deliver proper operation.

案例分析 2018-07-28

PDF PDF 3.28 MB
5 Tips for Getting the Most out of Your Function Generator - eBook
Today’s function generators can do much more than their predecessors, but many engineers are not aware of these advanced capabilities. This eBook will introduce you to five advanced waveform capabilities that can help improve testing and save you time in the lab.

电子书 2018-07-18

PDF PDF 6.65 MB
DC-DC Converter Testing - Case Study
Manufacturer of automotive DC-DC converters slashes test time by 95 percent.

案例分析 2018-07-17

PDF PDF 4.49 MB
Completing Li-Ion Cell Self-Discharge Testing in Just Two Hour - Case Study
Leading Lithium-Ion cell manufacturer dramatically reduces overall battery test time and improves product quality assurance with innovative self-discharge tests from design to manufacturing.

案例分析 2018-07-04

PDF PDF 3.61 MB
IoT Device Functional Test Solution
Keysight's functional test solution helped a hearing aid manufacturer simplify product testing process, saving test time and reducing costs and risks to result in improved throughput of their new hearing aid with BLE connectivity.

案例分析 2018-06-19

PDF PDF 1.93 MB
Automotive & Energy Solutions - eBook
Automotive electronics is the underlying platform for all operations and diagnostics, convenience and comfort, safety and security, and main support for the three areas of innovation: e-mobility, autonomous driving, connected car.

电子书 2018-06-19

PDF PDF 4.31 MB

以前 1 2 3 4 5 6 7 8 9 10 ... 下一页