Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discutez avec un expert

Support technique

Mesure Electronique

Support by Product Model Number:

Affiner la liste

retirer tout le raffinement

Par industrie/technologie

Par type de contenu

Par catégorie de produit

151-175 sur 1220

Tri:
Redefining 5G New Radio Drive Testing
This white paper describes the key challenges involved in field testing 5G.

Étude de cas 2019-01-31

PDF PDF
University Professor Cuts Lab Setup and Configuration Time by 75 Percent
Pre-lab setup and tracking of all lab instruments can be tedious and time-consuming. See how an EE Professor centralizes control of Keysight and non-Keysight instruments, saving precious time.

Étude de cas 2019-01-31

PDF PDF
Accelerate 5G Testing: 5G Manufacturing Test Considerations
The promise of 5G is faster and more reliable communications. To enable mobile broadband communications, 5G uses existing and new technologies to achieve extreme data throughputs. In this white paper, you will learn about the impact of the 3GPP evolution on your testing and solutions available to help you scale to production quickly.

Étude de cas 2019-01-29

PDF PDF
The Journey of a Signal – Optimize your Signal Analysis Measurements
This paper explains the high-level design of a signal analyzer and how to use that knowledge to avoid mistakes and make optimum measurements.

Étude de cas 2019-01-16

PDF PDF
Redefining Wireless Transceivers to Deliver Groundbreaking 5G Connectivity
Eridan Communications used Keysight circuit design software to create a transceiver module with exceptional system efficiency and signal flexibility.

Étude de cas 2019-01-14

PDF PDF
Analysis of Test Time in Electronics Development Workflows
How test engineers can increase productivity.

Étude de cas 2019-01-07

PDF PDF
Revisiting Mismatch Uncertainty with the Rayleigh Distribution
This paper examines several important aspects of estimating mismatch uncertainty, which is often a major component of the total uncertainty for RF and microwave measurements.

Étude de cas 2019-01-05

PDF PDF
Damaged Connectors Impact the Quality of Measurements
This paper raises awareness of the importance to keep connectors free from damage for optimal measurement performance.

Étude de cas 2019-01-04

PDF PDF
5G Transceiver Manufacturer Cuts Test Time by 20X
Working with Keysight, a leading manufacturer achieved a 20x improvement in test speed, 10x improvement in asset utilization, and easily repurposed their test stations.

Étude de cas 2019-01-03

PDF PDF
The Essential Signal Generator Guide: Building a Solid Foundation in RF – Part 2
Eliminate uncertainties and doubts from your test results with a reliable signal generator. In Part 2, we’ll introduce you to signal generators and basic specification such as modulation, signal purity, and distortion.

Étude de cas 2019-01-03

PDF PDF
Fully-Automatic DMM Calibration System
This paper describes a fully-automatic calibration system for digital multimeters (DMMs), and uncertainty estimation of the DCV measurements of the system.

Étude de cas 2018-12-22

PDF PDF
Specifications Guidelines
Keysight Technologies has definitions for its Test and Measurement product specifications and how they are presented. The following material is extracted from these manufacturing recommendations.

Étude de cas 2018-12-17

PDF PDF
Calibration of Precision Step Attenuators
This paper describes an automated parallel IF substitution system for precision attenuator calibration and presents results of tests made on some very accurate attenuators.

Étude de cas 2018-12-15

PDF PDF
Using a Manufacturer's Specification as a Type B Error Contribution
To better understand the implications of using manufacturers’ specifications in an uncertainty analysis, multiple technical topics are explored.

Étude de cas 2018-12-14

PDF PDF
Car Manufacturer Speeds Ahead with Automotive Ethernet Compliance Solution
Learn how one car maker achieved 100% test coverage for physical layer Rx test, meeting IEEE 802.3bw-2015 standards with Keysight's automotive Ethernet solution.

Étude de cas 2018-12-14

PDF PDF
Calibration of a Ratio Transformer
Describes a calibration technique for decade ratio transformers which is performed by comparison measurement at 1 kHz.

Étude de cas 2018-12-14

PDF PDF
Evaluation of the Performance of a State-of-the-Art Digital Multimeter
The purpose of this paper is to describe some methods to help verify the performance of a very accurate automatically calibrated DMM, the HP 3458A.

Étude de cas 2018-12-14

PDF PDF
ATE System Level Calibration and Its Impact on Cost, Quality and Schedule
This paper proposes an alternative method to provide system level specification and system measurement calibration which will extend the system's ability to be used for multiple products.

Étude de cas 2018-12-14

PDF PDF
Calibration of Time Base Oscillators
As more accurate clocks were produced, new uses of time measurement were explored. As new uses were discovered, the need for even more accurate clocks became apparent.

Étude de cas 2018-12-13

PDF PDF
Successful Deployment of eCall Live Crash Test - Case Study
Car maker successfully emulates over-the-air environments in live crash test for their emergency call in-vehicle systems, with the eCall/ERA-GLONASS conformance test solution from Keysight.

Étude de cas 2018-12-13

PDF PDF 5.10 MB
Too Much Calibration?
This paper explains the variables at work in the world of calibration – how they can be used to find the elusive balance point between cost and confidence, or "too much" and "not enough" calibration.

Étude de cas 2018-12-13

PDF PDF
Successful Deployment of eCall Live Crash Test
Car maker successfully emulates over-the-air environments in live crash test for their emergency call in-vehicle systems, with the eCall/ERA-GLONASS conformance test solution from Keysight.

Étude de cas 2018-12-13

PDF PDF
Assurance of Calibration Results: Applying the Power of Visual Information to Improve Quality
Three success stories show how Keysight ensures the quality of test and calibration results with systematic monitoring of results from our highest-volume instrument calibrations.

Étude de cas 2018-12-12

PDF PDF
Language of Specifications
This paper explains some of the arcane language used in describing a product's characteristics.

Étude de cas 2018-12-12

PDF PDF
Sensitivity Analysis of One-port Characterized Devices in Vector Network Analyzer
This paper shares the results of a study on the use of characterized devices in microwave vector network analyzer (VNA) calibrations and measurements.

Étude de cas 2018-12-12

PDF PDF

Précédente 1 2 3 4 5 6 7 8 9 10 ... Page suivante