Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По Отрасли/Технологии

По типу содержания

По типу оборудования

51-75 из 5743

Упорядочить:
Make Accurate Radar Receiver Measurements - White Paper
In this paper you will review a typical test setup for a radar receiver under test, analyze drift of critical power level accuracy, model the results, and gain insights to reduce risk.

Руководство по применению 2019-11-07

Effective Multi-tap Transformer Measurement using a Scanner and the 4263B LCR Meter
With the progress of recent electronics equipment and digital networks, production amounts are increasing of the transformers which contribute to equipment miniaturization, low power dissipation and higher quality. Therefore, improvement of select estimate efficiency is required at the production line or incoming inspection. Noticed recently, improvement of estimation efficiency is required for pulse transformer which are used in LAN or ISDN digital networks, and for multi-tap transformers with three or more pole taps, such as switching power transformers. This application note shows an effective multi-tap an effective multi-tap transformer measurement using a scanner and the Agilent 4263B LCR Meter.

Руководство по применению 2019-11-06

PDF PDF
Investigate Interference Issues in the Field with RTSA - White Paper
Interference is everywhere — and traditional analysis isn’t reliable. This white paper discusses interference sources, the flaws of traditional analysis, and how RTSA aids interference detection.

Руководство по применению 2019-11-06

PDF PDF 2.77 MB
Effective Multi-tap Transformer Measurement using a Scanner and the 4263B LCR Meter – App Note
This application note shows an effective multi-tap transformer measurement using a scanner and the 4263B LCR Meter.

Руководство по применению 2019-11-05

Improve Electronic Product Quality and Performance with Precision LCR Meters
This note describes the general application of passivecomponent measurements in incoming inspection and R&D andshows the benefits of Keysight's Precision LCR Meter family;the 4284A and the 4285A 30 MHz LCR meter with digital Q capability.

Руководство по применению 2019-11-04

PDF PDF
Keysight Pass/Fail Decision Rules
A decision rule is a “rule that describes how measurement uncertainty is accounted for when stating conformity with a specified requirement.” When you perform a measurement and subsequently compare the result to a specification, making a statement of conformity (for example, in or out of tolerance, or pass / fail), you have two possible outcomes: You make a correct pass / fail decision or you make an incorrect pass / fail decision.

Руководство по применению 2019-11-02

PDF PDF
Keysight Pass/Fail Decision Rules - Application Note
A decision rule is a “rule that describes how measurement uncertainty is accounted for when stating conformity with a specified requirement.” When you perform a measurement and subsequently compare the result to a specification, making a statement of conformity (for example, in or out of tolerance, or pass / fail), you have two possible outcomes: You make a correct pass / fail decision or you make an incorrect pass / fail decision.

Руководство по применению 2019-11-02

PDF PDF 866 KB
Keysight Pass/Fail Decision Rules
Learn how Keysight applies Pass/Fail decision rules to ensure you mitigate risk and select the right calibration service based on recent changes in ISO/IEC 17025 and ILAC-G8.

Руководство по применению 2019-11-02

PDF PDF
Balanced Circuit Measurement with an Impedance Analyzer/LCR Meter/Network Analyzer
This application note describes the difference between a balanced circuit and an unbalanced circuit, and also explains how to make an unbalanced circuit measurement by the unbalanced instrument (impedance Analyzer, LCR meter, network analyzer) step by step. File Size: 500 KB.

Руководство по применению 2019-11-01

PDF PDF
Overcome Forward Error Correction Challenges in 400G Device Designs - White Paper
Test standards for 400G and beyond require FEC in layer1 testing to characterize the system margin and to correct errors in data transmission that otherwise do not run error-free by design.

Руководство по применению 2019-10-31

PDF PDF 2.68 MB
How to Choose Spectrum Emission Mask (SEM) Measurement Settings Accurately
This is the application note for How to Choose Spectrum Emission Mask (SEM) Measurement Settings Accurately in N9085EM0E 5G NR X-Series Measurement Application

Руководство по применению 2019-10-30

PDF PDF
First Steps in 5G: Overcoming New Radio Device Design Challenges Series - Part 4 - White Paper
Over-the-air (OTA) testing is one of the most challenging aspects of 5G device development. In this series, we’ve looked at many aspects of 5G for device designers, including the new 5G NR standard, flexible numerology, millimeter-wave (mmWave) design considerations, MIMO, and beamforming challenges. The combination of these technologies introduces substantial new test challenges that can only be validated with OTA testing.

Руководство по применению 2019-10-30

PDF PDF 2.47 MB
First Steps in 5G: Overcoming New Radio Device Design Challenges Series - Part 3 - White Paper
MIMO (multi-input, multiple-output), beam steering, and beamforming are the most talked about technologies in 5G. They are essential to deliver 100x the data rates and 1000x the capacity goals specified in IMT-2020 vision. MIMO is one of the best ways to improve the capacity and efficiency of a network to meet these demands. For devices, multi-antenna technologies must be supported across multiple frequency bands – from sub-6 GHz to mmWave frequencies – and across many scenarios, including massive IoT connections and extreme data throughput.

Руководство по применению 2019-10-30

PDF PDF 2.98 MB
Infiniium Oscilloscopes with 89600 VSA Software
This application note describes the characteristics, setup, and operation of an Infiniium Series oscilloscope with 89600B vector signal analysis software to provide broadband vector signal analysis.

Руководство по применению 2019-10-28

PDF PDF
Infiniium Oscilloscopes with 89600 VSA Software - Application Note
This application note describes the characteristics, setup, and operation of an Infiniium Series oscilloscope with 89600B vector signal analysis software to provide broadband vector signal analysis.

Руководство по применению 2019-10-28

PDF PDF 4.86 MB
Infiniium OscilloscopesWith 89600 VSA Software
This application note describes the characteristics, setup, and operation of an Infiniium Series oscilloscope with 89600B vector signal analysis software to provide broadband vector signal analysis.

Руководство по применению 2019-10-28

PDF PDF
Discover the Best Oscilloscope - Keysight InfiniiVision vs Tektronix 4 Series - White paper
With so many high-quality oscilloscopes available today, determining which is the best for your testing needs can be difficult. Learn the key differences between the Keysight InfiniiVision oscilloscopes and the Tektronix 4 Series oscilloscopes to discover the right oscilloscope for your bench.

Руководство по применению 2019-10-24

PDF PDF 4.30 MB
Signal Integrity Fundamentals - White Paper
Learn signal integrity fundamentals from simulation to measurement to help you design your high-speed digital devices with higher reliability and lower costs.

Руководство по применению 2019-10-23

PDF PDF 3.28 MB
Numerical Simulation of a Bipolar-Sequence TMA System
Numerical modeling of an 8-element bipolar time-modulated array (BTMA) system composed of microstrip patches and designed for operating at 5-GHz.

Руководство по применению 2019-10-22

PDF PDF
IV and CV Measurement Using the Keysight B1500A MFCMU and SCUU
This eight-page application note illustrates how an accurate IV and CV measurement system can be confugured using the B1500A MFCMU and SCUU.

Руководство по применению 2019-10-22

PDF PDF
Numerical Simulation of a Bipolar-Sequence TMA System
Numerical modeling of an 8-element bipolar time-modulated array (BTMA) system composed of microstrip patches and designed for operating at 5-GHz.

Руководство по применению 2019-10-22

PDF PDF 1.29 MB
Address Phase Compensation Challenge in 5GNR Signal Generation - Application Note
This is the application note for addressing phase compensation challenge in 5G NR.

Руководство по применению 2019-10-22

PDF PDF 2.56 MB
Plug and Play i3070 In-Circuit Tester
Keysight’s i3070 In-Circuit test system supports Industry 4.0 machine to machine communication protocol of IPC-CFX standard, as well as other communication protocols such as MQTT, OPC-UA and Panasonic’s iLNB.

Руководство по применению 2019-10-21

PDF PDF
Address Phase Compensation Challenge in 5GNR Signal Generation
This is the application note for addressing phase compensation challenge in 5G NR.

Руководство по применению 2019-10-21

PDF PDF
Plug and Play i3070 using IPC-CFX - Application Note
Keysight’s i3070 In-Circuit test system supports Industry 4.0 machine to machine communication protocol of IPC-CFX standard, as well as other communication protocols such as MQTT, OPC-UA and Panasonic’s iLNB.

Руководство по применению 2019-10-21

PDF PDF 545 KB

Назад 1 2 3 4 5 6 7 8 9 10 ... Следующие