Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-23 из 23

Упорядочить:
Is there a 3D model of the InfiniiVision DSOX1202A/G and EDUX1052A/G oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2020-03-02

Is there a 3D model of the InfiniiVision DSOX1204A/G oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2020-01-24

Is there a 3D model of the InfiniiVision 1000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2020-01-24

Is there a 3D model of the P9241A USB oscilloscopes?
Yes, see the IGES, Step, and PKG format file downloads.

FAQ 2018-09-21

Is there a 3D model of the InfiniiVision 4000 X-Series oscilloscopes?
Yes, see the IGES, SAP, Step, and PKG format file downloads.

FAQ 2017-05-05

Is there a 3D model of the Infiniium V-Series oscilloscopes?
Yes, see the Step format file downloads.

FAQ 2017-01-25

Is there a 3D model of the InfiniiVision 6000L Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2016-07-18

Is there a 3D model of the InfiniiVision 2000/3000/3000T X-Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2015-02-18

Is there a 3D model of the InfiniiVision 6000 X-Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2014-04-29

Why does handheld scope’s date/time display disappears or shows hexa characters?
This condition indicates that the internal memory battery level is low.

FAQ 2013-11-22

Are the input channels on the U1602A and U1604A Handheld Oscilloscopes isolated?
No, the scope channels 1 and 2 on the U1602A and U1604A Handheld Oscilloscopes are not isolated. They share the same ground.

FAQ 2013-11-17

Why i can't find other languages help file setting in U160X A/B series HH oscilloscope?
In order to access to other language, please go to respective product support page in www.Keysight.com. Go to Driver & Software page, select Firmware Update.

FAQ 2011-09-12

Are the input channels on the U1602B and U1604B Handheld Oscilloscopes isolated?
No, both scope channels (channel 1 and channel 2) on the U1602B and U1604B Handheld Oscilloscopes are not isolated.

FAQ 2011-03-31

When will Keysight USB modular instruments and USB Modular DAQs supports Windows 7?
For 32 bit Windows 7, the supportability of modular instruments and DAQs will happen...

FAQ 2010-07-18

VEE 9.0 has SCPI completion. How do I make my own SCPI command built-in with VEE?
Please refer to the attached Microsoft Word document for a step by step explanation...

FAQ 2009-11-12

I've written my own text format for SCPI in *.txt. How do I use these for SCPI completion within VEE 9.0. What tool should I use?
You can use the tool found within Keysight.com. Just search using the keyword "Keysight VEE SCPI...

FAQ 2009-11-12

Where to find the USB modular scopes IVI-COM programming guide?
download the programming guide.

FAQ 2009-09-29

What is the update rate for U1600A series handheld scope?
update rate is 14 waveforms per second

FAQ 2009-08-06

Why does handheld scope’s DMM measurement frequently stall after one hour of continuous operation?
This condition indicates that the internal memory battery level has dropped to 1.4V or lower.

FAQ 2009-07-16

What type of USB cable do the U1602A and U1604A Handheld Oscilloscopes use?
The U1602A and U1604A Handheld Oscilloscopes use the USB type-A to mini-B cable….

FAQ 2009-05-03

How do I connect my InfiniiVision oscilloscope directly to a PC via the LAN interface?
To establish a point-to-point LAN connection, you will need either a PC with an Auto-MDIX network adapter or a crossover (not straight-through) LAN cable.

FAQ 2009-04-23

Keysight Infiniium Oscilloscopes: What LAN Connectors Are Available?

FAQ 2003-08-01

Keysight Infiniium Oscilloscopes: How Do I Order a Keysight Infiniium Oscilloscope?
54800-Series Infiniium Oscilloscopes

FAQ 2003-08-01