Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-25 из 40

Упорядочить:
Why don’t my Keysight PXI modules show up in National Instruments-Measurement & Automation Explorer (NI-MAX)?
Older versions of Keysight and other vendor’s PXI software could result in Keysight modules not appearing in NI Max....

FAQ 2013-08-30

How do I find a partner to help develop my modular solution?
Keysight has a number of solution partners that can help define and create your modular solution...

FAQ 2010-10-06

Do you have anti-aliasing filter for U2300A and U2500A ?
No, we do not have anti-aliasing filter for our DAQs

FAQ 2010-09-22

How do I locate the serial number for my 34980A Mainframe?
The serial number is located on the rear panel of the 34980A on the left of the LAN and USB connectors.

FAQ 2010-09-15

Where can I get the drivers for the U2300A Series USB Data Acquisition (DAQ) devices?
The drivers for the U2300A Series Data Acquisition (DAQ) devices are available on the Keysight website….

FAQ 2010-09-08

Where can I get the Programming Guide for the U2300A Series USB Data Acquisition (DAQ) devices?
You can download the Programming Guide for the U2300A Series USB Data Acquisition (DAQ) devices from the Product Reference CD….

FAQ 2010-09-08

Why do we see unused port in U2300A/U2500A with similar waveform and frequency but with lower amplitude to its adjacent or close by used port?
It is recommended to ground all the AI connection that is not being used. If you have multiples of AI channels to be used, one good way is to have…

FAQ 2010-08-09

When I sent commands using VISA (Both Keysight VISA and NI VISA), why must i put '\n' or '\r' after the commands for U2600A…
Please upgrade your U2600A firmware to version 1.05 or above

FAQ 2010-08-09

I get error from the example "C:\Program Files\Keysight\RF Switch Driver\Examples\VS.NET\CSharp\Example1".
The temporary solution to this is to load the U2931A .dll file that was not loaded with the...

FAQ 2010-07-18

When will Keysight USB modular instruments and USB Modular DAQs supports Windows 7?
For 32 bit Windows 7, the supportability of modular instruments and DAQs will happen...

FAQ 2010-07-18

What is the clock rate for Digital Inputs(DI) and Digital Outputs(DO) of U23xxA and U25xxA USB Data Acquisition?
The DAQ DIO is not meant to measure DI with clock rate precision or to control frequency of digital output

FAQ 2010-07-18

Can the measurements taken be read from the 34980 Data Acquisition Front Panel?
No

FAQ 2010-05-14

Why USB modular instruments (U272XA, U2741A, U2751A and U2761A) is not detectable by E5813A?
PC is failed to enumerate the USB modular instrument.

FAQ 2010-04-09

Is U2751A compatible with E5813A?
U2751A is not compatible with E5813A.

FAQ 2010-03-22

Is the USB connection of U2300A,U2500A and U2600A optically coupled?
No. It is not.

FAQ 2010-03-22

Is there any special setting that I need to do in Keysight VEE before using the U2300A or U2500A DAQ with it?
Yes. In fact it is the most important thing you need to set before using the DAQ with Keysight VEE. As most instruments uses MSB byte ordering, DAQ...

FAQ 2009-12-15

I've written my own text format for SCPI in *.txt. How do I use these for SCPI completion within VEE 9.0. What tool should I use?
You can use the tool found within Keysight.com. Just search using the keyword "Keysight VEE SCPI...

FAQ 2009-11-12

VEE 9.0 has SCPI completion. How do I make my own SCPI command built-in with VEE?
Please refer to the attached Microsoft Word document for a step by step explanation...

FAQ 2009-11-12

How do I know what is the best sampling rate to use for my measurement?
Typically if you follow Nyquist theory, your sampling rate should be 2x the highest frequency of the incoming signal that you are measuring. However, we recommend that you use 5x...

FAQ 2009-09-29

On the ENA can I use the embedded GPIB Interface to control and perform a power meter calibration?
A Keysight 82357A/B USB/GPIB interface is required.

FAQ 2009-08-16

Where On the Web Can I Find the IO Library for My GPIB Card?
The latest release of the Keysight PC IO Libraries is available at http:///find/iolib

FAQ 2009-02-18

Do terminal blocks and SCSI cables come with the USB data acquisition (DAQ) devices?
No, terminal blocks and SCSI cables do not come with the USB data acquisition (DAQ) devices....

FAQ 2008-09-25

What are some typical applications of the U2300A Series USB Data Acquisition (DAQ) devices?
The U2300A Series USB Modular Data Acquisition (DAQ) devices have a variety of applications such as:….

FAQ 2008-09-25

Do the U2300A USB data acquisition (DAQ) devices have DMA channels?
No. The U2300A Series DAQ devices are USB interface devices therefore, they do not have any DMA channels.

FAQ 2008-09-25

Is the Universal Serial Bus (USB) interface a good choice for data acquisition applications?
The Universal Serial Bus (USB) interface is ideal for data acquisition applications because USB offers plug-and-play capabilities….

FAQ 2008-09-25

1 2 Следующие