Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Industry/Technology

By Type of Content

By Product Category

201-225 of 1160

Sort:
Can we get user defined data in ARB mode?
No, it is the same random pattern as in first-generation N5181A MXG. Real-time custom modulation has user defined data.

FAQ 2012-04-30

Will the MXG and EXG X-Series signal generator work with the signal analyzers for ESC (external source control)?
Yes.

FAQ 2012-04-30

Can you bypass the internal reference chain with clean rubidium source on the X-Series signal generators?
The 10 MHz path is very clean and works with an external reference. The 1-50 MHz tunable path is noisier, see the data sheets for more details.

FAQ 2012-04-30

What does the S/N mode affect negatively on the X-Series signal generators? Why not leave it on all the time?
The harmonics can degrade with S/N mode on.

FAQ 2012-04-30

Can waveforms be written to removable SD card?
Yes, this capability is available through security Option 006.

FAQ 2012-04-30

Does Option UNY, enhanced low phase noise, require Option UNX, low phase noise,on the X-Series signal generators?
No, they are independent options with different levels of phase noise performance above 3 GHz.

FAQ 2012-04-30

Can the user scale the output attenuation in IQ mod for N5182B MXG or N5172B EXG signal generator?
Yes, by using runtime scaling or IQ attenuator.

FAQ 2012-04-30

Can I use custom digital modulation in ARB mode?
Yes, but the data will be a fixed, random pattern.

FAQ 2012-04-30

What is the maximum size user file that can be played real-time on the N5182B MXG or N5172B EXG X-Series signal generator?
For real-time custom modulation, it is 1024 MSa for the MXG and 512 MSa for the EXG. For real-time signal studio applications, it is up to 4 GB. Refer to specific Signal Studio Application for detailed specifications.

FAQ 2012-04-30

Is the phase coherency supported on the X-Series signal generators?
Yes, with Option 012, LO in/out for phase coherency.

FAQ 2012-04-30

Is the tuning speed the same as switching speed on the X-Series signal generators?
Yes, switching speed is the same as tuning speed.

FAQ 2012-04-30

What are the plans to upgrade the N5102A DSIM, if I want it to go to 160 MHz BW on the N5182B MXG or N5172B EXG X-Series signal generators?
DSIM will be able to run up to 200MSa/sec.

FAQ 2012-04-30

Can you master/slave MXG and EXG or must they all be the same model number?
You can master/slave first generation MXG N5182A with the N5182B MXG and N5172B EXG X-Series signal generators. The N5172B or N5182B must be the master.

FAQ 2012-04-30

Will we be able to have more than 2 USB power sensors on the X-Series signal generators?
Yes, we are able to connect to 4.

FAQ 2012-04-30

What is the size and format of the removable memory (SD card) on the X-Series signal generators?
The size of the card has varied over the years, RAW storage. This is only available with Option 006 instrument security and removable memory card.

FAQ 2012-04-30

On the ENA 6 series, can I get TTL signal indicating Pass/Fail of the limit test like the 871x?
Yes.

FAQ 2012-04-17

Do the ENA provide a probe power connection for active probes?

FAQ 2012-04-17

Does the ENA support USB mouse or keyboard?
It depends on the models.

FAQ 2012-04-17

Does the ENA 6 series support mixer measurements like the 871x?
No.

FAQ 2012-04-17

On the ENA 6 series, is the User Defined BEGIN key available like the 871x?
The "Load & Run" of the E5061A/62A and E5061B are equivalent to the User Defined BEGIN key.

FAQ 2012-04-17

Is it possible to generate touchstone files on the ENA?

FAQ 2012-04-17

Does the ENA allow user access to the Error Coefficient Arrays?

FAQ 2012-04-17

Does the ENA 6 series support barcode reader?
No.

FAQ 2012-04-17

Why is a negative D value sometimes displayed when a furnished PTFE plate is measured with the 16453A?
When resistance value of Short compensation data is too large, measured D value is overcompensated for the Short resistance and results in a negative value

FAQ 2012-04-08

Using the E8267D PSG Vector Signal Generator in a System
Browse through this index of resources generated to ease your test system design challenge

FAQ 2012-03-30

Previous 1 2 3 4 5 6 7 8 9 10 ... Next