Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Industry/Technology

By Type of Content

By Product Category

176-200 of 1160

Sort:
Can the E4406A or PSA Series cdmaOne personality (Option BAC) make power timing and phase measurements?
Yes. In the cdmaOne personality you will first need to change the Measure Method to Timing and Phase under the Measure Setup key and then change the view to Power Timing and Phase under the View/Trace key.

FAQ 2012-05-29

What file formats does the 89601A VSA software support for signal waveforms?
Recorded data from the following files can be interpreted by the 89600: ASCII (.txt and .csv), Binary (89600 SDF .sdf, .dat), Binary (E3238 .cap), Binary (N5510A .bin), MATLAB 7 (or earlier, .mat)

FAQ 2012-05-28

Do the E4406A, PSA Series and 89600 VSA Software report Peak Code Domain Error for W-CDMA and cdma2000?
Yes. The screen capture below shows a W-CDMA Modulation Accuracy measurement on the E4406A and PSA Series, and Peak Code Domain Error is reported in the results table.

FAQ 2012-05-26

Do the E4406A and PSA Series support Complementary Cumulative Distribution Function (CCDF) measurement for cdmaOne?
Yes. The Power Statistics CCDF measurement is not in the cdmaOne personality (Option BAC), but it does come standard in the Basic measurement personality for E4406A and in the Spectrum Analysis mode for PSA and can be used to measure cdmaOne sign...

FAQ 2012-05-26

Which Application Notes are Most Relevant to the PSA Series Spectrum Analyzer?
This page contains links to application notes that are relevant to PSA Series spectrum analyzers.

FAQ 2012-05-11

Why do I get a Meas Uncal message when I select either the Quasi-Peak or EMI Average detector for taking a full band sweep with the MXE EMI Receiver?
Sweeptime has reached its maximum. See complete FAQ for further details...

FAQ 2012-05-10

How do I make the signal list compare measurements made with the detectors used to different limit lines in my MXE EMI Receiver?
Meas Setup, Detectors (Measure)...

FAQ 2012-05-10

How do a take a sweep with both the Quasi-Peak and EMI Average detector at the same time with an MXE EMI Receiver?
Switch to EMI Receiver mode...

FAQ 2012-05-10

Can I use the 16092A with the 4395A/4396B/4287A/E4991A?
Yes, you can use the 16092A with the 4395A/4396B/4287A/E4991A.

FAQ 2012-05-10

What is required to use Remote UI for the E4991A?
You need to prepare the following items: the E4991A, a PC, the E4991A VBA software (E4991A_vba.msi) included in the furnished CD-ROM and, LAN environment. For details, please refer to chapter 10 "Using LAN" of the E4991A operation manual.

FAQ 2012-05-10

How do you clear the M9045A, M9045B, M9047A and M9048A memory?
Please refer to the link below for the procedure on how to clear the memory for the M9045B and M9048A adapters.

FAQ 2012-05-01

Is the pulse generator specification still the same with ALC On/Off on the X-Series signal generators?
Yes, it still cuts off at <2µs, however, open loop power accuracy has improved with or without power search being run. In most cases, you will see tenths of dB accuracy without running power search. This is a significant improvement over first-generation MXG.

FAQ 2012-04-30

Is the tuning speed the same as switching speed on the X-Series signal generators?
Yes, switching speed is the same as tuning speed.

FAQ 2012-04-30

Can I use custom digital modulation in ARB mode?
Yes, but the data will be a fixed, random pattern.

FAQ 2012-04-30

Can you bypass the internal reference chain with clean rubidium source on the X-Series signal generators?
The 10 MHz path is very clean and works with an external reference. The 1-50 MHz tunable path is noisier, see the data sheets for more details.

FAQ 2012-04-30

Can we upgrade N5181A or N5182A first-generation MXG to an N5181B or N5181B MXG X-Series signal generator?
No, there is not a hardware upgrade path from the first-generation MXG to MXG X-Series signal generator.

FAQ 2012-04-30

What is the maximum size user file that can be played real-time on the N5182B MXG or N5172B EXG X-Series signal generator?
For real-time custom modulation, it is 1024 MSa for the MXG and 512 MSa for the EXG. For real-time signal studio applications, it is up to 4 GB. Refer to specific Signal Studio Application for detailed specifications.

FAQ 2012-04-30

Can we support atmospheric conditions with N7609B GPS on the N5182B MXG or N5172B EXG X-Series signal generators?
Yes.

FAQ 2012-04-30

Does N5181B or N5182B MXG Option UNY/UNX have backward code compatibility with E8663D or 8663D signal generators?
Yes, the N5181B and N5182B MXG Option UNY/UNX has the same SCPI as PSG E8663D. E8663D is the replacement of 8663D with BWCC (backward code compatibility).

FAQ 2012-04-30

Do the new sources de-crypt waveforms in the same way as the legacy sources? Can we just use pre-existing waveforms?
Yes. First-generation MXG N5182A Signal Studio N76xxB waveforms will play in new sources. Exception will be N7613A Signal Studio for Fixed WiMAX which has the legacy N76xxA structure.

FAQ 2012-04-30

What are the plans to upgrade the N5102A DSIM, if I want it to go to 160 MHz BW on the N5182B MXG or N5172B EXG X-Series signal generators?
DSIM will be able to run up to 200MSa/sec.

FAQ 2012-04-30

Can we get user defined data in ARB mode?
No, it is the same random pattern as in first-generation N5181A MXG. Real-time custom modulation has user defined data.

FAQ 2012-04-30

What does the S/N mode affect negatively on the X-Series signal generators? Why not leave it on all the time?
The harmonics can degrade with S/N mode on.

FAQ 2012-04-30

Is the phase coherency supported on the X-Series signal generators?
Yes, with Option 012, LO in/out for phase coherency.

FAQ 2012-04-30

Will we be able to have more than 2 USB power sensors on the X-Series signal generators?
Yes, we are able to connect to 4.

FAQ 2012-04-30

Previous 1 2 3 4 5 6 7 8 9 10 ... Next