Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Industry/Technology

By Type of Content

By Product Category

1-25 of 1160

Sort:
FieldFox Manuals, Firmware, Software and Product Support
Manuals, firmware upgrade, software trials & upgrade and support page for FieldFox analyzers

FAQ 2018-11-14

Where can I find the user documentation for the U5340A FPGA Development Kit (FDK)?
The user documentation is installed on your computer with the software.

FAQ 2018-01-18

Can the B01 bundle for the M9703B digitizer support 1 GHz of bandwidth?
No, the AXIe carrier board in the B01 bundle contains different assemblies than the standard M9703B board. Click on the link for additional information.

FAQ 2017-08-01

Does M9393A work without M9300? If so, when using the M9393A with 100MHz reference on a pulse generator, what is the external reference input voltage?
When replacing the M9300 with a pulse generator, self-test and alignments may pass. Click on the question for additional information.

FAQ 2017-06-28

Is Option RTS a license key or hardware upgrade?
Option RTS is a hardware and license key upgrade. Therefore, this upgrade requires the analyzer to be returned to Keysight.

FAQ 2017-06-28

How do I display the mixer conversion loss of M1970 Series or M1971 Series Harmonic Mixer on an X-Series Signal Analyzer?
There is no way to display the conversion loss values from these mixers on screen. There is a hard copy of the conversion loss data supplied with each mixer that can be referenced.

FAQ 2017-06-28

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2017-06-28

Is it possible to develop specific macros for E5061B to support TRL cal or the unknown thru method under a 9-term calibration method?
Yes, it is possible to perform a user developed 8-term calibration, like TRL, using an external program for the E5061B. Click on the question for additional information.

FAQ 2017-06-28

If we use external clocks for both the Pattern Generator and Error Detector parts, can we run them at different data rates?
It would be more straight-forward to provide the PG (TX) with a 10 GHz clock (for 10 Gb/s data) and then use the 1:4 demux and provide the ED (RX) with a 2.5 GHz clock (measuring 2.5 Gb/s data). Click on the question for additional information.

FAQ 2017-06-28

Is there a PDF version available of the user guide for the M9210A? There are issues with the .chm file that is available.
No, there is not a PDF version available for the M9210A user manual. To read the .chm file, it must be downloaded and copied on the local C drive before opening.

FAQ 2017-06-28

For signals requiring wider bandwidth, how can Keysight’s LTE Signal Studio waveform creation products be used to increase carrier spacing?
Set the FFT length to 8192 and a sample rate of 800 MHz. Subcarrier spacing = sampleRate/FFT size

FAQ 2017-06-28

How do I create a Mono FM Signal using N5182B MXG ARB?
You can configure N7611B Signal Studio Broadcast Radio to play a mono/FM signal.

FAQ 2017-06-28

Can a CalPod system be used with the N1500A software?
No, the CalPod and N1500A Software are not compatible.

FAQ 2017-06-28

What is the time out limit of response time (2.4) in M8020A Interactive link training?
The LTSSM (Link Training and Status State Machine) implements the timeouts as specified in the PCIe specification. Click on the question for additional information.

FAQ 2017-06-28

Does the noise figure application on the PNA-X (option 029) provide a full noise-parameter system (tuners and software)?
No, we don’t provide a full noise-parameter system. Click on the question for additional information.

FAQ 2017-06-28

I am using an electronic load to draw current into my DUT, but when I draw current the voltage drops. Why is this happening?
A voltage drop will appear across this impedance as current flows through it in accordance with Ohm’s Law. Click on the question for additional information.

FAQ 2017-06-28

What is the raw jitter tolerance for the N4960A/N4952A?
There is no CDR in the N4960A, so by itself, the JTOL plot will be a flat line somewhere below 1 UI. An external CDR can be used. Click on the question for additional information.

FAQ 2017-06-28

Does the Maury Microwave MT7553B03 50 GHz Noise Receiver Module lower the effective noise figure of the N5245A beyond that of option 029?
Yes, the NF of the 50 GHz PNA-X is about 10 dB for most of its range while the typical NF from the MT7553B03 is 6 dB.

FAQ 2017-06-28

Can I use multiple M9485A with one controller?
Yes, but there are some limitations. Please refer to below.

FAQ 2017-05-25

What is the difference of software options between M9485A and PNA/ENA series VNA?
There is no difference for option 007/009/010. There are some differences for options 025, 028, 086 and 551.

FAQ 2017-05-25

Which power meter is recommended for system power calibration?
U2000 Series USB Average Power Sensors or U8480 Series USB Thermocouple Power Sensors are recommended.

FAQ 2017-05-25

Is There a GPS Receiver for FieldFox?
GPS capability has been added to FieldFox starting from firmware revision A.05.33.

FAQ 2017-01-23

34972A with USB data logging may eventually freeze. How to prevent?
Yes, experience has shown that using a powered USB 2.0 Hub between the 34972A and the PC usually eliminates the problem.Using LAN instead of USB is the recommended solution if possible.

FAQ 2016-10-26

In N7625B, how many instances of carriers and carrier aggregations do the software support?
One connected signal generator can support one instance of Carrier Aggregation mode. One instance of Carrier Aggregation can support 5 component carriers.

FAQ 2016-07-08

Why isn’t the unit being discovered by VSA software hosted inside the instrument itself?
Check to see if Keysight Technologies is returned from the analyzer as part of the *IDN query.

FAQ 2016-07-08

1 2 3 4 5 6 7 8 9 10 ... Next