Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-25 из 146

Упорядочить:
34972A with USB data logging may eventually freeze. How to prevent?
Yes, experience has shown that using a powered USB 2.0 Hub between the 34972A and the PC usually eliminates the problem.Using LAN instead of USB is the recommended solution if possible.

FAQ 2016-10-26

Where can I find manuals for discontinued and obsolete Hewlett-Packard, Agilent and Keysight test equipment?
Most Keysight products have PDF manuals that can be found on product pages. Other vendors also supply old manuals.

FAQ 2014-08-01

What type of internal memory is installed into the 34972A LXI Data Acquisition Switch Unit?
The Keysight 34972A LXI Data Acquisition Switch Unit utilizes Windows CE...

FAQ 2014-04-07

How do you clear the 34980A multifunction switch/measure mainframe and modules, L44xxA series LXI switch and control instruments memories?
Please refer to the documents for a comprehensive listing of memory installed into these products.

FAQ 2014-04-07

How can previously created data in BenchLink II be exported?
Open a previously saved configuration file with data and then export the data as a Text (.txt) file or Comma Separated values (.csv) file.

FAQ 2012-11-05

The Keysight 8761B SPDT Coaxial Switches are not listed in the "Keysight 34945A, L4445A and L4490A/L4491A Configuration Guide". Why?
Due to the 8761B’s internal design the RF path selection is achieved via DC polarity reversal across the coil control terminals. The Keysight 34945A, L4445A and L4490A/L4491A Control Units do not provide a polarity reversal mode. Thus the 8761B cannot be controlled by the 34945A, L4445A and L4490A/L4491A Control Units.

FAQ 2012-01-16

Why does BenchLink DataLogger 3 generate the "MDAC installation failed" error message?
The MDAC (Microsoft Data Access Components) may be corrupted and needs to be repaired.

FAQ 2011-12-20

How do you clear the M91xxA memory?

FAQ 2011-06-22

Is it normal to not be able to set sample point in AMM for U2300A/2500A?
Yes. AMM assigns the sample point automatically.

FAQ 2010-12-20

Must we need 2 units of SCSI cable connected in between U2802A and U2355/56A?
Yes.

FAQ 2010-12-20

How do I rack mount two instruments of different depths?
There are three ways to rack instruments of different depths side-by-side; for example, a Keysight 33220A with a Keysight 34401A.

FAQ 2010-10-12

How can I input 28V digital signal to U2651A/U2652A when it support digital input voltage < 24V?
You can connect a voltage divider in front of the digital input to reduce the voltage to <24V

FAQ 2010-10-07

What is the compatibility between PXIe chassis and Keysight new PXI/PXIe modules?
Keysight modules come in several varieties, so inspection is required to determine compatibility...

FAQ 2010-10-06

Can I use SCPI to communicate with my Keysight modules?
No. Connectivity is provided through Drivers.

FAQ 2010-10-06

Can I replace other vendors' module (for example a digitizer) with a Keysight one?
There are two aspects to consider...

FAQ 2010-10-06

Will ExpressVIs work with Keysight hardware?
No. Keysight has VIs available to use with LabView but not ExpressVIs.

FAQ 2010-10-06

Are all PXIe system modules/controllers compatible with all chassis?
No, the PXIe standard requires the chassis support certain configurations but not all...

FAQ 2010-10-06

Can I use the PXIe products over LAN?
If the PXIe chassis has an embedded controller with a LAN port then the PXI system can connect to a LAN port...

FAQ 2010-10-06

Can I use PXI-1 existing cards in the Keysight Card cages and are there any that will no longer work?
Older PXI (PXI-1) modules (which have a J2 present) will not work in Keysight 18-slot PXIe chassis...

FAQ 2010-10-06

Can I run a program that is controlling my PXI instrument while using its soft front panel (SFP)?
Not at this time...

FAQ 2010-10-06

Where can customers find user manuals and example programs for AXIe & PXIe products?
Datasheets of modular products will be included on the CD shipped with every product and will be available on Keysight.com from the product page...

FAQ 2010-10-06

Does Keysight have mass interconnect solutions?
There are mass interconnect solutions from MAC panel....

FAQ 2010-10-06

What is the difference between PXIe and AXIe?
The AXIe standard provides the maximum scalability to address a range of platforms...

FAQ 2010-10-06

How to monitor and scan on alarm with the 34980A?

FAQ 2010-10-04

IO Libraries Suite: Is it possible to have both an NI GPIB card and a Keysight GPIB card or converter working in the same system?
Yes, it is possible with many version’s of Keysight IO Libraries.

FAQ 2010-09-08

1 2 3 4 5 6 Следующие