Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 35

Sort:
How many capacitance measurement units (MFCMUs) can be installed in the B1500A?
Only one MFCMU can be installed in a B1500A mainframe.

FAQ 2012-06-07

How can I make a list sweep measurement?
Click the above link for details.

FAQ 2011-05-31

I can't make a correct measurement with N1294A Banana-Triax Adaptor.
Click the above link for details.

FAQ 2011-05-31

How can I enable the low current measurement?
Click the above link for details.

FAQ 2011-05-26

What is the interlock feature of the Keysight B2901/02/11/12A?
Click the above link for details.

FAQ 2011-05-26

How do I get measurement data into a spreadsheet from Keysight B2901/02/11/12A?
You can save measurement data to USB flash memory device as CSV files on File Selection dialog box.

FAQ 2011-05-26

How can I make a single point measurement?
Click the above link for details.

FAQ 2011-05-26

The Keysight B2901/02/11/12A shows the message "Interlock terminal is open" and don't accept to input voltage more than 42 V.
Click the above link for details.

FAQ 2011-05-26

What are the differences among B2901A, B2902A, B2911A and B2912A?
The differences are summarized in the data sheet of the B2901/02/11/12A.

FAQ 2011-05-26

How can I find the sensing type of the channels?
If the sensing type of the channel is set to 4-WIRE, you can see the status indicator on GUI.

FAQ 2011-05-26

How can I make a sweep measurement using 2 channels?
Click the above link for details.

FAQ 2011-05-26

How can I make a pulsed sweep measurement?
Click the above link for details.

FAQ 2011-05-26

How do I find my Keysight B2901/02/11/12A firmware revision?
You can find the firmware revision on the Revision dialog box.

FAQ 2011-05-26

How can I enable the resistance measurement?
Click the above link for details.

FAQ 2011-05-26

Is it possible to append the data to the previous one in Graph View?
No

FAQ 2011-05-26

How can I make a pulsed single point measurement?
Click the above link for details.

FAQ 2011-05-26

How can I make a sweep measurement?
Click the above link for details.

FAQ 2011-05-26

How can I make a sampling measurement?
Click the above link for details.

FAQ 2011-05-26

How can I get a Keysight B2901/02/11/12A screen display into text editor or presentation software?
You can save screen images to USB flash memory device as JPEG files by pressing Graph Dump Assist key in Graph View and Roll View.

FAQ 2011-05-26

How can I save or load the measurement setups?
Click the above link for details.

FAQ 2011-05-26

How can I make a resistance measurement?
Click the above link for details.

FAQ 2011-05-26

How can I find the low terminal state of the channels?
If the low terminal state of the channel is set to FLOATING, you can see the status indicator on GUI.

FAQ 2011-05-25

Can I output 3A each on two channels?
No, you cannot. The maximum current is limited and the limitation is shown on the datasheet.

FAQ 2011-05-18

Can I output the 210V and 3A at the same time?
No, you cannot. The maximum current is limited by the voltage range. The details are shown in the data sheet.

FAQ 2011-05-18

How many steps can I store into the program memory?
The program memory of B2900A is 100k bytes and typically 2500 lines can be stored into the memory.

FAQ 2011-05-18

1 2 Next