这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-25 / 38

排序:
How can I source a pulsed signal on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-09-16

我可以在哪里找到是德科技、安捷伦和惠普的已停产测试与测量设备手册?
是德科技的大部分产品页面都能提供 PDF 版本手册。另外,其他厂商也可能提供旧版手册。

FAQ 2013-05-29

66xxA, E363xA and E364xA: Ca Keysight Power Supplies Sink Current?
Yes! Sinking, or down-programming, is the ability to pull current into the positive terminal of a power supply.

FAQ 2013-01-22

当我计划在N6705A直流功率分析仪中使用N6751A、N6752A和N6754A高性能直流电源模块时,我需要订购这些模块的选件054(高速测试扩展)吗?
当在直流功率分析仪中使用直流电源模块时不需要选件054。

FAQ 2011-06-22

N6751A和N6752A模块上的LGA选件可提供什么功能?
强烈推荐在N6751A/52A模块上安装LGA选件。LGA选件支持大型门阵列。

FAQ 2011-06-22

What does the check mark at the rear panel label of the E3600 series bench power supply mean?
The check mark on the rear panel label shows the AC power rating for this unit which shipped from the factory.

FAQ 2010-09-20

How do you change the programming language expected by the the 6030A, 6031A, 6032A, 6033A, 6035A, or 6038A power supplies?
These products are shipped from the factory in their native language (called Compatible Language Mode) with their hardware address set to "Adr 5". The programming language can only be changed to SCPI Mode via a controller by sending the string "SY...

FAQ 2010-09-09

How can you change or view the secondary address in the 6030A, 6031A, 6032A, 6033A, 6035A, or 6038A power supplies?
These products have been retrofitted with SCPI language capability, in addition to the original or compatibility mode. Secondary addressing of these products is only available in SCPI mode.

FAQ 2010-09-08

E363xA and E364xA: Disabling the Control Knob
To disable the front-panel control knob, scroll the flashing digit on the front-panel display to the right or left using the selection keys (<) or (>) until the flashing digit disappears. Notice that the control knob and all front-panel keys are n...

FAQ 2010-09-08

How can I eliminate the flashing single digit in the front-panel display?
The flashing digit indicates the digit of the output parameter displayed that can be changed by turning the front panel knob. Use the resolution key (<) or (>) to move the flashing digit to the left or right until the flashing stops.

FAQ 2010-09-08

66xxA and E36xxA: Determining Power Supply Constant Current Mode
The power supply cannot be "put" into the constant current mode.

FAQ 2010-08-27

What are the differences between the Keysight N6705A DC Power Analyzer and the N6705B DC Power Analyzer?
The N6705B mainframe has new labeling that identifies which knobs have secondary functions when you press them...

FAQ 2010-08-09

When will Keysight USB modular instruments and USB Modular DAQs supports Windows 7?
For 32 bit Windows 7, the supportability of modular instruments and DAQs will happen...

FAQ 2010-07-18

66000A: Setting Dwell Time
The List mode can contain up to 20 Voltage, Current or Dwell steps if controlled over the GPIB, or up to 8 steps if controlled from the optional keyboard...

FAQ 2010-05-26

How can I clear the content of power supply memory for programmable E36xxA power supplies?
There is no way to clear the contents of the store/recall states. They can be overwritten as many times as desired but there is not an explicit way to delete saved states.

FAQ 2010-05-16

Why USB modular instruments (U272XA, U2741A, U2751A and U2761A) is not detectable by E5813A?
PC is failed to enumerate the USB modular instrument.

FAQ 2010-04-09

Is U2722A compatible with E5813A?
No

FAQ 2010-03-22

Is U2723A compatible with E5813A?
No

FAQ 2010-03-22

What is the voltage and current limit setting for U8001A and U8002A upon powered up?
Same as the setting before power cycle.

FAQ 2010-02-01

How can I make U8001A or U8002A to be in Output On stage upon powered up?
Order option AUT.

FAQ 2010-02-01

Does the Keysight Measurement Manager (AMM) support regional language settings other than English (US)?
Yes, the Keysight Measurement Manager (AMM) supports regional language settings other than English (US)….

FAQ 2009-01-12

How do I adjust the voltage or current settings when the Output is disabled on a Keysight E36xxA-Series power supply?
When the Output is disabled, press the 'Display Limit' button on the front panel to place the power supply in the limit mode. Then, set the limit values for the output voltage and current. Press the 'Output Off' button again to enable the power su...

FAQ 2008-09-23

66xxA, E362xA, E363xA, E364xA: DC Power Supplies Connecting in Series or in Parallel
The resultant voltage for series connections cannot exceed the maximum floating voltage allowed for any on the component power supplies. While this is typically +/-240 volts dc, there are some supplies as low as +/-25 volts dc, and others as high ...

FAQ 2008-09-22

What types of output connections are allowed?
The Keysight E364xA offers new versatile binding posts on the front panel and screw type terminals on the rear panel.

FAQ 2008-09-22

E364xA: Bench vs. System Applications
These power supplies have all the features and performance necessary for both benchtop and system ATE applications where throughput is not critical, at a surprisingly low price.

FAQ 2008-09-22

1 2 下一页