検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

絞込み

絞込みのリセット

トピック

業種/テクノロジー

コンテンツのタイプ

製品カテゴリ

1-25 / 330

並べ替え
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2020-05-22

What software and options do I need to access the FPGA sandbox in my high-speed digitizer?
Digitizer option FDK enables programming access to the on-board FPGA. Click on the question for additional information.

FAQ 2020-02-06

What is the CPU / Storage / Windows OS history?
The history of CPU type/memory size, storage type/size, windows OS is listed in the table.

FAQ 2018-08-21

Xシリーズ モジュール計測器用のXシリーズ測定アプリケーションの30日間無料試用ライセンス
Xシリーズ モジュラー・シグナル・アナライザ用Xシリーズ 測定アプリケーションの30日間無料試用ライセンス。

FAQ 2018-07-25

ベンチトップ/モジュラー/ハンドヘルドモデルのシグナル・アナライザ/スペクトラム・アナライザのファームウェア・アップデート・センター
ベンチトップ/モジュラー/ハンドヘルドモデルのシグナル/スペクトラム・アナライザのファームウェア/ソフトウェアの最新バージョンを利用するために。

FAQ 2018-05-17

Can antivirus programs run on the Windows based PNA-X?
Yes, antivirus programs can run on any Windows based machine.

FAQ 2017-06-28

Can the PNA-X be configured to install Windows updates as they are pushed out by Microsoft?
Yes, any Windows based machine can be configured to install Windows updates.

FAQ 2017-06-28

Is there a software application for the E5062A to calculate K factor?
No, there is not a software application to calculate K factor for the E5062A.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

Does the noise figure application on the PNA-X (option 029) provide a full noise-parameter system (tuners and software)?
No, we don’t provide a full noise-parameter system. Click on the question for additional information.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

Is there a software application for the 8714ES to calculate K factor?
No, there is not a software application to calculate K factor for the 8714ES.

FAQ 2017-06-28

Is calibration included in the 86100DU-WN7 Windows 7 upgrade?
86100DU-WN7 is a return to service center upgrade and does include calibration, in addition to a certificate of calibration and data.

FAQ 2017-06-28

What is the difference of software options between M9485A and PNA/ENA series VNA?
There is no difference for option 007/009/010. There are some differences for options 025, 028, 086 and 551.

FAQ 2017-05-25

M8000シリーズの30日間の無料試用ライセンス
M8000製品シリーズのすべての試用ライセンスへのリンクおよび概要

FAQ 2017-01-30

【VSA】【SG】RF信号をキャプチャして信号源で再生することはできますか?
はい。ベクトル・シグナル・アナライザを使用することで、RFキャプチャ信号を信号源から再生することが可能です。

FAQ 2016-02-03

How to enable 34410A/34411A/L4411A browser web control work in Java 8?
To enable browser web control to work in Java 8, update instrument to firmware version 2.41...

FAQ 2015-09-21

Why 34405A can't be detected in Windows 7?
There are two posibilities causing 34405A couldn't be detected. 1. IO Libraries Suit 15.1 or below...

FAQ 2015-09-21

Microsoft社によるWindows XPのサポート終了は、ENAにどのような影響を及ぼしますか?
Microsoft社は、2014年4月8日にWindows XPオペレーティング・システムのサポートを終了しました。このドキュメントは、いくつかの重大な疑問に答えます。

FAQ 2015-07-27

Can I recover the E7515A operating system if it fails to start correctly?
Yes, E7515A has an Instrument Image Recovery mode. Click on the question above for a fuller description.

FAQ 2015-05-15

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

How does the Microsoft end of support for Windows XP affect my M9036A?
In Keysight’s ongoing efforts and commitment to provide the best possible product quality and improve the overall customer experience with our M9036A PXIe Embedded Controller, we would like to inform you that we have made the conscious decision to not migrate the XP version of the M9036A to Windows 7.

FAQ 2014-10-12

M9290A CXA-m PXIeシグナル・アナライザは、スペクトラム解析用の掃引モードをサポートしていますか?
はい。M9290Aは、スペクトラム解析用の掃引モードとFFTモードをサポートしています。

FAQ 2014-09-11

Xシリーズ・シグナル・アナライザ・ソフトウェア・アップデート
ソフトウェア・アップデート、Xシリーズ・シグナル・アナライザ(PXA/MXA/EXA/CXA/MXE)

FAQ 2014-08-14

従来のUIを備えたX-シリーズ シグナル・アナライザ用X-シリーズ 測定アプリケーションの30日間無料試用版
X-シリーズ シグナル・アナライザ用X-シリーズ 測定アプリケーションの30日間無料試用ライセンス。

FAQ 2014-08-01

1 2 3 4 5 6 7 8 9 10 ... 次へ