您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

126-150 / 320

排序:
Does Keysight EEsof EDA support Linux?
Yes, some Keysight EDA products are supported on the Linux platform.

FAQ 2010-05-11

我可否將 Windows® XP 邏輯分析儀應用軟體升級至 Service Pack 3?
可以,請使用 3.80.0002 版或更新版本的是德邏輯分析儀應用軟體。

FAQ 2010-05-11

What is the meaning of this statement from the data sheet: "The acoustic noise is louder than typical Keysight equipment."
The instrument has a set of fans to remove internally generated heat. These fans generate ...

FAQ 2010-05-07

N5532A 感測器模組的頻率範圍為何?
100 kHz 至 4.2 GHz、10 MHz 至 18 GHz、30 MHz 至 26.5 GHz,與 30 MHz 至 50 GHz。

FAQ 2010-04-13

Why my N8300A will shut down when I select restart?
The application at N8300A must be close before you restart.

FAQ 2010-03-24

Is 432A compatible with Keysight Intuilink software?
432A is not compatible with Keysight Intuilink software.

FAQ 2010-03-22

Is N8262A compatible with Keysight Intuilink software?
N8262A is not compatible with Keysight Intuilink software.

FAQ 2010-03-22

Is N1911A compatible with Keysight Intuilink software?
N1911A is not compatible with Keysight Intuilink software.

FAQ 2010-03-22

Is N1912A compatible with Keysight Intuilink software?
N1912A is not compatible with Keysight Intuilink software.

FAQ 2010-03-22

我可否將 Windows® XP 邏輯分析儀應用軟體升級至 Windows Vista?
不可以,是德邏輯分析儀應用軟體僅在用於主機電腦作為離線播放程式時,才受 Windows Vista 支援。

FAQ 2010-01-25

For Xilinx FPGA Dynamic Probe, when should I use Xilinx Core Generator instead of Core Inserter?
Core Generator is usually preferable if you need partitions, since Core Inserter does not support partitions. Core Generator does support partitions but is much less convenient.

FAQ 2010-01-24

Can we control N9320B with N9320A PC software?
No, N9320A PC software cannot be used to control N9320B spectrum analyzer. Free N9320B PC software is available for download.

FAQ 2009-12-16

Is VEE able to interpret "," as decimal point in Formula box running under German Windows?
No. Please use "." as decimal point as per international standard.

FAQ 2009-11-17

Why did VEE displayed an "out of memory" message even the PC has more than 1GB of memory free after using up only 300MB of memory?
Keysight VEE's could not support such a large memory of usage in a single object or interface.

FAQ 2009-11-08

Why do I not see all the data points on my graph tab?
When viewing your readings from the Graph Tab, some times not all of your data is displayed.

FAQ 2009-11-05

Does E5805A or E5813A driver supports Linux operating systems?
No, E5805A or E5813A does not support Linux operating systems

FAQ 2009-10-20

How do I avoid getting "The memory could not be "read"" error upon closing the software?
It’s most likely this issue is caused by a bad memory...

FAQ 2009-08-19

How to speed up my computer processing time while running the BenchLink DataLogger software continuously for a long period of time?
Do not leave the Quick Graph tab active in the BenchLink DataLogger...

FAQ 2009-08-19

How do I avoid getting “Out of memory” exception errors when using the BenchLink DataLogger software?
Do not leave the Quick Graph tab active in the BenchLink DataLogger...

FAQ 2009-08-19

本系列各種是德邏輯分析儀主機支援那些模組?
請參閱 Keysight 16900、16700 和 16500 主機/模組相容性矩陣

FAQ 2009-08-17

Can I use the Quick Print button to quickly save my waveforms into the USB thumbdrive?
Yes, but with software version 5.10 and above you have to enable the feature...

FAQ 2009-08-17

Is U2300A and U2500A series DAQ supported in Linux environment?
No. U2300A and U2500A are not supportable in Linux environment.

FAQ 2009-08-06

Does U8903A unit contain a hard disk?
No. The U8903A is using flash memory as storage.

FAQ 2009-07-16

Does N9320B support Intuilink?
No, N9320B doesn’t support Intuilink. It does supports Benchvue software and BSA PC software.

FAQ 2009-07-13

Does the Measurement Manager (AMM) run on Window Vista operating system?
Yes. The Measurement Manager (AMM) rev. 1.8.3.0 and above will able to run on Windows Vista ...

FAQ 2009-06-10

上一個 1 2 3 4 5 6 7 8 9 10 ... 下一頁