이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

상세 분류

상세분류 제거

주제별

산업/기술

분야별 검색결과

제품 카테고리별

1-25 / 320

정렬방식:
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2019-08-28

신호 및 스펙트럼 분석기 벤치탑/모듈러/핸드형 펌웨어 업데이트 센터
벤치탑 및 핸드형 모델의 신호 및 스펙트럼 분석기용 펌웨어 또는 소프트웨어 최신 버전 액세스.

FAQ 2019-07-11

How do I update my X-Series Signal Analyzer Benchtop Software
Software updates for the X-Series Signal Analyzers Benchtop (PXA/MXA/EXA/CXA/MXE/ PXE)

FAQ 2019-05-14

FieldFox Manuals, Firmware, Software and Product Support
Manuals, firmware upgrade, software trials & upgrade and support page for FieldFox analyzers

FAQ 2018-11-14

What software and options do I need to access the FPGA sandbox in my high-speed digitizer?
Digitizer option FDK enables programming access to the on-board FPGA. Click on the question for additional information.

FAQ 2018-01-18

Is there a software application for the 8714ES to calculate K factor?
No, there is not a software application to calculate K factor for the 8714ES.

FAQ 2017-06-28

Is there a software application for the E5062A to calculate K factor?
No, there is not a software application to calculate K factor for the E5062A.

FAQ 2017-06-28

Can antivirus programs run on the Windows based PNA-X?
Yes, antivirus programs can run on any Windows based machine.

FAQ 2017-06-28

Can the PNA-X be configured to install Windows updates as they are pushed out by Microsoft?
Yes, any Windows based machine can be configured to install Windows updates.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

Is calibration included in the 86100DU-WN7 Windows 7 upgrade?
86100DU-WN7 is a return to service center upgrade and does include calibration, in addition to a certificate of calibration and data.

FAQ 2017-06-28

Does the noise figure application on the PNA-X (option 029) provide a full noise-parameter system (tuners and software)?
No, we don’t provide a full noise-parameter system. Click on the question for additional information.

FAQ 2017-06-28

What is the difference of software options between M9485A and PNA/ENA series VNA?
There is no difference for option 007/009/010. There are some differences for options 025, 028, 086 and 551.

FAQ 2017-05-25

M8000 시리즈를 위한 30일 무료 체험판 라이선스
M8000 제품군 내의 모든 체험판 라이선스에 대한 개요 및 링크

FAQ 2017-01-31

Is it possible to get an error log of incorrectly sent remote commands to my PSA, E4406A, EMC, or ESA Series Spectrum Analyzer?
Yes. PSA, E4406A and the ESA Series (with firmware A.08.00 and later) support this. You may turn Verbose error logging on through the front panel or remotely, SYST:ERR:VERBOSE ON

FAQ 2016-07-05

만약 Windows XP를 계속 사용한다면, 앞으로 오류수정 서비스를 받을 수 있을까요?
네. Keysight는 서비스 지원종료되기 전까지는 마지막으로 판매된 Windows XP 까지 유지보수 되도록 할 것입니다.

FAQ 2016-07-05

몇몇 기능들은 오직 Windows 7에서만 지원이 될 예정인가요?
네. 새롭게 나올 기능들은 Windows 7 장비에서만 지원이 될 것으로 예상됩니다.

FAQ 2016-07-04

Keysight는 Windows® XP 옵션 업그레이드 판매를 계속 할 것인가요?
네. Keysight는 Windows® XP 옵션판매에 대해 종료할 계획이 없습니다.

FAQ 2016-07-04

30-Day Free Trial for X-Series Measurement Applications for X-Series Modular Instruments
30-day trial license available for the X-Series measurement applications for X-Series modular signal analyzers.

FAQ 2016-06-09

Why 34405A can't be detected in Windows 7?
There are two posibilities causing 34405A couldn't be detected. 1. IO Libraries Suit 15.1 or below...

FAQ 2015-09-21

How to enable 34410A/34411A/L4411A browser web control work in Java 8?
To enable browser web control to work in Java 8, update instrument to firmware version 2.41...

FAQ 2015-09-21

Microsoft Windows XP의 지원이 종료되면 현재 사용하는 ENA에는 어떤 영향을 미칩니까?
Microsoft는 2014년 4월 8일자로 Windows XP 운영 체제에 대한 지원을 중단합니다. 이 문서는 중요한 질문에 답변하는 데 유용할 것입니다.

FAQ 2015-07-27

Can I recover the E7515A operating system if it fails to start correctly?
Yes, E7515A has an Instrument Image Recovery mode. Click on the question above for a fuller description.

FAQ 2015-05-15

Does N9320B support Intuilink?
N9320B는 Intuilink는 지원하지 않습니다.

FAQ 2015-04-20

1 2 3 4 5 6 7 8 9 10 ... 다음