您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

76-100 / 320

排序:
Which is Most Accurate: CalReady, QuickCal (Without Load), or 2 Port Calibration?
When nothing connected at the end of RF port, CalReady is the most accurate calibration method at test port.

FAQ 2012-08-15

Why won't my Signal Analyzers Display Pulse Type Signals Properly?
These signals may be missed if the Sweep Acquisition setting is on Auto. We recommend using a Sweep Acquisition setting of 50 or 100 for GSM signals.

FAQ 2012-08-15

Opt.100 VBA utility programs do not run properly. What is wrong?

FAQ 2012-08-09

What is the maximum bit clock cycle per frame for DSI interface of U8903A?
64 bit clock cycle per frame.

FAQ 2012-07-25

What is the OS (operating system) of the X-Series signal generators?
Windows® CE

FAQ 2012-04-30

What is preventing the 89600 VSA software, running on a PC, from connecting to an X-Series signal analyzer?
Procedure for connecting from 89600 VSA software to an X-Series signal analyzer.

FAQ 2012-03-16

Can the N9342C PC software work with the N9340B?
No, the N9342C PC software can’t work with the N9340B.

FAQ 2012-03-02

How much the default RF port power of N4375B? And can I change it?
It is 0 dBm, and you can change it.

FAQ 2012-03-01

PDF PDF 46 KB
Why must my N4010A instrument firmware be A.05.04.01 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during December 2011.

FAQ 2012-02-24

是德手持式頻譜分析儀使用哪一種作業系統?
是德手持式頻譜分析儀使用 VxWorks 即時作業系統。

FAQ 2012-02-20

是德手持式頻譜分析儀是否有可用的電腦軟體?
是德所有的 HSA 均提供可免費下載的電腦軟體。

FAQ 2012-02-20

是德手持式頻譜分析儀是否支援 89600 VSA 軟體?
否,89600 VSA 軟體無法在手持式頻譜分析儀上運作。

FAQ 2012-02-20

是德手持式頻譜分析儀的軟體是否支援 Windows 7 作業系統?
是的

FAQ 2012-02-20

When does the BER test apply in the N9081A Bluetooth® measurement application?
The BER test only applies for EDR with a PRBS9 signal pattern.

FAQ 2012-01-10

How do I repair the E6621A measurement application if it fails to launch?
A utility is available that will fix the E6621A measurement application. Click on the question above for a fuller description.

FAQ 2011-12-23

Can I recover the E6621A operating system if it fails to start correctly?
Yes, E6621A has a System Software Recovery mode. Click on the question above for a fuller description.

FAQ 2011-12-21

The ENA / ENA-L was infected with the virus. What should I do?
Remove the LAN cable and perform system recovery.

FAQ 2011-10-07

Keysight ENA-L是否支援類似871x系列的內建網頁?

FAQ 2011-10-07

常見問答集 (FAQ)
常見問答集 (FAQ)

FAQ 2011-10-07

Why is my N1918A Power Analyzer USB dongle key not detected by Windows7 64bit OS.
You need to upgrade the sentinel USB system(dongle key) driver to support Windows7 64bit OS.

FAQ 2011-09-12

Can I run the Keithley 2400 program on the conventional command set mode?
Most of Keithley 2400 SCPI commands are supported by the conventional command set of B2900A, but it is not fully compatible. You can see the details in the B2900A SCPI Command Reference.

FAQ 2011-07-29

How do I transfer waveforms, screen images, and measurements from my InfiniiVision oscilloscope to a PC using IntuiLink Data Capture?
Keysight’s free IntuiLink Data Capture software provides an easy way to transfer deep-memory waveform data, screen images, and measurements from your oscilloscope to your PC via the USB, LAN, or GPIB interface.

FAQ 2011-06-06

What is EVO and what are the known issues?
EVO is an abbreviation for Extensible VEE Object, which introduce after VEE Pro Version 9.21

FAQ 2011-03-31

What are the connectivity ports on the X-Series Signal Analyzer?
There are nine connectivity ports on the X-Seires signal analyzer.

FAQ 2011-03-24

What AntiVirus software does Keysight recommend for the Keysight X-Series Signal Analyzers?
Click here for information...

FAQ 2011-03-24

上一個 1 2 3 4 5 6 7 8 9 10 ... 下一頁