您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

176-200 / 320

排序:
Can I change the regional setting of Windows system running in the E5052B?
No, the default setting is "English (United States)" and the E5052B can not support the other setting.

FAQ 2008-07-18

What are the default logins and passwords for the N9039A RF Preselector?
User name = instrument, Password = measure4u. See FAQ content for more details...

FAQ 2008-07-01

Do I need to install Antivirus software on my N9039A RF Preselector?
This would be a matter of choice depending on your use and your IT department requirements...

FAQ 2008-07-01

PNA Firmware; How do I upgrade Firmware?

FAQ 2008-06-29

Is it possible to parallel more than 2 units of the 42841A to expand bias current output range?
No. Instrument does not have firmware to control more than 2 units of the 42841A. In addition, connecting more than 2 units of the 42841A may cause an "OVLD" status due to possible imbalance of DC bias source and sink currents.

FAQ 2008-05-26

Can I use any instrument driver supporting the 4294A?
Yes. The LabView driver for the 4294A is available.

FAQ 2008-05-26

Why doesn't Signal Studio N76xxB software recognize a N76xxA license?
All N76xxB Signal Studio products should recognize the licenses of their equivalent N76xxA products...

FAQ 2008-02-25

What does channel add mean?
You can add the signal from one channel to the signal of the other channel this might be adding noise to a clean pulse, this might be a FM signal added with noise… The possibilities you have are huge.

FAQ 2008-01-29

Is there a sample project that demonstrates the operation of the VPT501?
Yes, there are 2 sample projects to be found in the directory “Samples” in the program installation directory...

FAQ 2008-01-29

How can I find out the serial number of the VPT501?
Start the Configuration Tool. Click “Scan”. All VPT501 Hardware Devices found are listed...

FAQ 2008-01-29

Does the MXG use embedded software?

FAQ 2008-01-18

Can I transfer my software licenses from my existing ESG to my new MXG?

FAQ 2008-01-18

How can I find out when new firmware or software is released?
There are three ways to check for updates.

FAQ 2008-01-09

Is it possible to save a full-sized screen capture, without the softkeys?
Yes... See content for details...

FAQ 2007-12-20

How do I change Daylight Saving Time Settings on the ENA?
Keysight confirmed that Daylight Saving Time Setting can be changed with following procedure...

FAQ 2007-10-05

I remotely changed my 8648X modulation from Pulse to AM, but the display still indicates 'PULSE'. Is the 8648X outputting an AM or PM modulation?
The AM modulation is activated now. The annotation can be corrected using a short program.

FAQ 2007-09-24

What are the differences between the BenchLink DataLogger software for 34970A and 34980A?

FAQ 2007-07-20

設定Keysight ENA、I/O程式庫及Intuilink,以透過LAN來進行通訊

FAQ 2007-07-10

How do I open older Keysight Logic Analyzer application files in newer versions?

FAQ 2007-06-19

How do I update the Scope Connect software and 3000 Series oscilloscope firmware?
Follow these instructions.

FAQ 2007-04-26

Are the x6000 Automated X-ray Inspection System algorithms better or different than the 5DX?
The x6000 Automated X-ray Inspection System algorithms are based on and follow the same basic approach as those from the 5DX.

FAQ 2007-04-22

Can the user have different levels of control on the x6000 Automated X-ray Inspection system? Are there different logins?
There are 4 levels of logins on the x6000 Automated X-ray Inspection System: administrator, developer, operator, and service. The system administrator has ability to specify the account capability.

FAQ 2007-04-22

When are you going to support Vista?
Once Vista is proven to be a robust, stable operating environment for manufacturing applications a date will be selected for move on the x6000 Automated X-ray Inspection System.

FAQ 2007-04-22

Are computed channels supported in the Keysight 34970A?
Computed channels are not supported on the 34970A, but are on the BenchLink Data Logger software.

FAQ 2006-01-18

How do I configure channels in BenchLink Data Logger 3, run a scan in a remote location, and upload the data back into my computer?
Create a setup in BenchLink Data Logger 3 software as you normally would, then go to the "Configuration | Download Open Configuration to 34970A..." menu to download the setup to the 34970A...

FAQ 2006-01-18

上一個 1 2 3 4 5 6 7 8 9 10 ... 下一頁