您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

151-175 / 320

排序:
If I already have an E4438C-406 Bluetooth® license, can I upgrade to N7606B Signal Studio Software Bluetooth® without any extra charges?
Yes, you can upgrade to the N7606B Signal Studio Software free of charge.

FAQ 2009-06-09

ESA-L1500A: Spectrum Analyzer Firmware Upgrade and Service Connector
A Keysight Service Center may be able to provide this service...

FAQ 2009-04-14

Will all versions of the Keysight Logic Analyzer application run on Windows® 2000?
No, the highest version supported under Windows 2000 is 3.67.1009. Use 3.80.0002 or higher for Windows XP SP3 or Windows Vista.

FAQ 2009-02-17

Why when using the parallel interleave mode and 1 clock per sample, the data seems to be clocked on the opposite clock edge than what the GUI state...
This is a known issue and has been noted for future consideration. The workaround is...

FAQ 2009-02-12

How do I do transfer my Keysight EEsof EDA products from one platform to another?
Codeword platform transfers are best arranged by contacting Keysight EEsof EDA Business Support.

FAQ 2009-02-04

Is training available for Keysight EEsof EDA products?
Yes, Keysight EEsof EDA Customer Education and Services provides training.

FAQ 2009-01-22

Are National Instruments software drivers available for Keysight signal generators?
Yes. LabView drivers are available from the National Instruments website for many current and discontinued Keysight signal generators.

FAQ 2009-01-12

Does the Keysight Measurement Manager (AMM) support regional language settings other than English (US)?
Yes, the Keysight Measurement Manager (AMM) supports regional language settings other than English (US)….

FAQ 2009-01-12

Why doesn't Windows® detect new hardware when I plug the E5813A USB Hub into the computer?
The new hardware is not detected when you plug the E5813A USB Hub into the computer because the PC driver may not be installed properly....

FAQ 2009-01-12

Why is an incorrect version of Signal Studio N7613A, N7612B, and N7606B shown when I use the “Add or Remove Programs” window in “Control Panel” on ...
This Signal Studio version number discrepancy can be ignored, please proceed with your application removal. This error will be corrected with the next version roll.

FAQ 2008-12-02

Is it possible to get an error log of incorrectly sent remote commands to my PSA, E4406A, EMC, or ESA Series Spectrum Analyzer?
Yes. PSA, E4406A and the ESA Series (with firmware A.08.00 and later) support this. You may turn Verbose error logging on through the front panel or remotely, SYST:ERR:VERBOSE ON

FAQ 2008-11-21

Can I write my own measurement personalities or downloadable programs (DLPs) for the E4406A, PSA Series, or ESA Series Analyzers?
No. We do, however, offer many tools to facilitate remotely interfacing of our instruments to a PC to write custom applications. We do also offer flexible digital demod through the 89601A software, and this software does have custom macro capabi...

FAQ 2008-11-21

Does the E4406A or PSA Series support an external keyboard or mouse?
The external keyboard port is only used to control the instrument during firmware upgrades. The user interface for the E4406A or PSA allows you to completely control the instrument via the front panel keys.

FAQ 2008-11-20

I use Keysight VEE and Labview and would like instrument drivers for the E4406A, PSA Series, ESA Series, and EMC Series. Where can I download VXI ...
The E4406A, PSA Series, ESA Series, and EMC Series new IVI-Com drivers as well as the older VXI Plug and Play drivers are available in the "Drivers and Software" section for each product.

FAQ 2008-11-20

Why do I get a message telling me that I need Option B72 when I try to load the latest version of firmware into my ESA Spectrum Analyzer?
Due to the increased number of features included, firmware versions A.08.02 or later require a larger amount of memory.

FAQ 2008-10-27

Can I install Signal Studio license files on the ESG or MXG over GPIB?
No. Signal Studio licenses, perpetual, transportable and time-based cannot be installed using GPIB.

FAQ 2008-10-13

ESA Series L1500A: Spectrum Analyzer Chirping Noise

FAQ 2008-10-08

ESA Series L1500A: Spectrum Analyzer Screen Display Brightness

FAQ 2008-10-08

ESA Series L1500A: Spectrum Analyzer Power-On Selection
The analyzer's power-on selection switch, located on the rear panel (immediately below the DC fuse), is probably set to PWR ALWAYS ON, instead of PWR NORM.

FAQ 2008-10-08

During 5DX application development, sometimes automatic alignment and surface mapping run each time I try to run any type of test in Algorithm Tune...
A work around exists to help the user from having to restart the system to eliminate this issue.

FAQ 2008-10-05

What is the required operating system for the U2300A Series Modular Multifunction Data Acquisition (DAQ) devices?
The operating system required for the U2300A Series Modular Multifunction Data Acquisition (DAQ) devices is….

FAQ 2008-09-25

Does the Measurement Manager (AMM) run on a Linux operating system?
No, the Measurement Manager (AMM) does not run on a Linux operating system.

FAQ 2008-09-25

是否可針對已儲存的波形進行量測?
是否可針對已儲存的波形進行量測?

FAQ 2008-08-03

是否能夠儲存多重 TDR 軌跡,然後在示波器上將其顯示為波形,並與目前的量測波形做比較?
可以將多重 TDR 軌跡儲存為內部格式,以供未來參考……

FAQ 2008-08-03

是否能夠儲存先前的 TDR 量測波形,然後載入該波形,並與目前的 TDR 量測波形做比較?
是否能夠儲存先前的 TDR 量測波形,然後載入該波形,並與目前的 TDR 量測波形做比較?

FAQ 2008-08-03

上一個 1 2 3 4 5 6 7 8 9 10 ... 下一頁