您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

101-125 / 320

排序:
Firmware Upgrades via the Web

FAQ 2011-02-15

8720的升級

FAQ 2010-11-20

Why won't Help (.hlp) files view properly with Windows Vista?
In order to view 32-bit Help (.hlp) files with Windows® Vista, you must download the WinHlp32.exe Help program from the Microsoft web site at http://go.microsoft.com/fwlink/?LinkID=82148.

FAQ 2010-10-12

Where can customers download instrument drivers? (LabVIEW, Visual-studio.net,…)
The instrument drivers are provided with each instrument on a CD...

FAQ 2010-10-06

What drivers will be provided with modular products?
IVI-COM, IVI-C and LabVIEW (G), are provided with all Keysight modular products...

FAQ 2010-10-06

How do I control instruments such as 82357A, E5810A, and 82350B using the GPIB interface?
There are several approaches to control instruments via the GPIB interface...

FAQ 2010-10-04

如何更新 Keysight 邏輯分析儀的 BIOS?
所有 1680、16800 及 16900 系列邏輯分析儀的 BIOS 接可透過一片 BIOS 更新光碟進行更新。

FAQ 2010-09-25

我要如何將 Keysight 5000/6000/7000 系列 InfiniiVision 示波器上的螢幕畫面,儲存到 USB 儲存裝置上?
下列指示假設您的示波器使用系統軟體 05.00 或以上版本 (如需得知示波器的版本,請參見 公用程式 (Utility) | 服務 (Service) | 關於示波器 (About Oscilloscope) -> 系統版本 (System version) )。

FAQ 2010-09-15

我要如何安裝圖形量測應用程式 (GMA) Keysight N4017A 軟體的授權?
當您透過 http:///find/softwarelicense 取回 Keysight N4017A 權利認證時,必須決定是否要將軟體鎖定在 Keysight N4010A 測試儀或 PC 上使用。

FAQ 2010-09-15

IO Libraries Suite: What pieces of software do I need to install for the IO Libraries to work?
View the data sheet for the full list of requirements.

FAQ 2010-09-08

IO Libraries Suite: What interfaces and operating systems are supported?
View the Keysight IO Libraries Support matrices.

FAQ 2010-09-08

Will a PCI-X slot work for the N5101A Baseband Studio PCI Card?
Yes, PCI-X should be backward compatible with conventional PCI 2.2.

FAQ 2010-09-08

What type of internal memory is installed into the 33520A-Series Function/Arbitrary Waveform Generators?
Please refer to the document linked to this page for a comprehensive listing of memory installed into the Keysight 33520A-Series Function / Arbitrary Waveform Generators

FAQ 2010-08-09

Why does the error message "Failed to retrieve available devices. Please make sure the connection to Keysight IO libraries is available" appear…
The message "Failed to retrieve available devices. Please make sure the connection to Keysight IO libraries is available" appear because….

FAQ 2010-08-09

What should I do when seeing crash during the installation of Power Analyzer (software licensing version) into my non-English version of Windows…
The workaround steps to resolve this are listed below….

FAQ 2010-08-09

How can I prevent a loading delay when using the Measurement Manager with Microsoft® .NET 2.0 on a computer that is connected to a LAN…
To prevent a loading delay when using the Measurement Manager (AMM) with Microsoft® .NET 2.0, follow the instructions below:….

FAQ 2010-08-09

Why is my acquired data for U2300A and U2500A shifted? eg. Column 2 data is in column 1, column 3 data is in column 2, and so on.
Install DAQ hardware driver version 1.05 and above.

FAQ 2010-08-09

When will Keysight USB modular instruments and USB Modular DAQs supports Windows 7?
For 32 bit Windows 7, the supportability of modular instruments and DAQs will happen...

FAQ 2010-07-18

I have purchased the Segmented Memory option, N5454A, for my InfiniiVision oscilloscope. However, I can’t find the feature in the menus. What can I...
You need to upgrade your oscilloscope to the latest firmware...

FAQ 2010-07-02

Does Sweep End signal output on 24-bit I/O port of the 4294A have similar definition as End of Measure (EOM) signal on LCR meters?
Sweep End signal means the end of entire sweep measurement, not the end of measurement at each sweep point.

FAQ 2010-07-02

ENA/ENA-L does not go directly to the instrument mode after power on, but shows the password dialog box or the windows desktop. How do I fix it?
This is because the user registration was improperly done when the first time the power was turned on. Performing system recovery is recommended to fix it.

FAQ 2010-07-02

Serial BERT Software
Find all the latest software and firmware for the Serial BERT including: N4902B, N4906A, N4906B, and N4917A.

FAQ 2010-06-24

In the ESA Series, how can I save the results of a Channel Power, ACP, OBW, Emission Bandwidth, or Harmonic Distortion measurement?
Save a screen image to the floppy disk drive.

FAQ 2010-06-14

What operating systems are supported for use with the 89601A/AN Series software?
Windows NT4 (SP6 or greater), Windows 2000, Windows XP Professional, Windows Vista, Windows 7

FAQ 2010-05-17

在是德ENA繫列網絡分析儀中,要做如何的設置才能支持外部顯示屏?
为了支持外部显示屏,必须在ENA-B中显示模式中选“Intel Dual Display Twin”。请根据以下步骤操作做具体设置

FAQ 2010-05-14

上一個 1 2 3 4 5 6 7 8 9 10 ... 下一頁