这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

1-16 / 16

排序:
How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

How do I update the operating system in an N9038A MXE EMI receiver from Windows XP to Windows 7?
See what is required to update the operating system in an N9038A MXE EMI Receiver...

FAQ 2014-04-02

Which version of the CPRI standard is the N5120A compliant to?
The N5120A is compliant up to v1.1.

FAQ 2013-09-27

现有客户在购买了 N9094AK-PC4 或 N9094AK-SSD 选件后,是否要把仪器送往当地的 SSU 服务中心进行升级?
不是。N9094AK-PC4 和 N9094AK-SSD 升级选件均配备了镜像 SSD。

FAQ 2013-05-08

我现有的处理器是否支持 Windows 7 系统?
处理器应当符合 Windows 7 系统的最低配置/型式要求,在仪器的显示系统屏幕上以 PC4 和 PC5 表示。

FAQ 2013-05-08

能否保存早先的 TDR 测量波形,并载入与当前的 TDR 测量结果进行比较?
可以保存早先的 TDR 测量波形,并载入到示波器上与当前的 TDR 测量结果进行比较。

FAQ 2011-06-22

能否保存多条 TDR 迹线并在示波器上显示其波形,以便与当前的测量进行比较?
可以将多条 TDR 迹线保存为内部格式,供以后参考……

FAQ 2011-06-06

How do I control instruments such as 82357A, E5810A, and 82350B using the GPIB interface?
There are several approaches to control instruments via the GPIB interface...

FAQ 2010-10-04

Serial BERT Software
Find all the latest software and firmware for the Serial BERT including: N4902B, N4906A, N4906B, and N4917A.

FAQ 2010-06-24

N5532A 传感器模块的频率范围是多少?
100 kHz 至 4.2 GHz,10 MHz 至 18 GHz,30 MHz 至 26.5 GHz 和 30 MHz 至 50 GHz。

FAQ 2010-04-13

Does E5805A or E5813A driver supports Linux operating systems?
No, E5805A or E5813A does not support Linux operating systems

FAQ 2009-10-20

Why when using the parallel interleave mode and 1 clock per sample, the data seems to be clocked on the opposite clock edge than what the GUI state...
This is a known issue and has been noted for future consideration. The workaround is...

FAQ 2009-02-12

Why doesn't Windows® detect new hardware when I plug the E5813A USB Hub into the computer?
The new hardware is not detected when you plug the E5813A USB Hub into the computer because the PC driver may not be installed properly....

FAQ 2009-01-12

Is it possible to get an error log of incorrectly sent remote commands to my PSA, E4406A, EMC, or ESA Series Spectrum Analyzer?
Yes. PSA, E4406A and the ESA Series (with firmware A.08.00 and later) support this. You may turn Verbose error logging on through the front panel or remotely, SYST:ERR:VERBOSE ON

FAQ 2008-11-21

可以对保存的波形进行测量吗?

FAQ 2008-08-03