이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 545

정렬방식:
U2651A / U2652Ar에서 디지털 입력 전압 <24V를 지원할 때 28V 디지털 신호를 U2651A / U2652A에 어떻게 입력 할 수 있습니까?
전압 분배기를 연결...

FAQ 2017-10-25

How do I measure a pulsed RF signal output with a sampling oscilloscope?
There are two possible ways. Click on the question for additional information.

FAQ 2017-06-28

If we use external clocks for both the Pattern Generator and Error Detector parts, can we run them at different data rates?
It would be more straight-forward to provide the PG (TX) with a 10 GHz clock (for 10 Gb/s data) and then use the 1:4 demux and provide the ED (RX) with a 2.5 GHz clock (measuring 2.5 Gb/s data). Click on the question for additional information.

FAQ 2017-06-28

N9080B SEM measurement defaults seem to be different from 3GPP 36.141 V12.12.0 (2016-06). Is N9080B doing something it shouldn’t?
To make a “True RMS detection”, as requested by the 3GPP conformance testing, based on ITU-R SM.329, for a mix of noise-like & CW-like signals under test, use “Peak Detector with very narrow VBW”. Click on the question for additional information.

FAQ 2017-06-28

When using the DIQ application, what happens when I set the internal receiver to measure beyond the frequency range of my instrument?
Data for frequencies beyond the instrument hardware limitations is extrapolated from the hardware’s maximum and minimum limits. Click on the question for additional information.

FAQ 2017-06-28

What is the raw jitter tolerance for the N4960A/N4952A?
There is no CDR in the N4960A, so by itself, the JTOL plot will be a flat line somewhere below 1 UI. An external CDR can be used. Click on the question for additional information.

FAQ 2017-06-28

What is the difference between the Integrated true-mode stimulus application (opt 460) and the Differential and I/Q devices application (opt 089)?
The Integrated TMSA and the DIQ both simplify measurements of differential (balanced) devices. The two applications however, are used for different measurements. Click on the question for additional information.

FAQ 2017-06-28

In N7625B, how many instances of carriers and carrier aggregations do the software support?
One connected signal generator can support one instance of Carrier Aggregation mode. One instance of Carrier Aggregation can support 5 component carriers.

FAQ 2016-07-08

파워미터 화면에 dBm을 dBmV로 어떻게 변환 합니까?
Load 임피던스가 50ohm이면, dBmV = dBm + 47

FAQ 2016-07-05

Is it possible to get an error log of incorrectly sent remote commands to my PSA, E4406A, EMC, or ESA Series Spectrum Analyzer?
Yes. PSA, E4406A and the ESA Series (with firmware A.08.00 and later) support this. You may turn Verbose error logging on through the front panel or remotely, SYST:ERR:VERBOSE ON

FAQ 2016-07-05

4396B 옵션 010에서 On-board 칩 디바이스 측정을 위한 프로브가 있습니까?
키사이트에서는 관련 픽스쳐를 제공하지 않습니다.

FAQ 2016-04-24

How do I measure accurately below -60dBm using U2040 X-Series Sensor?
Click on the question above for recommended steps.

FAQ 2015-12-14

왜 5MHz 또는 15MHz에서 측정데이터가 불연속 적으로 나타나는지와 4294A에서는 이 현상을 제거할 수 있습니까?
4294A는 측정 주파수 테스트 리드의 공진을 제거하기 위해 50 옴에서 각 측정 단자를 terminating해서 110 MHz까지의 주파수 측정범위가 확장되어 있습니다.(4294A 내부의 리드를 포함합니다).

FAQ 2015-10-28

Can the counter make simultaneous measurements on channels 1 and 2?
No. The channels are independent and can be configured separately; however, they do not have separate processors.

FAQ 2015-09-21

Why will the counter not make low frequency measurements?
Verify the System Timeout setting by pressing Utility - Instr Setup - Time Out Settings. Turn the time out off or set it to a large value.

FAQ 2015-09-01

Why does the counter fail to make a very low frequency measurement?
Verify the System Timeout setting by pressing Utility - Instr Setup - Time Out Settings. Turn the time out off or set it to a large value.

FAQ 2015-09-01

하나의 위성 웨이브폼 파일에 어떤 데이터가 담겨있습니까?
웨이브폼 파일에는 데이터로 0과 1이 교대로 구성되어 있습니다.

FAQ 2015-08-02

16452A에서 사용할 수 없는 액체물질의 리스트나 조건이 있나요?
산성, 알카리성, 이온 성 물질

FAQ 2015-07-23

ENA를 사용하여 어떻게 75 Ω 측정을 할 수 있습니까?
ENA를 사용하여 시스템 특성 임피던스를 75 Ω으로 변경시켜 75 Ω 측정을 할 수 있습니다.

FAQ 2015-03-09

16454A에 정의된 전기적인 길이 값은 무엇입니까?
16454A의 전기적인 길이는 E4991A에서 0mm로 초기설정되어있습니다.

FAQ 2015-01-28

2-포트 ENA로 픽스처 시뮬레이터 기능을 사용할 수 있습니까?
예. 그러나 기능이 제한적입니다...

FAQ 2015-01-09

4339B장비에 외부 DC 소스를 사용할 수 있습니까?
예.4339B는 내부 DC 소스 또는 외부 DC 소스가 사용되는 DUT의 전류 또는 저항을 측정 할 수있다.

FAQ 2014-10-13

Is there a summary of available cable test methods when using the FieldFox Hand Held portable analyzers?
Yes. Please refer to the FieldFox Hand Held Cable Test details and methods below.

FAQ 2014-08-11

E4991A와 test head가 분리 하거나 케이블로 연결이 가능 한가요?
네 E4991A-010또는 E4991-007옵션으로 가능 합니다.

FAQ 2014-04-23

How do you calculate the individual output power of each satellite?
ESG와 PSG의 경우 power level은 각각의 위성들에게 동일하게 분배됩니다.

FAQ 2014-04-18

1 2 3 4 5 6 7 8 9 10 ... 다음