検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

絞込み

絞込みのリセット

トピック

コンテンツのタイプ

製品カテゴリ

1-25 / 594

並べ替え
If we use external clocks for both the Pattern Generator and Error Detector parts, can we run them at different data rates?
It would be more straight-forward to provide the PG (TX) with a 10 GHz clock (for 10 Gb/s data) and then use the 1:4 demux and provide the ED (RX) with a 2.5 GHz clock (measuring 2.5 Gb/s data). Click on the question for additional information.

FAQ 2017-06-28

What is the difference between the Integrated true-mode stimulus application (opt 460) and the Differential and I/Q devices application (opt 089)?
The Integrated TMSA and the DIQ both simplify measurements of differential (balanced) devices. The two applications however, are used for different measurements. Click on the question for additional information.

FAQ 2017-06-28

What is the raw jitter tolerance for the N4960A/N4952A?
There is no CDR in the N4960A, so by itself, the JTOL plot will be a flat line somewhere below 1 UI. An external CDR can be used. Click on the question for additional information.

FAQ 2017-06-28

N9080B SEM measurement defaults seem to be different from 3GPP 36.141 V12.12.0 (2016-06). Is N9080B doing something it shouldn’t?
To make a “True RMS detection”, as requested by the 3GPP conformance testing, based on ITU-R SM.329, for a mix of noise-like & CW-like signals under test, use “Peak Detector with very narrow VBW”. Click on the question for additional information.

FAQ 2017-06-28

When using the DIQ application, what happens when I set the internal receiver to measure beyond the frequency range of my instrument?
Data for frequencies beyond the instrument hardware limitations is extrapolated from the hardware’s maximum and minimum limits. Click on the question for additional information.

FAQ 2017-06-28

How do I measure a pulsed RF signal output with a sampling oscilloscope?
There are two possible ways. Click on the question for additional information.

FAQ 2017-06-28

In N7625B, how many instances of carriers and carrier aggregations do the software support?
One connected signal generator can support one instance of Carrier Aggregation mode. One instance of Carrier Aggregation can support 5 component carriers.

FAQ 2016-07-08

【VSA】【SG】RF信号をキャプチャして信号源で再生することはできますか?
はい。ベクトル・シグナル・アナライザを使用することで、RFキャプチャ信号を信号源から再生することが可能です。

FAQ 2016-02-03

How do I measure accurately below -60dBm using U2040 X-Series Sensor?
Click on the question above for recommended steps.

FAQ 2015-12-14

Can the counter make simultaneous measurements on channels 1 and 2?
No. The channels are independent and can be configured separately; however, they do not have separate processors.

FAQ 2015-09-21

Why will the counter not make low frequency measurements?
Verify the System Timeout setting by pressing Utility - Instr Setup - Time Out Settings. Turn the time out off or set it to a large value.

FAQ 2015-09-01

Why does the counter fail to make a very low frequency measurement?
Verify the System Timeout setting by pressing Utility - Instr Setup - Time Out Settings. Turn the time out off or set it to a large value.

FAQ 2015-09-01

ENAで75 Ω測定を実行する方法は?
ENAで75 Ω測定を実行するには、システム特性インピーダンスを75 Ωに変更します。

FAQ 2015-03-09

[仕様] ファンクションジェネレーターは電流値で出力値の設定は出来ますか?また、ドライブできる電流はどの程度ですか?
電流値で設定をすることはできません。ドライブできる能力は仕様化されておりません。

FAQ 2014-11-11

[操作]ファンクションジェネレーターはフローティング(浮かせて)で使用することができますか?
グランドから42Vpk(出力+DCオフセット)まで浮かせることができます。

FAQ 2014-11-11

[操作] 振幅電圧、オフセット電圧を設定しても、上限と言われて設定できない。どうすればよいか?
振幅とオフセットの間には制限事項があります。ご確認ください。

FAQ 2014-11-11

[操作] ファンクションジェネレーターに設定以上のオフセットを載せて出力したいです。どのようにすればよいですか?
外部にDC電源を用意し、DC電源をFGに直列に接続すれば、オフセットを追加することができます。

FAQ 2014-11-11

Is there a summary of available cable test methods when using the FieldFox Hand Held portable analyzers?
Yes. Please refer to the FieldFox Hand Held Cable Test details and methods below.

FAQ 2014-08-11

[アプリケーション]USBコンプライアンステストに関する資料を探していますが、どのような資料を用意していますか?

FAQ 2014-03-03

Why does my FieldFox spectrum analyzer preamplifier increase the noise floor when engaged?
The FieldFox spectrum analyzer preamplifier selection will normally reduce the displayed noise floor when activated. However, if the FieldFox RF attenuation AUTO selection is set to ON then the preamp may not reduce the noise floor.

FAQ 2014-03-03

Can I do voltage measurement using the U2802A rather than temperature measurement?
Yes, you can do voltage measurement easily by using the Keysight Measurement Manager (AMM)...

FAQ 2013-11-17

8508Aベクトル電圧計をE5061Bネットワーク・アナライザに置き換え
外部CW信号の位相差の測定は、8508Aベクトル電圧計の代表的なアプリケーションです。

FAQ 2013-10-14

[仕様/機能] セグメント・メモリ捕捉モードはなぜ有用ですか?どのInfiniiumがこのモードを備えていますか?
セグメント・メモリ・モードは、長期間で分割されたイベントによって波形を捕捉するための、効率的な捕捉メモリの活用方法を提供します。現行のすべてのInfiniiumおよび多くの旧型のInfiniiumがセグメント・メモリをサポートしています。

FAQ 2013-09-18

[アプリケーション] USB2.0:HS Electrical Test Tool (USBHSET)は、どこから入手できますか?
被測定対象物をテストモードに入れるには、USB2.0(EHCI)を備えたコンピューターが必要になります。

FAQ 2013-09-03

PNAシリーズのベクトル・ネットワーク・アナライザでは、Touchstone(SnP)ファイルを折り返しのない位相で保存することはできますか?
はい、できます。PNAシリーズのベクトル・ネットワーク・アナライザは、Touchstone(SnP)ファイルを折り返しのない位相として位相情報を保存することができます。Touchstoneファイルの保存で折り返しのない位相を実現するには、次の手順を実行します。

FAQ 2013-09-02

1 2 3 4 5 6 7 8 9 10 ... 次へ