Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-23 of 23

Sort:
Why is the segmented memory acquisition mode useful and which Infiniium oscilloscopes support it?
Segmented memory mode offers more efficient acquisition memory usage for storing waveforms with events of interest that are separated by long periods of time. All currently shipping Infiniiums and many older units support segmented memory.

FAQ 2013-09-18

Can I manually set the sample rate on my InfiniiVision oscilloscope?
Although the sample rate cannot be directly set on any InfiniiVision oscilloscope, it can be set indirectly by adjusting the oscilloscopes time per division setting.

FAQ 2012-10-30

What is the difference between the Auto and Normal trigger modes on InfiniiVision oscilloscopes?
In auto trigger mode, the trigger will be forced if the specified conditions are not met. In normal trigger mode, the trigger will never be forced and a trigger will only occur if the specified conditions are met.

FAQ 2012-10-17

Which Keysight oscilloscopes have a 10 MHz reference input/output?
6000 Series, 6000L Series, 7000A Series, 7000B Series, 9000 Series, 54850 Series (Output only), 80000A Series, 80000B Series, 90000A Series and 90000 X-Series

FAQ 2012-10-17

How can I de-embed a test fixture using the 86100C/D Digital Communications Analyzer?
N1010A software with InfiniiSIM-DCA option provides the capability to de-embed and embed fixtures, cables, probes, and other circuit elements.

FAQ 2012-09-25

Are the input channels on the U1602B and U1604B Handheld Oscilloscopes isolated?
No, both scope channels (channel 1 and channel 2) on the U1602B and U1604B Handheld Oscilloscopes are not isolated.

FAQ 2011-03-31

For the InfiniiMax probes, what effect does the "Signal being probed" setting have? Why do I have to specify single-ended or differential?
Infiniium scopes and InfiniiMax differential probe amplifiers have a unique method of applying DC offset which considers whether the signal being probed is single-ended or differential...

FAQ 2010-10-06

How do I extract the 32Mpts from U270xA?
One way of “viewing” the full memory waveform is using the zoom function (that the red arrow...

FAQ 2010-09-14

Why does the pulse shape of my scope probe compensation look different from the pulse shape shown…
The compensation signal (square wave) that you see is different from the pulse shape shown in the U1602A/U1604A's user’s manual because….

FAQ 2010-08-09

How do I convert *.svw file to *.csv file in PC Link for U160xA/B?
1) From within PC Link, click on the "Load SVW" icon on the tool bar...

FAQ 2010-07-18

My InfiniiMax probe fails calibration or does not accurately pick up the cal signal when I use the E2655A test fixture. What could be wrong?
The first step in troubleshooting a failed probe calibration should be to compare the actual signal and the probed signal. If the probed signal does not track the actual signal well, it is most likely due to a poor connection.

FAQ 2010-03-09

Keysight Infiniium Oscilloscopes: Programming the Oscilloscope
Use the example programs and programming manual available for download from this web site.

FAQ 2009-12-11

How do I get the maximum available memory depth from my Infiniium oscilloscope?
The various Infiniium models offer between 32K and 128M points of memory per channel. The following guide shows you how to get the maximum available memory from your particular scope.

FAQ 2009-11-19

How do I put an Infiniium oscilloscope into XY mode?
All Infiniium models have a math function called "versus", which plots one channel or function versus another channel or function.

FAQ 2009-02-17

How can I use a Keysight oscilloscope as a basic I-V curve tracer?
You can use the ocsilloscope's XY mode to plot I-V characteristics...

FAQ 2008-10-13

Can I automatically position the Y1 and Y2 cursors to the voltage values at X1 and X2?
Yes, using SCPI remote programming commands, follow these steps...

FAQ 2008-09-30

Why do I see more noise on my oscilloscope when a probe is connected?
When a probe is connected, the scope changes its attenuation setting so that it correctly displays the voltage coming from the probe.

FAQ 2006-12-04

When using TV trigger mode with a Keysight oscilloscope, can I trigger only on even or odd fields?
Yes. All current Keysight scopes with TV triggering are capable of exclusively triggering on odd or even fields.

FAQ 2006-12-04

Can my 54600-series or 6000-series scope use channels 3 and 4 for XY mode or math functions?
These oscilloscopes can perform math functions such as FFT, integration, and differentiation on any analog channel or even on another math function. But they cannot use channel 3 or 4 for XY mode, addition, subtraction, or multiplication.

FAQ 2006-11-04

Keysight Infiniium Oscilloscopes: What Trigger Modes Does the Instrument Have?

FAQ 2003-08-01

Keysight Infiniium Oscilloscopes: Can You Trigger One Keysight Infiniium Oscilloscope From Another?
Infiniium Oscilloscopes

FAQ 2003-08-01

Keysight Infiniium Oscilloscopes: Will Keysight Infiniium Scopes Trigger on HDTV Signals?
Infiniium Oscilloscopes

FAQ 2003-08-01

1653xA: Can I Do High Frequency Rejection to Filter a Signal Captured by the 16534A?

FAQ 2002-06-27