Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По теме

По типу содержания

По типу оборудования

1-25 из 102

Упорядочить:
How can I make 75 Ω measurements using the ENA?
You can make 75 Ω measurements with the ENA by shifting system characteristic impedance to 75 Ω.

FAQ 2015-03-09

Replacing the 8508A vector voltmeter with the E5061B network analyzer
Measuring the phase difference of an external CW signals is a typical measurement application of the 8508A vector voltmeter.

FAQ 2013-10-14

How can I perform the calibration/compensation when I use the 16094A with a 7-mm connector extension cable?
It is recommended to perform the following compensation procedure...

FAQ 2013-06-05

Does the ENA 6 series have the swept sweep mode in the frequency sweep?
No. The E5061A/62A and E5061B have only stepped sweep mode in the frequency sweep.

FAQ 2013-04-25

Is it possible on the Keysight ENA series Network Analyzers to over-ride the output source blanking at every sweep end?
Yes, the output source blanking on sweep retrace can be prevented by turning off the Initial Source Port Control function.

FAQ 2012-12-18

Does the ENA 6 series support User Characterized ECal?
No.

FAQ 2012-12-10

Are mixed mode S-parameter measurements possible on the 2-port ENA?
Yes. The equation editor function allows for the real-time calculation of mixed mode S-parameters on the 2-port ENA.

FAQ 2012-12-10

What resources does Keysight recommend to help facilitate learning proper impedance measurement techniques?

FAQ 2012-07-17

Why is a negative D value sometimes displayed when a furnished PTFE plate is measured with the 16453A?
When resistance value of Short compensation data is too large, measured D value is overcompensated for the Short resistance and results in a negative value

FAQ 2012-04-08

What is an alternative solution to the 87075C / 87050E replacement?
Build your home-made switch box using the L4491A RF/MW switches. Refer to the application note for details.

FAQ 2012-01-11

What is the difference between Smoothing and Averaging on a Keysight network analyzer?

FAQ 2011-10-07

Is it possible to measure the velocity of propagation utilizing a Keysight Vector Network Analyzer (VNA)?
Keysight VNAs do not directly provide the velocity of propagation measurement. As an alternative the steps below outline a method to calculate the velocity of propagation based upon the physical length of the cable under test.

FAQ 2011-10-07

Are the adapters in the 85033E 30kHz to 9GHz calibration kit phase matched?
Yes.

FAQ 2011-10-07

For Cable Testing should I use a TDR, a network analyzer, or both?
The cable specifications will determine the test equipment requirements...

FAQ 2011-10-07

The "set Zo" function does not appear to affect the displayed S-parameters of my network analyzer. How does this function work?

FAQ 2011-10-07

What is the difference between "sweep speed", "cycle time" and "time per data point" as related to a vector network analyzer?

FAQ 2011-10-07

On the ENA / ENA-L, what occurs if I select "order-based display" in sweep mode?
Measurement points of different segments are plotted in constant intervals.

FAQ 2011-10-07

On the ENA, how can I make CW sweep (Fixed frequency) without turning off the ENA's output signal each time a sweep finishes?
Turn off the "Init Src Ctrl" feature, then hold trigger.

FAQ 2011-10-07

In limit line test, the marker value at that point is beyond the limit line. However, the Pass/Fail indicates a Pass condition. Why?

FAQ 2011-10-07

Can the 4294A display a polar chart and an R vs. jX (G vs. jB) diagram?
Yes, a polar chart and a real part vs. imaginary part diagram can be selected when the measurement parameter of the 4294A is set to "COMPLEX X-Y".

FAQ 2011-06-07

How can the E4980A or the 4263B measure internal impedance of batteries?
Insert DC blocking capacitors between the measurement terminals and a battery DUT. The 16065C can substitute for the DC blocking capacitors.

FAQ 2011-06-07

What is the possible cause of the difference when the permittivity measured with the 16453A is different from the value previously obtained?
Most likely cause of the measurement discrepancy or drift is insufficient electrode pressure due to improper pressure adjustment.

FAQ 2011-06-07

How should a DC blocking capacitor be inserted between the 42941A probe and a DUT when a live DC voltage exists on the device?
It is recommended to insert a SMA DC blocking adapter between the furnished pin probe and 3.5-mm connector at the tip of the 42941A.

FAQ 2011-06-07

Why is permeability measurement result unstable when a low permeability magnetic material or a thin magnetic material is measured with the 16454A?
It is because the impedance of the magnetic material inserted into the 16454A is too low for the impedance analyzer to measure it accurately.

FAQ 2011-06-07

What is the measurement setup for obtaining same spectral levels of measured signal or noise irrespective of the sweep frequency span of the 4395A?
Change the detection mode to sample detection mode.

FAQ 2011-06-03

1 2 3 4 5 Следующие