이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 218

정렬방식:
FieldFox Manuals, Firmware, Software and Product Support
Manuals, firmware upgrade, software trials & upgrade and support page for FieldFox analyzers

FAQ 2020-02-24

U2651A / U2652Ar에서 디지털 입력 전압 <24V를 지원할 때 28V 디지털 신호를 U2651A / U2652A에 어떻게 입력 할 수 있습니까?
전압 분배기를 연결...

FAQ 2017-10-25

How to measure output frequency of E4981A Capacitance Meter?
To measure the output frequency of E4981A Capacitance Meter, interface box (Keysight part number: 04294-61002) is required…

FAQ 2017-09-20

When using the DIQ application, what happens when I set the internal receiver to measure beyond the frequency range of my instrument?
Data for frequencies beyond the instrument hardware limitations is extrapolated from the hardware’s maximum and minimum limits. Click on the question for additional information.

FAQ 2017-06-28

What is the difference between the Integrated true-mode stimulus application (opt 460) and the Differential and I/Q devices application (opt 089)?
The Integrated TMSA and the DIQ both simplify measurements of differential (balanced) devices. The two applications however, are used for different measurements. Click on the question for additional information.

FAQ 2017-06-28

4338B에는 4단자 쌍 측정 회로구성이 있습니까?
아니요. 4338B는 차폐된 4단자 쌍 회로 구성으로 되어있습니다.

FAQ 2017-01-24

왜 DC bias를 ON 했을 때 4294A의 Sweep delay time이 길어 집니까?
4294A 내부의 DC 바이어스 소스는 스윕 측정을 시작하기 전에 일정한 안정화 시간을 필요로합니다.

FAQ 2016-12-11

What termination model (Balanced vs. Unbalanced) should I use for my M8000 BERT?
For M8000 (M8041A/51A/61A/62A) BERT data outputs, a Termination Model must be selected in the Amplifier section of the Parameters window, Balanced or Unbalanced.

FAQ 2016-07-08

Is it possible to get an error log of incorrectly sent remote commands to my PSA, E4406A, EMC, or ESA Series Spectrum Analyzer?
Yes. PSA, E4406A and the ESA Series (with firmware A.08.00 and later) support this. You may turn Verbose error logging on through the front panel or remotely, SYST:ERR:VERBOSE ON

FAQ 2016-07-05

파워미터 화면에 dBm을 dBmV로 어떻게 변환 합니까?
Load 임피던스가 50ohm이면, dBmV = dBm + 47

FAQ 2016-07-05

왜 E4991A와 4287A는 load 보상 기능이 없나요?
Open,Short 보상에 추가로 Load 보상을 수행하는 것은 DUT 접촉단에서 open/short/load calibration을 하는 것과 동일합니다.

FAQ 2016-04-24

왜 4263A에서는 mF 영역의 높은 캐패시턴스의 정확한 측정이 가능한가요?
4263B는 낮은 임피던스 측정 범위를 갖고 있습니다.

FAQ 2015-04-20

2-포트 ENA로 픽스처 시뮬레이터 기능을 사용할 수 있습니까?
예. 그러나 기능이 제한적입니다...

FAQ 2015-01-09

Does the Keysight solution support the 4x4 MIMO tests for LTE TDD?
LTE TDD 4X4 MIMO Test를 지원하는 Keysight solution이 있습니다.

FAQ 2014-10-20

Is there a summary of available cable test methods when using the FieldFox Hand Held portable analyzers?
Yes. Please refer to the FieldFox Hand Held Cable Test details and methods below.

FAQ 2014-08-11

When automating markers on the ENA is it possible to programmatically query the indicated inductance or capacitance on a Smith Chart?
The inductance / capacitance information cannot be directly queried via the automation interfaces. The inductance (positive reactance, top half of the Smith Chart) or capacitance (negative reactance, lower half of the Smith Chart) is not available as an automation query.

FAQ 2014-08-11

Why does my FieldFox spectrum analyzer preamplifier increase the noise floor when engaged?
The FieldFox spectrum analyzer preamplifier selection will normally reduce the displayed noise floor when activated. However, if the FieldFox RF attenuation AUTO selection is set to ON then the preamp may not reduce the noise floor.

FAQ 2014-03-03

802.11af란 무엇이며, 키사이트는 802.11af 디바이스 테스트 솔루션을 제공합니까?
키사이트의 802.11af 솔루션에 대한 자세한 내용 보기…

FAQ 2014-02-28

I am looking at a 160 MHz OFDM signal at 5 GHz on my MXA or PXA signal analyzer. Why can’t I see the whole signal?
Preselector는 입력의 bandwidth를 제한합니다.

FAQ 2014-01-13

Can I adjust the measurement parameters for the Wireless measurement personalities in E4406A and PSA Series?
네, 여러 개의 파라미터를 조정하는 것이 가능합니다.

FAQ 2014-01-13

Can I set a measurement interval on the U1251A and U1252A Handheld Digital Multimeters?
Yes, you can set a measurement interval on the U1251A and U1252A Handheld Digital Multimeters….

FAQ 2013-11-17

Can I do voltage measurement using the U2802A rather than temperature measurement?
Yes, you can do voltage measurement easily by using the Keysight Measurement Manager (AMM)...

FAQ 2013-11-17

인피니비전 스코프의 샘플레이트를 수동으로 설정할 수 있나요?
인피니비전 스코프의 샘플레이트를 수동으로 설정할 수 있나요?

FAQ 2013-10-17

10MHz 레퍼런스 인/아웃 을 제공하는 오실로스코프는 어떤 모델이 있습니까?
10MHz 레퍼런스 인/아웃 을 제공하는 오실로스코프는 어떤 모델이 있습니까?

FAQ 2013-10-17

Signal Studio에 대한 정보나 API를 사용한 예제 프로그램들을 어디서 찾을 수 있습니까?
Pulse building용 Signal Studio의 help 파일에 정보가 있으며, 해당 파일의 장에 예제 프로그램들이 있습니다.

FAQ 2013-10-16

1 2 3 4 5 6 7 8 9 다음