Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discutez avec un expert

Support technique

Mesure Electronique

Support by Product Model Number:

126-150 sur 217

Tri:
Can we test TD-LTE CCDF in 89601A-BHE?
Yes, additional information can be found here...

FAQ 2009-11-13

What is the main difference between the digital output (DO) of the U2100A, U2600A, U2300A and U2500A?
The DO port of U2100A and U2600A requires external power supply to be pumped into the port...

FAQ 2009-10-20

How much of data points from my data acquired can I save into one file?
What we observed is that if you log your file into *.csv file, the most no. of points you will be capturing is 65536 points. However, if you are saving into *.txt file, it will depend on the type of...

FAQ 2009-09-29

Can U2651A work with 3.3V input signal or not?
As long as there is a potential exceeding 10V and less than 24V between DIin and DIcom, the digital input should be able to observe the incoming signal as logic high...

FAQ 2009-09-29

How do I know what is the best sampling rate to use for my measurement?
Typically if you follow Nyquist theory, your sampling rate should be 2x the highest frequency of the incoming signal that you are measuring. However, we recommend that you use 5x...

FAQ 2009-09-29

Where can I find documentation for the PCIe Analyzer/Exerciser?
The best documentation is found in the online help installed on the controller.

FAQ 2009-08-25

What features or functions are different between ENA and PNA-L?
Followings are the difference between the ENA and the PNA-L...

FAQ 2009-08-21

Does the Keysight E2960B, also known as N5309A, Exerciser have a signal or chip reset for the output signal?
Yes. There is a TCL command for this.

FAQ 2009-08-10

What is the actual size of the E2960B (N5309A) PCIe Exerciser Data Memory?
The E2960B (N5309A) PCI Express internal data memory is 256K.

FAQ 2009-08-10

Why do I receive an error message below ?
Generally, if you are sampling at 60kSa/s and above, you should use high sampling mode to acquire data. This is just a rough guideline. If you encountered this message even when....

FAQ 2009-08-06

How can I remotely connect to all my USB DAQ devices, Digital IOs, and card cage?
Please make sure that your remote PC (which is connected to all your USB instruments) is connected to the same network as yourself. However, your remote PC cannot be connected...

FAQ 2009-08-06

Can I use the MWA software for my ENA without the multiport test set?
Yes, the 4-port ENA without the test set can be controlled by the MWA.

FAQ 2009-07-15

Can we set up a set of different tests (i.e. different limit tests) with the MWA software?
Yes, you can manage up to ten different measurement setups on the same device with the MWA.

FAQ 2009-07-15

How do I confirm if my measurements can be performed with the selected configuration of the E5092A?
The MWA software for the ENA recognizes the architecture of the E5092A, and automatically detects measurement paths that can not be performed with the selected switching configuration.

FAQ 2009-07-15

Can I convert my MWA file of the E5091A Multiport Test Set for utilizing with the E5092A Configurable Multiport Test Set?
Yes, you can convert your MWA file for the E5092A by selecting the equivalent configuration to the E5091A.

FAQ 2009-07-15

Can we control the MWA software from an external PC?
Yes, some functions on the MWA are supported for the remote control.

FAQ 2009-07-15

What are the frequency limitations on the various probes utilized with the Keysight 85070E Dielectric Probe Kit and why?
The 85070E Dielectric Probe options 020, 030 and 050 have maximum frequeny via the E4991A Impedance Analyzer of 3 GHz.

FAQ 2009-06-26

Is there a sample file of the MWA software that I can customize for my DUT?
Yes, MWA files of some example devices can be downloaded from Keysight web page.

FAQ 2009-06-22

Is it possible to supply a DC control voltage to a multiport DUT with the E5092A?
Yes, the E5092A has the functions of internal DC sources that can be supplied to the DUT.

FAQ 2009-05-25

How does one understand the "Count" in InfiniiVision oscilloscope measurement statistics?
"Count" refers to the waveform count from the time Statistics are enabled ...

FAQ 2009-03-30

Do the mean, min, and max values of the InfiniiVision oscilloscopes measurement statistics refer to one signal on the screen or all previously capt...
They refer to the "Count" number of captured waveforms ...

FAQ 2009-03-30

Can the U1731A/U1732A Handheld LCR Meter measure a battery's internal resistance?
No, the U1731A and U1732A Handheld LCR meters cannot measure active parts like batteries etc.....

FAQ 2009-03-25

Is the laser turned on all the time?
The lasers are turned on during the raster scanning.

FAQ 2009-03-01

What is the gray flat plate on the right side of the machine, near the exit conveyor for?
The grey flat plate on the right (exit) side of the machine is for Laser safety.

FAQ 2009-03-01

What happens if you have 2 deposits within 1 span of the laser line?
The laser triangulation measurement is computed the exact same way regardless of how many deposits fall within the 30mm sheet width of the laser beam.

FAQ 2009-02-26

Précédente 1 2 3 4 5 6 7 8 9 Page suivante