Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

1-10 из 10

Упорядочить:
Can I manually set the sample rate on my InfiniiVision oscilloscope?
Although the sample rate cannot be directly set on any InfiniiVision oscilloscope, it can be set indirectly by adjusting the oscilloscopes time per division setting.

FAQ 2012-10-30

Which Keysight oscilloscopes have a 10 MHz reference input/output?
6000 Series, 6000L Series, 7000A Series, 7000B Series, 9000 Series, 54850 Series (Output only), 80000A Series, 80000B Series, 90000A Series and 90000 X-Series

FAQ 2012-10-17

What is the difference between the Auto and Normal trigger modes on InfiniiVision oscilloscopes?
In auto trigger mode, the trigger will be forced if the specified conditions are not met. In normal trigger mode, the trigger will never be forced and a trigger will only occur if the specified conditions are met.

FAQ 2012-10-17

How can I de-embed a test fixture using the 86100C/D Digital Communications Analyzer?
N1010A software with InfiniiSIM-DCA option provides the capability to de-embed and embed fixtures, cables, probes, and other circuit elements.

FAQ 2012-09-25

How do I extract the 32Mpts from U270xA?
One way of “viewing” the full memory waveform is using the zoom function (that the red arrow...

FAQ 2010-09-14

How does one understand the "Count" in InfiniiVision oscilloscope measurement statistics?
"Count" refers to the waveform count from the time Statistics are enabled ...

FAQ 2009-03-30

Do the mean, min, and max values of the InfiniiVision oscilloscopes measurement statistics refer to one signal on the screen or all previously capt...
They refer to the "Count" number of captured waveforms ...

FAQ 2009-03-30

Is it possible to save a previous TDR measurement waveform and load as a comparison for my current TDR measurement?
It is possible to save a previous TDR measurement waveform and load it onto the oscilloscope as a comparison to the current measurement.

FAQ 2008-08-03

Is it possible to save multiple TDR traces and display them as waveforms on the oscilloscope for comparison to my current measurement?
It is possible to save multiple TDR traces as an internal format for future reference...

FAQ 2008-08-03

Can measurements be made on the saved waveforms?

FAQ 2008-08-03