这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

按主题

按内容类型

按产品类别

1-25 / 34

排序:
在 Keysight E4980A 中,什么是“直流电源选件 001(±10 VDC 最大值)”及其用法?
E4980A 选件 001 的增强性能概述——“增强功率和直流偏置选件”

FAQ 2012-12-02

What are the implications of swapping test heads between different Keysight 4287A Impedance Analyzers?
The Keysight 4287A Impedance Analyzer must be used with the furnished test head as a set because it is an indivisible portion of the calibrated 4287A.

FAQ 2012-01-16

Keysight ENA-L是否与871x系列类似,支持内置网页?
不。ENA-L包括型号E5061A和E5062A,与前身871x不同的是,它们没有内置网页服务器。

FAQ 2011-10-07

Is there an outline for configuring my HP Basic to communicate with the Keysight ENA analyzer via SCPI-LAN?

FAQ 2011-10-07

把 Keysight Intuilink 4395A 连接到 4395A, 4396B 分析仪上发生异常
错误是由于分析仪的内存RAM磁盘被格式化为LIF引起的。把磁盘重新格式化为DOS驱动器,应用程序将正确运行。

FAQ 2011-06-28

当通过 Keysight IntuiLink 4395A / 4396B / 49294A 使用 Keysight 4294A 阻抗分析仪时,Excel 软件报告错误“Failed to Capture State from Instrument(无法从仪器捕获状态)”。您有什么建议?
当 4294A 固化软件的版本低于 Rev 1.11 或更高版本所要求的版本时,便会出现下面的错误提示。

FAQ 2011-06-12

What is the interface cable or adapter required to control external GPIB equipment by using VBA macro function of the E4991A?
The 10833A/B/C/D, 82357A or 82357B is required depending on the OS version of the E4991A.

FAQ 2011-06-07

Why isn't calibration option (UK6) available for the 42941A?
The 42941A does not have calibration option because the 4294A specifies total measurement accuracy including the 4294A accuracy.

FAQ 2010-07-12

Is it possible to separate the test head from the E4991A and interconnect them with cables?
Yes. It is possible with option E4991A-010 or option E4991A-007 only.

FAQ 2010-07-02

有没有适用于扩展 E4991A 测试端口的选件或附件?
除了 E4991A-007 温度特征测试套件,不需要安装任何选件或附件来扩展 E4991A 的测试端口。

FAQ 2010-05-24

在不使用 16453A 和 16454A 的情况下,E4991A 选件 002 是否可以测量电容率或导磁率?
否,使用 E4991A 选件 002 测量电容率或导磁率时,必须使用 16453A 或 16454A。

FAQ 2010-05-24

当特定探针台与 E4991A 一起使用时,是否只需使用 E4991A 选件 010?
否,当探针台与 E4991A 一起使用时,通常需要使用 E4991A-010。

FAQ 2010-05-24

Can the 41951A Impedance Test Kit be used with the 4395A/ 4396B?
No, the 41951A cannot be used with the 4395A or 4396B.

FAQ 2010-04-13

Is calibration report included in the 16380V-001 Upgrade Kit which adds the 10 µF standard capacitor to the 16380C?
Yes, the 16380V-001 Upgrade Kit includes the 10 µF standard capacitor and its calibration report.

FAQ 2009-06-23

How do I connect the 16048G 1m BNC connector leads to the 16452A?
You need four BNC(m) to BNC(m) adapters (Keysight part number 1250-0216) to connect the 16048G to the 16452A.

FAQ 2009-01-12

Does the E4980A have 2 m / 4 m cable length option?
No option is required because the standard model of the E4980A has the cable length correction function for 0 m, 1 m, 2 m and 4 m test leads.

FAQ 2008-11-12

Are there any restrictions on the selection of the E4980A options?
The E4980A-001 "Power and DC Bias Enhancement" and E4980A-002 "Bias Current Interface" can be installed in the same unit but cannot be operated simultaneously.

FAQ 2008-11-12

Can the E4980A with option E4980A-005 be upgraded to standard model?
Yes. The E4980A-005 can be upgraded to the standard model by ordering the E4980AU-007 Upgrade Kit. The upgrade can be performed at Keysight service center only.

FAQ 2008-11-12

Can I integrate the 4287A into a semiconductor probe station?
The 4287A can be integrated in a semiconductor probe station, but is not suitable for C-V and high impedance measurement applications for the following reasons:

FAQ 2008-06-11

Can I use the 16048A/D/E with the 4294A?
No, the 4294A adapter setup function only supports 16048G/H cables to extend calibration plane. The 16048A/D/E are not available for the adapter setup and cannot provide accurate and specified measurements.

FAQ 2008-05-26

Can I order brand-new 16380A with ANSI Z540 accredited calibration?
Yes, the 16380A with the ANSI Z540 calibration can be ordered. Order the 16380A with R1295A.

FAQ 2008-05-22

Can I order brand-new 16380C with ANSI Z540 accredited calibration?
Yes, the 16380C with the ANSI Z540 calibration can be ordered. Order the 16380C with R1295A.

FAQ 2008-05-22

Can I order each standard resistor of the 42030A independently?
No, each standard resistor of the 42030A cannot be ordered to purchase independently.

FAQ 2008-05-20

Is calibration report furnished to the 16380C?
Yes, the COC and calibration report for the 16380C standard capacitors are furnished. No option is required for the calibration report furnished.

FAQ 2008-05-20

Can I use the 16454A with an LCR meter or Impedance Analyzer other than the E4991A-002 or 4291A/B-002?
Yes, basically, it is recommended to use an Impedance Analyzer with I-Basic programming function in order to automate the permeability calculation.

FAQ 2008-05-20

1 2 下一页