Here’s the page we think you wanted. See search results instead:

 

Sprechen Sie mit einem Experten

Technical Support

Electronic Measurement

Support by Product Model Number:

1-25 of 158

Sort:
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?
FlexDCA: What Licenses Do I Have, And What Features Do They Enable?

FAQ 2018-12-10

What Information Should I Collect From FlexDCA Before Asking Keysight For Help?
What Information Should I Collect From FlexDCA Before Asking Keysight For Help?

FAQ 2018-12-10

How many peripheral modules (M9379A, M9341A/B, M9161D, M9111A) are supported on M9485A?
M9485A supports one M9341A/B and up to 6 M9111A. There is no software limitation for M9379A and M9161D.

FAQ 2017-05-25

Is E5810B remote USB interface supported in NI MAX environment?
No. E5810B remote USB interface is not supportable in NI MAX environment. The E5810B remote USB interface only detectable in Keysight IO libraries Suite.

FAQ 2014-12-10

Why are USB modular instruments (U2700 Series) and USB DAQ modules (U2300, U2500, U2600 Series) not detectable by the E5810B?
Establish the connection between the USB modular Instrument and the PC directly, and then disconnect the device from the PC (while it’s still powered-on), and connect to E5810B.

FAQ 2014-04-17

IO Libraries Suite: Can the IO Libraries be installed as a silent install?
Yes. The install can be silent with the correct command line parameters.

FAQ 2014-04-07

How do I update the operating system in an N9038A MXE EMI receiver from Windows XP to Windows 7?
See what is required to update the operating system in an N9038A MXE EMI Receiver...

FAQ 2014-04-02

How do I upgrade my E8257D PSG Analog Signal Generator?
Find Information on Hardware Upgrades, Instrument Software, etc....

FAQ 2013-08-20

What is the maximum total length of the RJ45 control cable for connecting multiple 34945EXTs?
The maximum total length of the RJ45 control cables is 140 feet.

FAQ 2013-05-06

Why do I need to pay installation/calibration charges for N4010A license-only upgrades?
The N4010A has several license-only upgrade paths, most of which enhance the base technology options that are already enabled in the unit. Click on the question above for a fuller description.

FAQ 2013-02-06

What is the difference between E2731A & E2731B or E2730A & E2730B tuners for 89600S vector signal analyzer?
There are no visible differences, but there is a performance difference relating to the local oscillators.

FAQ 2012-12-10

What is the typical power consumption of the 86100C and 86100D Digital Communications Analyzer?
Typical measurements of 86100C and 86100D power consumption

FAQ 2012-09-25

What can I do if I fail to establish hardware connection after successfully installing Keysight USB modular instrument driver on a Win7 environment?
If you encountered the event mentioned above, follow the installation best practices steps below.

FAQ 2012-07-25

What can I do if the Keysight USB Modular Instrument driver installations failed to complete installation on a Windows 7 environment?
If you encountered the event mentioned above, follow the installation best practices steps below.

FAQ 2012-07-25

Why do the high-bandwidth 54850-series Infiniium scopes use a BNC connector?
The 54850-series Infiniium scopes use a "precision BNC" connector.

FAQ 2012-05-08

How do I establish a peer-to-peer connection between my PC and an InfiniiVision 5000/6000/7000 Series oscilloscope?
There are two methods ...

FAQ 2012-03-27

Is a W-CDMA Test uSIM included with the W-CDMA TA and LA?
The W-CDMA Test uSIM is included with the E6703C W-CDMA Lab Application. It is not included with E1963A Test Application.

FAQ 2012-03-02

How do I make spectrum analysis measurements on signals above 110 GHz using a PSA Series Spectrum Analyzer (E4440A, E4446A, E4448A)?
With the addition of option AYZ on the PSA a user can connect external harmonic mixers to measure signals up to 325 GHz. Mixers in the frequency range of 110 to 325 GHz are available from third party venders such as Olssen Microwave.

FAQ 2012-02-28

Do I need a bias tee or a diplexer for the 11970 or 11974 series harmonic mixers?
Neither the 11970 or 11974 Series requires a bias tee or diplexer.

FAQ 2012-02-28

What is the frequency range of the N5532A Sensor Module?
100 kHz to 4.2 GHz, 10 MHz to 18 GHz, 30 MHz to 26.5 GHz, and 30 MHz to 50 GHz.

FAQ 2012-02-26

What is difference between connector option 021, 022 and 023 in 8167 series and 8168 series tunable laser source (8167A/B, 8168A/B/C/D/E/F)?

FAQ 2012-02-17

The Keysight 8761B SPDT Coaxial Switches are not listed in the "Keysight 34945A, L4445A and L4490A/L4491A Configuration Guide". Why?
Due to the 8761B’s internal design the RF path selection is achieved via DC polarity reversal across the coil control terminals. The Keysight 34945A, L4445A and L4490A/L4491A Control Units do not provide a polarity reversal mode. Thus the 8761B cannot be controlled by the 34945A, L4445A and L4490A/L4491A Control Units.

FAQ 2012-01-16

Is there an outline for configuring my HP Basic to communicate with the Keysight ENA analyzer via SCPI-LAN?

FAQ 2011-10-07

Why i can't find other languages help file setting in U160X A/B series HH oscilloscope?
In order to access to other language, please go to respective product support page in www.Keysight.com. Go to Driver & Software page, select Firmware Update.

FAQ 2011-09-12

What are the minimum system requirements for i3070 TDW?

FAQ 2011-03-02

1 2 3 4 5 6 7 Next