이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

1-25 / 172

정렬방식:
FieldFox Manuals, Firmware, Software and Product Support
Manuals, firmware upgrade, software trials & upgrade and support page for FieldFox analyzers

FAQ 2018-11-14

Is calibration included in the 86100DU-WN7 Windows 7 upgrade?
86100DU-WN7 is a return to service center upgrade and does include calibration, in addition to a certificate of calibration and data.

FAQ 2017-06-28

Is it possible to develop specific macros for E5061B to support TRL cal or the unknown thru method under a 9-term calibration method?
Yes, it is possible to perform a user developed 8-term calibration, like TRL, using an external program for the E5061B. Click on the question for additional information.

FAQ 2017-06-28

When working with high power setups, is it valid to calibrate at low powers and then increase the power after calibration?
Yes, this is valid as long as the source attenuator setting does not change. Click on the question for additional information.

FAQ 2017-06-28

Can the PNA-X support SSLT or SSST calibration techniques?
Yes; however, the Cal Kit must be defined properly to work. The Cal can be modified via Advanced Modify Cal Kit for Definitions under the Calibration menu.

FAQ 2017-06-28

Why is the linearity of E441x, E930x, E932x and E/V/W8486A Power Sensors not tested per sensor’s dynamic range?
In actuality, there is little necessity to test linearity of the E4412A and E4413A Power Sensors below -20dBm….

FAQ 2017-03-29

How to maintain 16195B?
The 16195B which consists of Open, Short, 50 Ω Load and Low-loss Capacitor terminations is calibration kit for LCR Meter/Impedance Analyzer and Network Analyzer (NA). The 16195B itself does not have warranted specification as independent product. Maintenance of the 16195B depends on what instrument you calibrate with 16195B.

FAQ 2017-03-15

왜 5MHz 또는 15MHz에서 측정데이터가 불연속 적으로 나타나는지와 4294A에서는 이 현상을 제거할 수 있습니까?
4294A는 측정 주파수 테스트 리드의 공진을 제거하기 위해 50 옴에서 각 측정 단자를 terminating해서 110 MHz까지의 주파수 측정범위가 확장되어 있습니다.(4294A 내부의 리드를 포함합니다).

FAQ 2015-10-28

What is the calibration password to unlock the instrument?
The security code is "AT3446XA"...

FAQ 2015-09-21

Does FieldFox support data-based cal kits?
FAQ for FieldFox support of Cal Kits

FAQ 2015-09-09

How should I set the "Adapter Setting" of the 4294A when using the 16089A/B/C/D/E?
Please set to "NONE".

FAQ 2015-06-09

ENA를 사용하여 어떻게 75 Ω 측정을 할 수 있습니까?
ENA를 사용하여 시스템 특성 임피던스를 75 Ω으로 변경시켜 75 Ω 측정을 할 수 있습니다.

FAQ 2015-03-09

Certificates (Certification) for Calibration
Search and download calibration certificates for your Keysight instruments by model and serial number.

FAQ 2014-09-10

Where is my Calibration Certificate for the E6650A EXF?
The E6650A (EXF) does not have a calibration certificate because of its flexible TRX configuration. Only the M9300A Reference and M9440A TRX modules installed inside the E6650A chassis have a calibration certificate

FAQ 2014-09-09

교정 키트 토크 렌치를 위한 인증(및 재인증) 프로세스는 무엇입니까?

FAQ 2014-03-24

What is included with Option UK6?
Beginning December 19, 2013, the list below describes what will be included with Option UK6:

FAQ 2014-02-27

Keysight Accreditation Milestones: Australia and Great Britain
Keysight’s Melbourne service center was first accredited by NATA in August 1974; the Winnersh service center was accredited by the BCS in August 1984.

FAQ 2014-02-14

ENA 시간 도메인 측정의 정확도는 얼마입니까?
TDR/TDT 측정 불확도는 다음 표에 명시되어 있습니다.

FAQ 2014-02-01

Can you use EXA to run enhanced factory calibration or does it only work with PXA, MXA and PSA?
EXA는 보장되지 않습니다.

FAQ 2014-01-13

Are there any calibration options available for the U1251A/U1252A Handheld Digital Multimeter?
Yes, there are a variety of calibration options available for the U1251A and U1252A Handheld Digital Multimeter…

FAQ 2013-11-17

What calibrations are available on X-Series, PSA, ESA analyzers and X-Series, ESG-C, PSG Signal Generators at time of initial sale from the factory?
Details regarding time of sale calibrations can be found here...

FAQ 2013-10-15

ISO 17025 and Accreditation
Keysight provides ISO 17025 compliant services. Get more information and learn how to meet ISO 17025 requirements for electronic test equipment.

FAQ 2013-07-10

How can I perform the calibration/compensation when I use the 16094A with a 7-mm connector extension cable?
It is recommended to perform the following compensation procedure...

FAQ 2013-06-05

E4980A에서 RF 동축 케이블 사용 시 전기적 길이 보상이 필요하나요?
아니요, 필요하지 않습니다.

FAQ 2013-04-17

Do temperature changes affect the factory channel correction calibration?
temperature changes, channel correction calibration, factory correction calibration,x-series signal generators

FAQ 2013-02-26

1 2 3 4 5 6 7 다음