検索された製品ページを表示しています その他の検索結果:

 

お問い合わせ窓口

テクニカルサポート

電子計測

製品番号で検索:

1-25 / 182

並べ替え
Can the PNA-X support SSLT or SSST calibration techniques?
Yes; however, the Cal Kit must be defined properly to work. The Cal can be modified via Advanced Modify Cal Kit for Definitions under the Calibration menu.

FAQ 2017-06-28

When working with high power setups, is it valid to calibrate at low powers and then increase the power after calibration?
Yes, this is valid as long as the source attenuator setting does not change. Click on the question for additional information.

FAQ 2017-06-28

Is calibration included in the 86100DU-WN7 Windows 7 upgrade?
86100DU-WN7 is a return to service center upgrade and does include calibration, in addition to a certificate of calibration and data.

FAQ 2017-06-28

Is it possible to develop specific macros for E5061B to support TRL cal or the unknown thru method under a 9-term calibration method?
Yes, it is possible to perform a user developed 8-term calibration, like TRL, using an external program for the E5061B. Click on the question for additional information.

FAQ 2017-06-28

Why is the linearity of E441x, E930x, E932x and E/V/W8486A Power Sensors not tested per sensor’s dynamic range?
In actuality, there is little necessity to test linearity of the E4412A and E4413A Power Sensors below -20dBm….

FAQ 2017-03-29

How to maintain 16195B?
The 16195B which consists of Open, Short, 50 Ω Load and Low-loss Capacitor terminations is calibration kit for LCR Meter/Impedance Analyzer and Network Analyzer (NA). The 16195B itself does not have warranted specification as independent product. Maintenance of the 16195B depends on what instrument you calibrate with 16195B.

FAQ 2017-03-15

【VSA】【SG】RF信号をキャプチャして信号源で再生することはできますか?
はい。ベクトル・シグナル・アナライザを使用することで、RFキャプチャ信号を信号源から再生することが可能です。

FAQ 2016-02-03

What is the calibration password to unlock the instrument?
The security code is "AT3446XA"...

FAQ 2015-09-21

Does FieldFox support data-based cal kits?
FAQ for FieldFox support of Cal Kits

FAQ 2015-09-09

How should I set the "Adapter Setting" of the 4294A when using the 16089A/B/C/D/E?
Please set to "NONE".

FAQ 2015-06-09

ENAで75 Ω測定を実行する方法は?
ENAで75 Ω測定を実行するには、システム特性インピーダンスを75 Ωに変更します。

FAQ 2015-03-09

Certificates (Certification) for Calibration
Search and download calibration certificates for your Keysight instruments by model and serial number.

FAQ 2014-09-10

Where is my Calibration Certificate for the E6650A EXF?
The E6650A (EXF) does not have a calibration certificate because of its flexible TRX configuration. Only the M9300A Reference and M9440A TRX modules installed inside the E6650A chassis have a calibration certificate

FAQ 2014-09-09

ENAオプションTDRタイム・ドメイン測定の確度は?
TDR/TDTの測定の不確かさを以下の表に示します。

FAQ 2014-04-07

電子校正キットのトルクレンチは校正できますか?
トルクレンチの校正証明書も必要な場合は、別途費用をお支払い頂き、トルクレンチ校正としてご提供致します。

FAQ 2014-03-24

Keysight Accreditation Milestones: Australia and Great Britain
Keysight’s Melbourne service center was first accredited by NATA in August 1974; the Winnersh service center was accredited by the BCS in August 1984.

FAQ 2014-02-14

オプションUK6の内容
E8257D、E8257N、E8267D、E8663D、N5171B、N5172B、N5173B、N5181A、N5181B、N5182A、N5182B、N5183A、N5183B・ スペクトラム/シグナル・アナライザE4402B、E4403B、E4404B、E4405B、E4407B、E4408B、E4411B、E4440A...

FAQ 2014-01-28

FieldFoxハンドヘルド・アナライザのカスタマ・サポート(すべてのFieldFoxモデル)
セントラルFieldFox Webサイトには、アップグレード、ファームウェア、データ・リンク・ソフトウェア、ユーザーズ・ガイド、プログラミング・ガイド、セキュアな環境での使用方法、使用可能な校正キットなどへのリンクが含まれています。

FAQ 2014-01-16

Xシリーズ/PSA/ESAアナライザおよびXシリーズ/ESG-C/PSG信号発生器の工場出荷時に、オプションA6Jまたは1A7校正を利用できますか?
できます。特定のPSA構成については、詳細をこちらでご確認ください。

FAQ 2013-10-18

ISO 17025および認証評価
KeysightはISO 17025に準拠したサービスを提供しています。詳細および電子計測器に関するISO 17025の要件を満たす方法を学習できます。

FAQ 2013-07-10

How can I perform the calibration/compensation when I use the 16094A with a 7-mm connector extension cable?
It is recommended to perform the following compensation procedure...

FAQ 2013-06-05

ユーザ・チャネル補正ルーチンを実施する場合、スペクトラム・アナライザ/パワー・メータと信号源の間のケーブルを補償する必要はありますか?
必要ありません。ケーブル誤差は校正済みです。

FAQ 2013-03-12

ユーザ・チャネル補正校正について、スポットで行った方が良いでしょうか、レンジ全体で行った方が良いでしょうか?
レンジ全体で行っても問題ありませんが、必須ではありません。

FAQ 2013-03-12

ユーザ・チャネル補正校正で、ユーザ補正周波数範囲外の周波数には工場補正が適用されるのでしょうか?
はい、校正データの配列間でスムージングを行って、不連続がないようにしています。

FAQ 2013-03-12

工場チャネル補正校正が有効な期間は?
工場チャネル補正は、信号源が動作している限り有効です。

FAQ 2013-03-12

1 2 3 4 5 6 7 8 次へ