Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

Refine the List

remove all refinements

By Topic

By Type of Content

By Product Category

1-25 of 43

Sort:
Is it possible to develop specific macros for E5061B to support TRL cal or the unknown thru method under a 9-term calibration method?
Yes, it is possible to perform a user developed 8-term calibration, like TRL, using an external program for the E5061B. Click on the question for additional information.

FAQ 2017-06-28

How to maintain 16195B?
The 16195B which consists of Open, Short, 50 Ω Load and Low-loss Capacitor terminations is calibration kit for LCR Meter/Impedance Analyzer and Network Analyzer (NA). The 16195B itself does not have warranted specification as independent product. Maintenance of the 16195B depends on what instrument you calibrate with 16195B.

FAQ 2017-03-15

How should I set the "Adapter Setting" of the 4294A when using the 16089A/B/C/D/E?
Please set to "NONE".

FAQ 2015-06-09

How can I make 75 Ω measurements using the ENA?
You can make 75 Ω measurements with the ENA by shifting system characteristic impedance to 75 Ω.

FAQ 2015-03-09

How can I perform the calibration/compensation when I use the 16094A with a 7-mm connector extension cable?
It is recommended to perform the following compensation procedure...

FAQ 2013-06-05

What is the difference between an "ECal Confidence Check" and a Network Analyzer "System Verification" test?
The ECal Confidence Check is a method to check the accuracy of a calibration performed with either a mechanical cal kit or an ECal module. System verification testing provides network analyzer users a method to verify that the network analyzer is ...

FAQ 2012-12-18

What mechanical calibration kits and ECal (electronic calibration) kits does the ENA support?
Please refer to following documents...

FAQ 2012-12-11

Does the ENA 6 series support User Characterized ECal?
No.

FAQ 2012-12-10

Does the ENA allow user access to the Error Coefficient Arrays?

FAQ 2012-04-17

How is trace math implemented within the Keysight Technologies Vector Network Analyzers?

FAQ 2012-01-11

After performing a calibration with a user defined calibration kit, all log magnitude data is displayed as -200 dB; why?

FAQ 2011-10-07

Is there an error in the delay/thru definition for the 85039B F-Type Calibration Kit?
Yes.

FAQ 2011-10-07

Why isn't calibration option (UK6) available for the 42941A?
The 42941A does not have calibration option because the 4294A specifies total measurement accuracy including the 4294A accuracy.

FAQ 2010-07-12

Can 4263B preserve Open/Short/Load correction data by using Save/Recall function?
No.

FAQ 2010-07-02

Why does measurement data exhibit a discontinuity at 5 MHz or 15 MHz and how can the 4294A get rid of this phenomenon?
The 4294A extends its measurement frequency range up to 110 MHz by terminating each measurement terminal with 50 ohm in order to eliminate the resonance of test leads (including leads inside the 4294A).

FAQ 2010-07-02

The 16085B 4-Terminal Pair to 7 mm (APC-7) adapter: Is it advisable to use fixture compensation standards or coaxial calibration standards?

FAQ 2010-07-02

Why does the DC resistance measurement function of the 4287A require to be calibrated at the same time with Open/Short/Load calibration?
The specified accuracy for the DC resistance measurement is applied when the Open/Short/Load calibration for the DC resistance measurement is performed.

FAQ 2010-07-02

Do the coaxial Short and 50 Ω Load terminations for the 42941A have accuracy specifications?
No, both the coaxial Short and 50 Ω Load standard terminations for the 42941A do not have accuracy specifications.

FAQ 2010-07-02

How should I define or select the residual inductance values of Shorting Bars when performing Short compensation on the E4991A or the 4287A?
Nowadays, the authorized standards stipulate the dimensions of shorting devices and the Short Compensation method which uses the defined inductance values of the shorting devices. It is recommended to consider these authorized standards.

FAQ 2010-07-02

When the 4287A displays inaccurate Rdc measurement values, what is required to make more proper Rdc measurements for contact check?
Perform Open/Short/Load calibration and Open/Short compensation.

FAQ 2010-01-26

What is the recommended calibration period of the 16190B?
The recommended calibration period is every 12 months.

FAQ 2009-11-17

What is the recommended calibration period of the 42030A?
The recommended calibration period is every 12 months.

FAQ 2009-11-17

What is the recommended calibration period of the 16380C?
The recommended calibration period is every 12 months.

FAQ 2009-11-17

What is the recommended calibration period of the 16380A?
The recommended calibration period is every 12 months.

FAQ 2009-11-17

Is calibration report included in the 16380V-001 Upgrade Kit which adds the 10 µF standard capacitor to the 16380C?
Yes, the 16380V-001 Upgrade Kit includes the 10 µF standard capacitor and its calibration report.

FAQ 2009-06-23

1 2 Next